package ti.sysbios.interfaces |
|
Contains all interface specifications
The I<mod>Support interfaces define "internal" interfaces used by the
<mod> modules in their implementation. These interfaces simplify the
process of porting to a new architecture; one only needs to implement
the I<mod>Support interface to enable the full functionality of the
ti.sysbios.<mod> module.
package ti.sysbios.interfaces [2, 0, 0, 0] {
// Cache Interface
// Hardware Interrupt Support Module
// Interface for PowerSupport Manager
// Interface for family specific Settings modules
// Interface for Timer Peripherals Manager
// Interface for TimerSupport Manager
}
generated on Tue, 01 Sep 2009 00:35:54 GMT