1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Memory.xdc ========
    15     */
    16    
    17    /*!
    18     *  ======== Memory ========
    19     *  Static and run-time memory manager
    20     *
    21     *  All memory allocations are performed either by
    22     *  `{@link #staticPlace Memory.staticPlace()}` at build time or through
    23     *  `{@link #alloc Memory_alloc()}` (or its varients `Memory_calloc()`, 
    24     *  `Memory_valloc()`, etc.) at run-time. 
    25     *
    26     *  Run-time memory management is performed by modules that
    27     *  implement the `{@link xdc.runtime.IHeap}` interface.  The `Memory` module
    28     *  itself simply provides a common interface for any variety of system and
    29     *  application specific memory management policies implemented by `IHeap`
    30     *  modules; for example, `{@link HeadStd}` and `{@link HeadMin}`.
    31     *
    32     *  Heap instances are created statically or dynamically via heap specific
    33     *  create functions and these instances are then passed as an input
    34     *  parameter to the `Memory` calls that have a
    35     *  `{@link xdc.runtime.IHeap#Handle}` parameter.
    36     */
    37    module Memory {
    38    
    39        /*!
    40         *  ======== Q_BLOCKING ========
    41         *  Blocking quality
    42         *
    43         *  `{@link xdc.runtime.IHeap}`s with this "quality" may cause the
    44         *  calling thread to block; i.e., suspend execution until another thread
    45         *  leaves the gate.
    46         */
    47        const Int Q_BLOCKING = 1;
    48        
    49        /*!
    50         *  ======== Size ========
    51         *  Type to be used to specify heap buffer sizes
    52         */
    53        typedef UArg Size;
    54    
    55        /*!
    56         *  ======== Stats ========
    57         *  Memory heap statistics
    58         *
    59         *  This structure defines generic statistics that must be supplied
    60         *  by each module that implements the `{@link xdc.runtime.IHeap}`
    61         *  interface.
    62         *
    63         *  @field(totalSize)         total size (in MADUs) of heap.
    64         *  @field(totalFreeSize)     current size (in MADUs) of free memory in 
    65         *                            the heap
    66         *  @field(largestFreeSize)   current largest contiguous free block 
    67         *                            (in MADUs)
    68         */
    69        struct Stats {
    70            Size totalSize;
    71            Size totalFreeSize;
    72            Size largestFreeSize;
    73         }
    74         
    75        /*! @_nodoc */
    76        @XmlDtd
    77        metaonly struct Module_View {
    78            SizeT maxDefaultTypeAlignment;
    79        };
    80    
    81        /*!
    82         *  ======== defaultHeapInstance ========
    83         *  The default heap.
    84         *
    85         *  If no heap is specified in the `Memory` module's methods (i.e.
    86         *  heap == `NULL`) `defaultHeapInstance` is used. If
    87         *  `defaultHeapInstance` is not set (or set to `null`), a
    88         *  `{@link xdc.runtime.HeapStd}` heap instance is created and assigned
    89         *  to this configuration parameter. The size of the heap is determined
    90         *  by the `{@link #xdc.runtime.HeapStd.HEAP_MAX}` parameter.
    91         *
    92         *  By default, all modules are configured with a `null` instance heap.
    93         *  Instances created by modules with a `null` instance heap are
    94         *  allocated from the `defaultHeapInstance` heap.
    95         */
    96        config IHeap.Handle defaultHeapInstance;
    97    
    98        /*!
    99         *  ======== defaultHeapSize ========
   100         *  The size (in target MADUs) of the `defaultHeapInstance`.
   101         *
   102         *  This parameters is used when the `{@link #defaultHeapInstance}`
   103         *  is not configured. 
   104         */
   105        metaonly config int defaultHeapSize = 0x1000;
   106    
   107        /*!
   108         *  ======== alloc ========
   109         *  Allocate a block of memory from a heap.
   110         *
   111         *  @param(heap)    heap from which the memory is allocated
   112         *
   113         *                  The `heap` is created by a module that implements
   114         *                  the `{@link xdc.runtime.IHeap}` interface.
   115         *                  If `heap` is `NULL`, the 
   116         *                  `{@link #defaultHeapInstance}` is used.
   117         *
   118         *  @param(size)    requested memory block size (in MADUs)
   119         *  @param(align)   alignment (in MADUs) of the block of memory
   120         *
   121         *                  A value of 0 denotes maximum default type alignment.
   122         *
   123         *  @param(eb)      pointer to error block
   124         *
   125         *  @a(returns)     
   126         *  If the allocation was successful, `Memory_alloc()` returns non-`NULL` 
   127         *  pointer to the allocated and uninitialized block; otherwise it returns 
   128         *  `NULL` and the error block will indicate the cause of the error.     
   129         */
   130        Ptr alloc(IHeap.Handle heap, SizeT size, SizeT align, Error.Block *eb);
   131    
   132        /*!
   133         *  ======== calloc ========
   134         *  Allocate a block of memory from a heap and zero out the contents.
   135         *
   136         *  @param(heap)    heap from which the memory is allocated
   137         *
   138         *                  The `heap` is created by a module that implements
   139         *                  the `{@link xdc.runtime.IHeap}` interface.
   140         *                  If `heap` is `NULL`, the 
   141         *                  `{@link #defaultHeapInstance}` is used.
   142         *
   143         *  @param(size)    requested memory block size (in MADUs)
   144         *  @param(align)   alignment (in MADUs) of the block of memory
   145         *
   146         *                  A value of 0 denotes maximum default type alignment.
   147         *
   148         *  @param(eb)      pointer to error block
   149         *
   150         *  @a(returns)
   151         *  If the allocation was successful, `Memory_calloc()` returns non-`NULL` 
   152         *  pointer to the allocated and initialized block; otherwise it returns 
   153         *  `NULL` and the error block will indicate the cause of the error.     
   154         */
   155        Ptr calloc(IHeap.Handle heap, SizeT size, SizeT align, Error.Block *eb);
   156    
   157        /*!
   158         *  ======== free ========
   159         *  Frees the space if the heap manager offers such functionality.
   160         *
   161         *  @param(heap)   heap that the block of memory will be freed back to.
   162         *
   163         *                 The `heap` is created by a module that implements
   164         *                 the `{@link xdc.runtime.IHeap}` interface.
   165         *                 If `heap` is `NULL`, the 
   166         *                 `{@link #defaultHeapInstance}` is used.
   167         *
   168         *  @param(block)  block of memory to free back to the heap
   169         *  @param(size)   size (in MADUs) of the block of memory to free.
   170         *
   171         */
   172        Void free(IHeap.Handle heap, Ptr block, SizeT size);
   173        
   174        /*!
   175         *  ======== getStats ========
   176         *  Obtain statistics from a heap.
   177         *
   178         *  @param(heap)    the heap to get the statistics from
   179         *
   180         *                  The `heap` is created by a module that implements
   181         *                  the `{@link xdc.runtime.IHeap}` interface.
   182         *                  If `heap` is `NULL`, the 
   183         *                  `{@link #defaultHeapInstance}` is used.
   184         *
   185         *  @param(stats)   the output buffer for the returned statistics
   186         */
   187        Void getStats(IHeap.Handle heap, Stats *stats);
   188        
   189        /*!
   190         *  ======== query ========
   191         *  Test for a particular `{@link xdc.runtime.IHeap}` quality.
   192         *
   193         *  There currently is only one quality, namely `{@link #Q_BLOCKING}`.
   194         *
   195         *  @param(heap)    the heap to query
   196         *
   197         *                  The `heap` is created by a module that implements
   198         *                  the `{@link xdc.runtime.IHeap}` interface.  If `heap`
   199         *                  is `NULL`, the `{@link #defaultHeapInstance}`
   200         *                  is queried
   201         *
   202         *  @param(qual)    quality to test
   203         *
   204         *                   For example: `{@link #Q_BLOCKING}`.
   205         *
   206         *  @a(returns)
   207         *  If `heap` has the `qual` quality, this method returns `TRUE`,
   208         *  otherwise it returns `FALSE`.
   209         */
   210        Bool query(IHeap.Handle heap, Int qual);
   211    
   212        /*!
   213         *  ======== getMaxDefaultTypeAlignMeta ========
   214         *  Return the largest alignment required by the target
   215         *
   216         *  This method scans the standard base types supported by the current
   217         *  configuration's target
   218         *  (`{@link xdc.cfg.Program#build Program.build.target}`) and returns
   219         *  the largest alignment required for these types.
   220         *
   221         *  @a(returns)     Returns target-specific alignment in MADUs. 
   222         *
   223         *  @see xdc.bld.ITarget#stdTypes
   224         */
   225        metaonly SizeT getMaxDefaultTypeAlignMeta();
   226        
   227        /*!
   228         *  ======== getMaxDefaultTypeAlign ========
   229         *  Return the largest alignment required by the target
   230         *
   231         *  `getMaxDefaultTypeAlign` returns the largest alignment
   232         *   required for all the standard base types supported by the current
   233         *  configuration's target
   234         *  (`{@link xdc.cfg.Program#build Program.build.target}`) 
   235         *
   236         *  This is the runtime version of the
   237         *  `{@link #getMaxDefaultTypeAlignMeta}` function.      
   238         *
   239         *  @a(returns)     Returns target-specific alignment in MADUs. 
   240         *
   241         *  @see #getMaxDefaultTypeAlignMeta
   242         */
   243        SizeT getMaxDefaultTypeAlign();
   244    
   245        /*!
   246         *  ======== staticPlace ========
   247         *  Statically places buffers.
   248         *
   249         *  This function places the object specified by `obj` into the specified
   250         *  memory section. The section string is a target-specific name that is
   251         *  interpreted by the underlying target tool-chain.  In the case of TI
   252         *  tool-chains, this section can be a subsection (e.g.
   253         *  ".data:someSection").
   254         *
   255         *  The amount of memory that is created for `obj` is dependent on its
   256         *  size and the value of the property `length`. The length (number
   257         *  of elements in an array) is set before the `staticPlace()` is called.
   258         *  For example, setting `obj.length = 5;` before calling `staticPlace()`,
   259         *  will create `5 * sizeof (obj)` MADUs of memory.
   260         *
   261         *  If 0 is specified for the alignment, the allocated buffer is aligned 
   262         *  as determined by the target toolchain. For instance, if `obj` is an
   263         *  array of structs that have only 16-bit integers, the alignment would
   264         *  be on a 16-bit boundary. 
   265         *
   266         *  All non-zero alignments must be a power of 2. Not all targets support
   267         *  directives that allow one to specify alignment. The readonly config
   268         *  parameter
   269         *  `{@link xdc.cfg.Program#build Program.build.target.alignDirectiveSupported}`
   270         *  can be used to determine if the target supports alignment directives. 
   271         *
   272         *  @param(obj)     object to place
   273         *
   274         *      This object always has the `length` property; `obj.length`
   275         *      determines the size of the allocated buffer for `obj`
   276         *
   277         *  @param(align)   the alignment required by `obj`
   278         *
   279         *  @param(section) section name to contain `obj`
   280         *
   281         *      This parameter names the section where `obj` will be placed.  If
   282         *      this parameter is `null`, no explicit placement is done.
   283         *
   284         *  @a(returns)
   285         *  Returns `false` if the alignment request cannot be honored. The `obj` 
   286         *  is still placed regardless of the return code.
   287         */
   288        metaonly Bool staticPlace(any obj, SizeT align, String section);
   289    
   290        /*!
   291         *  ======== valloc ========
   292         *  Allocate a block of memory from a heap and initialize the contents
   293         *  to the value specified.
   294         *
   295         *  @param(heap)    heap from which the memory is allocated
   296         *
   297         *                  The `heap` is created by a module that implements
   298         *                  the `{@link xdc.runtime.IHeap}` interface.
   299         *                  If `heap` is `NULL`, the 
   300         *                  `{@link #defaultHeapInstance}` is used.
   301         *
   302         *  @param(size)    requested memory block size (in MADUs)
   303         *  @param(align)   alignment (in MADUs) of the block of memory
   304         *
   305         *                  A value of 0 denotes maximum default type alignment.
   306         *
   307         *  @param(value)   value to initialize the contents of the block
   308         *  @param(eb)      pointer to error block
   309         *
   310         *  @a(returns)
   311         *  If the allocation was successful, `Memory_valloc()` returns non-`NULL` 
   312         *  pointer to the allocated and initialized block; otherwise it returns 
   313         *  `NULL` and the error block will indicate the cause of the error.     
   314         */
   315        Ptr valloc(IHeap.Handle heap, SizeT size, SizeT align, Char value, 
   316                   Error.Block *eb);
   317    
   318    internal:
   319    
   320        proxy HeapProxy inherits IHeap;
   321    
   322        struct Module_State {
   323            SizeT maxDefaultTypeAlign;
   324        }
   325    }
   326    /*
   327     *  @(#) xdc.runtime; 2, 1, 0,420; 6-10-2013 12:10:04; /db/ztree/library/trees/xdc/xdc-z51x/src/packages/
   328     */
   329