Texas Instruments Technology for Innovators(tm)

XDCtools 3.16.04.39 Release Notes

June 11, 2010

Introduction, Documentation, License, What's New, Upgrade & Compatibility Information, Host Support, Dependencies, Device Support, Validation Info, Known Issues, Version Information, Technical Support.


Introduction

RTSC / XDC (eXpanDed C) is a standard for reusable software components, optimized for real-time embedded systems. RTSC components have hardware-neutral formal interfaces, are configurable offline to optimize memory and performance, and support custom automation in the development environment via a scripting language.

The XDCtools product includes the following components:

back to top

Documentation

The product documentation for this release is available in two formats:

Both formats are delivered with the product in the docs subdirectory. The most up-to-date docs can also be viewed on-line at:

Release notes from previous product releases are available in the relnotes_archive directory.

back to top


License

XDCtools contains elements released under the Eclipse Public License v1.0 and a number of other open-source licenses, detailed here.


What's New

The following  changes are included in 3.16.04.39:




Defect history for 3.16.04.39 (This Release)

Bugs against the XDCtools product maybe filed in the eclipse bugzilla.
The following defects were resolved in this release:

IDHeadline
ECL304758microsoft.targets.arm.WinCE's default platform is incorrectly an x86 device
ECL306433a second package release that specifies "exportAll" has an incomplete manifest
ECL312648When assigning Pkg.libTemplate, compile options need extra space padding
ECL315822Errant xdc.runtime dependency during config

back to top


Upgrade and Compatibility Information

Warning:Starting with XDCtool 2.95, RTSC packages with target content are incompatible with target content from previous releases. Compatibility of meta only content is not affected. Packages with target content would require a recompile. Starting with XDCtool 3.00 release both backward and forward compatibility is maintained for all content.

Package Compatibility Keys

The packages comprising the XDCtools release are uniquely identified by a compatibility key defined in the package.xdc file of a package. Please note that the package compatibility keys are independent of XDC product release numbers.

Package compatibility keys are intended to:

  1. Enable tooling to identify incompatibilities between components, and
  2. Convey a level of compatibility between different releases to set end user expectations.

Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:



back to top

Host Support

This release supports the following hosts:

back to top

Dependencies

This release requires the following other software components and tools versions to successfully function:

back to top

Device Support

This release supports the following device families:

back to top

Validation Information

This release was built and validated against using the following components:

back to top


Known Issues

The following major issue is known to exist in this release.

CCSv4 IDE integration not supported on Linux

Command-line operation on Linux is fully supported.

Outstanding defects in this release are shown below:

IDHeadline
ECL280878xgconf: Deleting project with cfg file open doesn't close the window
ECL280854
XGCONF: On changing Configuro �D options, config is not re-validated, need to re-save script
ECL309211
configuro exit status is 0 even when command usage is wrong
ECL287731Updating XDC version fails to regenerate package/rel/*.tar.dep files
ECL289229When xs xdc.tools.repoman fails it should exit with non-zero exit status
ECL289144cdoc: @_nodoc on per-instance config is ignored
ECL285460cdoc does not properly escape '<' in strings
ECL285331XGCONF gives NullPointerException when certain modules are used.
ECL280875xgconf: hand-editing to add ti.bios.MEM throws NPE
ECL280861xgconf: Renaming an instance does not create a Program.global entry if the instance has no Params struct
ECL276101xgconf: hover help text does not properly format xdoc text
ECL280858xgconf: Can't double-click on Problems view to go to offending module/instance
ECL301761xgconf should add the project cfg path when processing app.cfg file
ECL303793Platform wizard does not support c28xx devices
ECL313408package whose repository is in the current directory can cause NullPointer exception
ECL264025cannot define an interface instance as a global variable
ECL312963SysMin_ready fails
ECL307806the config error for uninitialized array values is confusing
ECL312965ROV view of SysMin outbuf is garbled
ECL302355Closure tool gives erroneous message
ECL296749Dereferencing undefined object in user's Build.targets array leads to confusing error msg
ECL309514System_printf bug with extended specifiers
ECL302614Incomprehensible error message when incorrect package name is loaded
ECL314790Default JVM memory not enough for cdoc
ECL314909Closing the Path app (launched from CCS) with File|Exit crashes CCS
ECL291830can't use modules that have @NoRuntime attribute set


back to top


Version Information

All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 3.15.01.51-eng or 3.15.01.58-beta).

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. xdctools_3_15_00_50.

Subsequent releases of patch upgrades will be identified by the patch number, ex. XDCtools 3.15.01.67 with directory xdctools_3_15_01_67. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.

back to top


Technical Support

Support questions on the product should be posted to the RTSC newsgroup.

back to top


Last updated: June 11, 2010 Build Ver: 3.16.04.39 Rev: l39