From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC

Command Line Tools

Command line tools overview

Contents

This reference provides an overview of the command-line tools provided for creating and working with packages. In addition, it provides a brief description of the most frequently used commands.

Core commands

XDCtools requires just two "core" commands shown in the table below.

Command - xdc eXpanDed C package build command
Command - xs XDCscript interpreter

XDCscript commands

In addition to the core commands above, many of the basic tools are implemented as packages containing XDCscript utilities. Each of the commands shown in the table below is run using the xs utility above.

Command - xdc.tools.cdoc Package documentation tool
Command - xdc.tools.cdoc.sg Interactive package documentation tool
Command - xdc.tools.check Repository compatibility check tool
Command - xdc.tools.closure Closure tool
Command - xdc.tools.configuro Target content configuration tool
Command - xdc.tools.path Package path display tool
Command - xdc.tools.path.sg Interactive Package Path browser tool
Command - xdc.tools.repoman Repository management tool
Command - xdc.tools.repoman.sg Interactive repository management tool


Utility commands

Finally, the commands above use a few "utility" commands that are useful in their own right. These last tools are most useful within makefiles or shell scripts.

Command - xdcdir eXpanDed C print package name or repository
Command - xdclpf eXpanDed C package file list command
Command - xdcpkg eXpanDed C package list command
[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved


Views
Personal tools
package reference