Configuration Demonstration

Basic Configuration Screen

This page is used for basic system configuration. To update the system configuration, enter the updated information in the gray sections below and press the "Submit Configuration" button at the bottom of the form.

Note this page contains a hidden 32 bit session id that prevents accidental (or intentional) reconfiguration by a stale copy of this HTML form.
Current Status:
This section displays the hardwares's current configuration status.
Hostname: 0123456789012345
Domain: 01234567890123456789012345678901
Addres Type: 0123456789
IP Address: 012345678901234
Subnet Mask: 012345678901234
Default Gateway: 012345678901234
DNS Server: 012345678901234

Hostname:
The hostname is used to identify your hardware on the local network.
Hostname:

IP Configuration:
Various IP addressed are used by your hardware to communicate with the Internet. These addresses can be set manually, or obtained automatically from services like DHCP or PPPOE (this demo supports only DHCP).
Select how your hardware should obtain its IP address information:
Auto: Use DHCP to obtain the IP address configuration automatically
Fixed: Assign the following IP address configuration to the hardware:
Domain Name:
IP Address:
IP Subnet Mask:
Default Gateway:
DNS Server:

Submit Configuration:
In order to apply any changes made to this form, press the "submit configuration" button below. Upon successful submission, the changes will take effect immediately. Press the "cancel" button to return to the main page.