206 extern int SNTP_start(uint32_t (*
get)(
void),
void (*set)(uint32_t newtime),
231 extern void SNTP_setservers(
struct sockaddr *servers,
unsigned int numservers);
int SNTP_start(uint32_t(*get)(void), void(*set)(uint32_t newtime), size_t stacksize)
Initialize and start the SNTP client Task.
void SNTP_stop(void)
Stops the SNTP client Task and frees resources used by the module.
void SNTP_setservers(struct sockaddr *servers, unsigned int numservers)
Initializes or updates the list of NTP servers to communicate with.