Introduction, Documentation, What's New, Compatibility Information, Validation Info, Known Issues, Version Information, Technical Support.
The Local Power Manager release consists of the following packages:
The following documentation is available:
Release notes from previous releases are also available in the relnotes archive directory.
ID | Headline |
ID | Headline |
SDOCM00077131 | Update to Linux 2.6.37 kernel |
ID | Headline |
ID | Headline |
SDOCM00069200 | Remove 'OPT' usage for DSP Link 1.65 compatibility |
ID | Headline |
ID | Headline |
SDOCM00060217 | Provide a GPL-free release of LPM for non-Linux users |
ID | Headline |
SDOCM00046148 | Invalid target isa check in config.xdt |
SDOCM00056022 | Make lpm_driver.c into a template |
SDOCM00056027 | Install of ocvc driver fails |
SDOCM00056217 | Use standard targets in linux driver makefiles |
SDOCM00058043 | Configuration error in config.xdt |
ID | Headline |
SDOCM00045996 | Remove the test build release, add build script to default release |
SDOCM00045997 | Remove dependecy on ti.bios.power.build package |
SDOCM00056830 | Add warning in lpm driver if ocvc is not registered |
SDOCM00058209 | Add check to ensure IVA DPLL is enabled |
Compatibility keys are intentionally independent of marketing product numbers and are intended to:
Compatibility keys are composed of 3 comma-delimited numbers - M,S,R - where:
This release was built and validated against using the following software components:
This release was validated using the following hardware platforms. Note that other devices and configurations supported in LPM 1.24.02 should also be supported. Device/OS support was not removed, although validation of this release was limited.
None
See the Codec Engine Known Issues wiki article for issues found after these release notes were compiled.
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, for example local_power_manager_1_24.
Subsequent releases of patch upgrades will be identified by the patch number, for example LPM 1.24.01 with directory local_power_manager_1_24_01. Typically, these patches only include critical bug fixes.
For technical support, contact softwaresupport@ti.com
Check the following web site for updates: https://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/lpm/index.html
Last updated: December 9, 2011