The cmem user interface library wraps file system calls to an associated kernel module (cmemk.ko), which needs to be loaded in order for calls to this library to succeed.
The following is an example of installing the cmem kernel module:
/sbin/insmod cmemk.ko pools=4x30000,2x500000 phys_start=0x0 phys_end=0x3000000
This particular command creates 2 pools. The first pool is created with 4 buffers of size 30000 bytes and the second pool is created with 2 buffers of size 500000 bytes. The CMEM pool buffers start at 0x0 and end at 0x2FFFFFF (max).
There is also support for a 2nd contiguous memory block to be specified, with all the same features supported for the 2nd block as with the 1st. This 2nd block is specified with *_1 parameters. The following example expands upon the first example above:
/sbin/insmod cmemk.ko pools=4x30000,2x500000 phys_start=0x0 phys_end=0x3000000 pools_1=4x65536 phys_start_1=0x80000000 phys_end_1=0x80010000
This particular command, in addition to the pools explained above, creates 1 pool (with 4 buffers of size 64KB) in a 2nd memory block which starts at 0x80000000 and ends at 0x8000FFFF (specified as "end + 1" on the insmod command).
In order to access this 2nd memory block, new APIs have been added to CMEM which allow specification of the block ID.
Pool buffers are aligned on a module-dependent boundary, and their sizes are rounded up to this same boundary. This applies to each buffer within a pool. The total space used by an individual pool will therefore be greater than (or equal to) the exact amount requested in the installation of the module.
The poolid used in the driver calls would be 0 for the first pool and 1 for the second pool.
Pool allocations can be requested explicitly by pool number, or more generally by just a size. For size-based allocations, the pool which best fits the requested size is automatically chosen. Some CMEM APIs (newer ones) accept a blockid as a parameter, in order to specify which of the multiple blocks to operate on. For 'legacy' APIs (ones that existed before the support for multiple blocks) where a blockid is still needed, block 0 is assumed.
There is also support for a general purpose heap. In addition to the 2 pools described above, a general purpose heap block is created from which allocations of any size can be requested. Internally, allocation sizes are rounded up to a module-dependent boundary and allocation addresses are aligned either to this same boundary or to the requested alignment (whichever is greater).
The size of the heap block is the amount of CMEM memory remaining after all pool allocations. If more heap space is needed than is available after pool allocations, you must reduce the amount of CMEM memory granted to the pools.
Buffer allocation is tracked at the file descriptor level by way of a 'registration' list. The initial allocator of a buffer (the process that calls CMEM_alloc()) is automatically added to the registration list, and further processes can become registered for the same buffer by way of the CMEM_registerAlloc() API (and unregister with the CMEM_unregister() API). This registration list for each buffer allows for buffer ownership tracking and cleanup on a per-file-descriptor basis, so that when a process exits or dies without having explicitly freed/unregistered its buffers, they get automatically unregistered (and freed when no more registered file descriptors exist). Only when the last registered file descriptor frees a buffer (either explictily, or by auto-cleanup) does a buffer actually get freed back to the kernel module.
Since the CMEM interface library doesn't use the GT tracing facility, there is one configuration option available for the CMEM module to control whether the debug or release interface library is used for building the application. This config parameter is named 'debug' and is of type bool, and the default value is 'false'.
The following line is an example of enabling usage of the debug interface library: var cmem = xdc.useModule('ti.sdo.linuxutils.cmem.CMEM'); cmem.debug = true; This will enable "CMEM Debug" statements to be printed to stdout.
Go to the source code of this file.
Data Structures | |
struct | CMEM_AllocParams |
Parameters for CMEM_alloc(), CMEM_alloc2(), CMEM_allocPool(), CMEM_allocPool2(), CMEM_free(). More... | |
struct | CMEM_BlockAttrs |
Defines | |
#define | CMEM_VERSION 0x02300000U |
#define | CMEM_WB 0x0100 |
#define | CMEM_INV 0x0200 |
#define | CMEM_HEAP 0x0400 |
#define | CMEM_POOL 0x0000 |
#define | CMEM_CACHED 0x0800 |
#define | CMEM_NONCACHED 0x0000 |
#define | CMEM_PHYS 0x1000 |
#define | CMEM_IOCALLOC 1 |
#define | CMEM_IOCALLOCHEAP 2 |
#define | CMEM_IOCFREE 3 |
#define | CMEM_IOCGETPHYS 4 |
#define | CMEM_IOCGETSIZE 5 |
#define | CMEM_IOCGETPOOL 6 |
#define | CMEM_IOCCACHE 7 |
#define | CMEM_IOCGETVERSION 8 |
#define | CMEM_IOCGETBLOCK 9 |
#define | CMEM_IOCREGUSER 10 |
#define | CMEM_IOCCACHEWBINV CMEM_IOCCACHE | CMEM_WB | CMEM_INV |
#define | CMEM_IOCCACHEWB CMEM_IOCCACHE | CMEM_WB |
#define | CMEM_IOCCACHEINV CMEM_IOCCACHE | CMEM_INV |
#define | CMEM_IOCALLOCCACHED CMEM_IOCALLOC | CMEM_CACHED |
#define | CMEM_IOCALLOCHEAPCACHED CMEM_IOCALLOCHEAP | CMEM_CACHED |
#define | CMEM_IOCFREEHEAP CMEM_IOCFREE | CMEM_HEAP |
#define | CMEM_IOCFREEPHYS CMEM_IOCFREE | CMEM_PHYS |
#define | CMEM_IOCFREEHEAPPHYS CMEM_IOCFREE | CMEM_HEAP | CMEM_PHYS |
#define | CMEM_IOCCMDMASK 0x000000ff |
Functions | |
int | CMEM_init (void) |
Initialize the CMEM module. Must be called before other API calls. | |
int | CMEM_getPool (size_t size) |
Find the pool that best fits a given buffer size and has a buffer available. | |
int | CMEM_getPool2 (int blockid, size_t size) |
Find the pool in memory block blockid that best fits a given buffer size and has a buffer available. | |
void * | CMEM_allocPool (int poolid, CMEM_AllocParams *params) |
Allocate memory from a specified pool. | |
void * | CMEM_allocPool2 (int blockid, int poolid, CMEM_AllocParams *params) |
Allocate memory from a specified pool in a specified memory block. | |
void * | CMEM_alloc (size_t size, CMEM_AllocParams *params) |
Allocate memory of a specified size. | |
void * | CMEM_alloc2 (int blockid, size_t size, CMEM_AllocParams *params) |
Allocate memory of a specified size from a specified memory block. | |
void * | CMEM_registerAlloc (unsigned long physp) |
Register shared usage of an already-allocated buffer. | |
int | CMEM_free (void *ptr, CMEM_AllocParams *params) |
Free a buffer previously allocated with CMEM_alloc()/CMEM_allocPool(). | |
int | CMEM_unregister (void *ptr, CMEM_AllocParams *params) |
Unregister use of a buffer previously registered with CMEM_registerAlloc(). | |
unsigned long | CMEM_getPhys (void *ptr) |
Get the physical address of a contiguous buffer. | |
int | CMEM_cacheWb (void *ptr, size_t size) |
Do a cache writeback of the block pointed to by ptr/ | |
int | CMEM_cacheInv (void *ptr, size_t size) |
Do a cache invalidate of the block pointed to by ptr/ | |
int | CMEM_cacheWbInv (void *ptr, size_t size) |
Do a cache writeback/invalidate of the block pointed to by ptr/ | |
int | CMEM_getVersion (void) |
Retrieve version from CMEM driver. | |
int | CMEM_getBlock (unsigned long *pphys_base, size_t *psize) |
Retrieve memory block bounds from CMEM driver. | |
int | CMEM_getBlockAttrs (int blockid, CMEM_BlockAttrs *pattrs) |
Retrieve extended memory block attributes from CMEM driver. | |
int | CMEM_exit (void) |
Finalize the CMEM module. | |
Variables | |
CMEM_AllocParams | CMEM_DEFAULTPARAMS |