Introduction, Documentation, What's New, Upgrade Info, Compatibility Information, Validation Info, Known Issues, Device Support, Examples, Version Information, Technical Support.
The IPC Utils are a collection of
Primary packages in this IPC Utils release are briefly described here. (There are others, see the Configuration Reference Guide documentation for a complete package list.)
The IPC Utils are provided as non-rebuildable libraries. Source is provided for debugging and educational value, but is not intended to be modified. Modified sources will not be supported.
Some distributions of this product include an "ipctools" directory containing some dependent products for convenience. Products included in this release are:
The following documentation is available:
In addition, users are encouraged to monitor (and contribute to!) the TI Embedded Processors Wiki.
The following significant changes have been made since 1.00
The IPC Utils packages are available in the "packages/" subdirectory of the product. If you have a previous release of this product, you can install this release next to it, and modify your application and/or server builds to use this newer release.
The details provided below describe each package's compatibility with the previous release ().
Note, the Configuration Reference Guide contains further details about each package.
Package | ipcutils_1_00_00_03 |
---|
The following packages are being introduced in this release, and therefore have no compatibility with previous releases.
Package | Compatibility key |
---|---|
ti.sdo.opencl | 1, 0, 0 |
ti.sdo.opencl.platforms.c6a8149 | 1, 0, 0 |
ti.sdo.rcm | 2, 0, 0 |
ti.sdo.tiler.remote | 1, 0, 0 |
If migrating from a release prior to <>, consult previous releases available in the relnotes_archive directory.
Compatibility keys are intentionally independent of Marketing product numbers and are intended to:
Compatibility keys are composed of 3 comma-delimited numbers - M,S,R - where:
This release supports the following devices:
Support for TI814X with QNX on ARM in this release, is limited.
This release was built and validated against using the following software components. Please use the versions below or any other that are compatible with the below:
IPC Utils examples and instructions are located in the "examples" directory.
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. ipcutils_1_00_00_03.
Subsequent releases of patch upgrades will be identified by the patch number, ex. IPC Utils 1.00.01.XX with directory IPC_Utils_1_00_01_XX. Typically, these patches only include critical bug fixes.
Questions/issues regarding this release may be posted at the E2E forum at https://e2e.ti.com/support/embedded/default.aspx
Check the following web site for updates: https://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/ipcutils/index.html
Last updated: August 10, 2012