ipc (InterProcessor Communications) This tree contains the IPC libraries, examples and regression tests BUILD o To build libraries: from top-level of tree type: MK .ipc (This will build all IPC libraries) MK .ipc,em3 (This will build all IPC libraries for the M3 target) o To build tests # edit src/ti/sdo/ipc/build/testPlatforms.xs and uncomment the devices that will be tested in regressionDevices MK .tests,em3 (this will build libraries/platforms if not already built, and build all regression tests for the target/device) o To build IPC examples MK .ipc (First build the IPC libraries) MK .interfaces (Generate .xdcenv.mak files in the example directories) cd src/ti/sdo/ipc/examples/multicore/evmTI81XX (descend into example dir) mk (Build the IPC multicore example) RELEASE o from Linux workstation: from $TREES/ipc/ipc.git: /* Ensure that you're on the master branch */ git checkout master /* * Grab contributions by user1 and user2 to ipc-g01 (assuming * that ipc-g00 is the latest current release) */ ggentree /db/path/user1/ipc/ipc-g01_g0123456 /db/path/user2/ipc/ipc-g01_g0987654 /* Ensure that you're on the master branch */ git checkout master /* * Merge user branches into master branch. Resolve conflicts if * necessary */ git merge ipc-g01_g0123456 git merge ipc-g01_g0987654 /* * Build tree */ MK .clean .all-files >& Make.log & /* * use "tail -f Make.log" to monitor build progress * Make sure Make.log is satisfactory * Update README */ /* Release the git tree */ greltree =========================================================================== For a changelog, navigate to $TREES/ipc/ipc.git and type # git log Or navigate to the gitweb at: http://gitweb.sanb.design.ti.com/apache/cgi-bin/gitweb.cgi?p=ipc.git/.git;a=shortlog