Data Structures

ires_common.h File Reference


Detailed Description

IRES Resource Protocol Definitions - IRES Resource.

#include "ialg.h"
Include dependency graph for ires_common.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  IRES_ProtocolRevision
 Protocol revision type. Used to ensure the given 'protocol' revision can be validated. More...
struct  IRES_ProtocolArgs
 Abstract Protocol Arguments structure definition. Actual arguments passed by the algorithm to request a resource from a specific IRES Protocol will extend and supply the concrete definitions. More...
struct  IRES_ResourceDescriptor
 Descriptor to Logical Resource. More...
struct  IRES_Properties
 Abstract Resource Properties structure/pointer definition. Actual resource protocol will supply the concrete property definitions. The list of attributes for the actual resource will expose the relevant features that needs to be known to a client to use the resource, such as: resource register base addresses and offsets, critical register and memory region addresses, ... More...
struct  IRES_Obj
 IRES_Obj holds the private state associated with each logical resource. More...

enum  IRES_Status {
  IRES_OK = 0,
  IRES_EALG = 1,
  IRES_EEXISTS = 2,
  IRES_EFAIL = 3,
  IRES_EINIT = 4,
  IRES_ENOINIT = 5,
  IRES_ENOMEM = 6,
  IRES_ENORESOURCE = 7,
  IRES_ENOTFOUND = 8
}
 

IRES_Status defines the standard error and success codes returned by IRES APIs.

More...
enum  IRES_RequestMode {
  IRES_SCRATCH,
  IRES_PERSISTENT,
  IRES_LATEACQUIRE
}
 

Mode in which resources can be requested.

More...
typedef enum IRES_Status IRES_Status
 IRES_Status defines the standard error and success codes returned by IRES APIs.
typedef struct
IRES_ProtocolRevision 
IRES_ProtocolRevision
 Protocol revision type. Used to ensure the given 'protocol' revision can be validated.
typedef enum IRES_RequestMode IRES_RequestMode
 Mode in which resources can be requested.
typedef struct IRES_ProtocolArgs IRES_ProtocolArgs
 Abstract Protocol Arguments structure definition. Actual arguments passed by the algorithm to request a resource from a specific IRES Protocol will extend and supply the concrete definitions.
typedef struct
IRES_ResourceDescriptor 
IRES_ResourceDescriptor
 Descriptor to Logical Resource.
typedef struct IRES_Properties IRES_Properties
 Abstract Resource Properties structure/pointer definition. Actual resource protocol will supply the concrete property definitions. The list of attributes for the actual resource will expose the relevant features that needs to be known to a client to use the resource, such as: resource register base addresses and offsets, critical register and memory region addresses, ...
typedef struct IRES_Obj IRES_Obj
 IRES_Obj holds the private state associated with each logical resource.
typedef struct IRES_ObjIRES_Handle
 Handle to "logical" resource.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2013, Texas Instruments Incorporated