Data Structures

iresman_protocol.h File Reference


Detailed Description

IRES Resource Protocol Definitions (C64P) - IRES Resource specific protocol interface to construct logical handles. This interface is exposed only to IRESMAN.

#include <ti/xdais/ires_common.h>
Include dependency graph for iresman_protocol.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  IRESMAN_ConstructArgs
 Abstract Protocol Construct Arguments structure/pointer definition. Arguments passed by the Resource manager to request a resource from a specific IRES Protocol will extend and supply the concrete definition. More...
struct  IRESMAN_ConstructFxns
 These functions are used to determine memory requirements for and initialize the IRES protocol's environment that will be allocated by the resource manager. More...

Typedefs

typedef struct
IRESMAN_ConstructArgs 
IRESMAN_ConstructArgs
 Abstract Protocol Construct Arguments structure/pointer definition. Arguments passed by the Resource manager to request a resource from a specific IRES Protocol will extend and supply the concrete definition.
typedef struct
IRESMAN_ConstructFxns 
IRESMAN_ConstructFxns
 These functions are used to determine memory requirements for and initialize the IRES protocol's environment that will be allocated by the resource manager.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated