Legend
Package Name | The name of the application or files |
Version | Version of the application or files |
License | Name of the license or licenses that apply to the Package. |
Location | The directory name and path on the media (or in an archive) where the Package is located. |
Delivered As |
This field will either be "Source", "Binary" or "Source and Binary" and is the form the content of the Package is delivered in. If the Package is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in "Limited Source" or "Limited Source and Binary" then only portions of the Source for the application are provided. |
Modified | This field will either be "Yes" or "No". A "Yes" means TI has made changes to the package. A "No" means TI has not made any changes. |
Obtained from[1] |
This field specifies where TI obtained the Package from. It may be a URL to an Open Source site, a 3rd party company name or TI. If this field contains a link to an Open Source package, the date it was downloaded is also recorded. |
Package Name | Version | License | Delivered As | Modified | Location | Obtained From |
---|---|---|---|---|---|---|
Framework Components | N/A | BSD | Source and Binary | No | framework_components_<version>/packages (all subdirectories below this are BSD licensed except for exceptions noted elsewhere in this manifest) |
TI |
[1] Any links appearing on this manifest were verified at the time it was created. TI makes no guarantee that they will remain active in the future.