xdas.h File Reference


Detailed Description

This header defines all types and constants used in the XDAS interfaces.

Remarks:
The types are mapped to the types defined in std.h.
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Defines

#define XDAS_TRUE   1
#define XDAS_FALSE   0

Typedefs

typedef Void XDAS_Void
typedef Uint8 XDAS_Bool
typedef Int8 XDAS_Int8
typedef Uint8 XDAS_UInt8
typedef Int16 XDAS_Int16
typedef Uint16 XDAS_UInt16
typedef Int32 XDAS_Int32
typedef Uint32 XDAS_UInt32

Copyright 2009, Texas Instruments Incorporated