Data Structures | Defines | Typedefs | Enumerations | Functions | Variables

packages/ti/sdo/ce/osal/Memory.h File Reference


Detailed Description

The Codec Engine OSAL Memory interface. Provides the user an OS-independent Memory abstraction.

Go to the source code of this file.

Data Structures

struct  ti_sdo_ce_osal_Memory_AllocParams
 Parameters for ti_sdo_ce_osal_Memory_alloc() & ti_sdo_ce_osal_Memory_free() More...

Defines

#define ti_sdo_ce_osal_Memory_DEFAULTALIGNMENT   ((UInt)(-1))
 Default Alignment.
#define Memory_MODNAME   "ti.sdo.ce.osal.Memory"
 Name to pass to Diags_setMask() to enable logging for Memory functions. For example, Diags_setMask(Memory_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect.
#define ti_sdo_ce_osal_Memory_GTNAME   "OM"
 GT name containing the trace mask for this module.
#define ti_sdo_ce_osal_Memory_CACHED   0x00000000
 Cached allocation.
#define ti_sdo_ce_osal_Memory_NONCACHED   0x00000001
 Non-cached allocation.
#define ti_sdo_ce_osal_Memory_CACHEDMASK   0x00000001
 Mask to isolate cache flag.

Typedefs

typedef struct
ti_sdo_ce_osal_Memory_AllocParams 
ti_sdo_ce_osal_Memory_AllocParams
 Parameters for ti_sdo_ce_osal_Memory_alloc() & ti_sdo_ce_osal_Memory_free()

Enumerations

enum  ti_sdo_ce_osal_Memory_type {
  ti_sdo_ce_osal_Memory_MALLOC = 0,
  ti_sdo_ce_osal_Memory_SEG = 1,
  ti_sdo_ce_osal_Memory_CONTIGPOOL = 2,
  ti_sdo_ce_osal_Memory_CONTIGHEAP = 3
}
 

Enum values for ti_sdo_ce_osal_Memory_AllocParams.type.

More...

Functions

Ptr ti_sdo_ce_osal_Memory_alloc (UInt size, ti_sdo_ce_osal_Memory_AllocParams *params)
 General memory allocation.
Void ti_sdo_ce_osal_Memory_cacheInv (Ptr addr, Int sizeInBytes)
 Invalidate a range of cache.
Void ti_sdo_ce_osal_Memory_cacheWb (Ptr addr, Int sizeInBytes)
 Write back cache.
Void ti_sdo_ce_osal_Memory_cacheWbInv (Ptr addr, Int sizeInBytes)
 Write back and invalidate cache.
Void ti_sdo_ce_osal_Memory_cacheWbInvAll ()
 Write back and invalidate the entire cache. Not supported yet on all OS's.
Ptr ti_sdo_ce_osal_Memory_contigAlloc (UInt size, UInt align)
 Allocate physically contiguous blocks of memory.
Bool ti_sdo_ce_osal_Memory_contigFree (Ptr addr, UInt size)
 Free memory allocated by ti_sdo_ce_osal_Memory_contigAlloc()
Bool ti_sdo_ce_osal_Memory_free (Ptr addr, UInt size, ti_sdo_ce_osal_Memory_AllocParams *params)
 Free memory allocated with ti_sdo_ce_osal_Memory_alloc().
Void ti_sdo_ce_osal_Memory_dumpKnownContigBufsList (Void)
 Dumps the list of all translated/registered bufs.
UInt32 ti_sdo_ce_osal_Memory_getBufferPhysicalAddress (Ptr virtualAddress, Int sizeInBytes, Bool *isContiguous)
 Converts application virtual address to a physical address.
Int ti_sdo_ce_osal_Memory_getHeapId (String name)
 Get the heap heap ID corresponding to a heap name. This number will be between 0 and the value returned by ti_sdo_ce_osal_Memory_getNumHeaps(). The heap Id can be passed to ti_sdo_ce_osal_Memory_redefine() and ti_sdo_ce_osal_Memory_restoreHeap().
Int ti_sdo_ce_osal_Memory_getNumHeaps ()
 Get the number of memory heaps.
Ptr ti_sdo_ce_osal_Memory_getBufferVirtualAddress (UInt32 physicalAddress, Int sizeInBytes)
 Obtains the virtual address of a physically contiguous buffer.
Void ti_sdo_ce_osal_Memory_registerContigBuf (UInt32 virtualAddress, UInt32 sizeInBytes, UInt32 physicalAddress)
 Register a physical buffer allocated without ti_sdo_ce_osal_Memory_contigAlloc()
Void ti_sdo_ce_osal_Memory_unregisterContigBuf (UInt32 virtualAddress, UInt32 sizeInBytes)
 Unregisters a physical buffer allocated without ti_sdo_ce_osal_Memory_contigAlloc().

Variables

ti_sdo_ce_osal_Memory_AllocParams ti_sdo_ce_osal_Memory_DEFAULTPARAMS
 Default parameters for ti_sdo_ce_osal_Memory_alloc() & ti_sdo_ce_osal_Memory_free()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated