Data Structures | Defines | Typedefs | Enumerations | Functions | Variables

Engine.h File Reference


Detailed Description

The Codec Engine Runtime.

Remarks:
Provides the user an interface to open and manipulate an Engine which can instantiate and communicate with XDAIS algorithms that run either on the local CPU or on a "remote" Server.
#include <ti/sdo/ce/Server.h>
#include <ti/sdo/ce/ipc/Comm.h>
#include <ti/xdais/ialg.h>
#include <ti/sdo/ce/node/node.h>
#include <stddef.h>
#include <stdio.h>
Include dependency graph for Engine.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  Engine_Attrs
 Attributes of an Engine. More...
struct  Engine_AlgInfo
 Properties of an Engine algorithm. More...
struct  Engine_AlgInfo2
 Properties of an Engine algorithm. More...
struct  Engine_AlgDesc
 Descriptor for an alg. This object can be passed to Engine_addAlg(), to dynamically add an alg to an engine. More...
struct  Engine_DllAlgDesc
 Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type. More...

Defines

#define Engine_MODNAME   "ti.sdo.ce.Engine"
 Name to pass to Diags_setMask() to enable logging for Engine functions.
#define Engine_EOK   0
#define Engine_EEXIST   1
#define Engine_ENOMEM   2
#define Engine_EDSPLOAD   3
#define Engine_ENOCOMM   4
#define Engine_ENOSERVER   5
#define Engine_ECOMALLOC   6
#define Engine_ERUNTIME   7
#define Engine_ECODECCREATE   8
#define Engine_ECODECSTART   9
#define Engine_EINVAL   10
#define Engine_EBADSERVER   11
#define Engine_ENOTAVAIL   12
#define Engine_EWRONGSTATE   13
#define Engine_EINUSE   14
#define Engine_ENOTFOUND   15
#define Engine_ETIMEOUT   16
#define Engine_GETALGDESCFXN   "GetEngineAlgDesc"
 Name of function that a dynamically loaded codec must supply.

Typedefs

typedef struct Engine_Obj * Engine_Handle
 Opaque handle to an engine.
typedef Int Engine_Error
 Engine error code.
typedef struct Engine_Attrs Engine_Attrs
 Attributes of an Engine.
typedef struct Engine_AlgInfo Engine_AlgInfo
 Properties of an Engine algorithm.
typedef struct Engine_AlgInfo2 Engine_AlgInfo2
 Properties of an Engine algorithm.
typedef enum Engine_CachedMemType Engine_CachedMemType
 Engine Cacheable Memory types.
typedef struct Engine_AlgDesc Engine_AlgDesc
 Descriptor for an alg. This object can be passed to Engine_addAlg(), to dynamically add an alg to an engine.
typedef struct Engine_DllAlgDesc Engine_DllAlgDesc
 Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type.
typedef Int(* Engine_GetAlgDescFxn )(Engine_DllAlgDesc *dllAlgDesc)
 Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc structure.

Enumerations

enum  Engine_CachedMemType {
  Engine_USECACHEDMEM_DEFAULT = -1,
  Engine_USECACHEDMEM_NONCACHED = 0,
  Engine_USECACHEDMEM_CACHED = 1
}
 

Engine Cacheable Memory types.

More...

Functions

Engine_Error Engine_addStubFxns (String fxnsName, IALG_Fxns *fxns)
 Register stub functions through which a remote algorithm can be called.
Engine_Error Engine_add (Engine_Desc *pDesc)
 Add an Engine to the database of engines that can be opened with Engine_open()
Engine_Error Engine_addAlg (String name, Engine_Handle engine, String location, Engine_AlgDesc *pAlgDesc)
 Dynamically add an algorithm to an Engine.
Engine_Error Engine_removeAlg (String name, Engine_Handle engine, String algName)
 Dynamically remove an algorithm that was added to an Engine with Engine_addAlg().
Void Engine_close (Engine_Handle engine)
 Close an Engine.
Void Engine_initAlgDesc (Engine_AlgDesc *pAlgDesc)
 Initialize an Engine_AlgDesc structure with default values.
Void Engine_initAttrs (Engine_Attrs *pAttrs)
 Initialize an Engine_Attrs structure with default values.
Void Engine_initDesc (Engine_Desc *pDesc)
 Initialize an Engine_Desc structure with default values.
Engine_Handle Engine_open (String name, Engine_Attrs *attrs, Engine_Error *ec)
 Open an Engine.
Int Engine_fwriteTrace (Engine_Handle engine, String prefix, FILE *out)
 Write Server's trace buffer to specifed file stream.
Engine_Error Engine_getAlgInfo (String name, Engine_AlgInfo *algInfo, Int index)
 Get details of an algorithm configured into an engine.
Engine_Error Engine_getAlgInfo2 (String name, Engine_Handle engine, Engine_AlgInfo2 *algInfo2, Int index)
 Get details of an algorithm.
Engine_Error Engine_getDesc (String name, Engine_Desc *desc)
 Fill in an Engine_Desc structure with the values of the Engine descriptor for an Engine.
Engine_Error Engine_getLastError (Engine_Handle engine)
 Get error code of the last failed operation.
String Engine_getName (Engine_Handle engine)
 Get the name of an opened engine.
Engine_Error Engine_getNumAlgs (String name, Int *numAlgs)
 Get the number of algorithms configured into an Engine.
Engine_Error Engine_getNumAlgs2 (String name, Engine_Handle engine, Int *numAlgs)
 Get the number of algorithms statically configured into an engine or the total number of algorithms both statically configured and dynamically added through server information when the engine was opened.
Server_Handle Engine_getServer (Engine_Handle engine)
 Get handle to an Engine's Server.
UInt32 Engine_getUsedMem (Engine_Handle engine)
 Get Server's total memory usage.
Engine_Error Engine_remove (String engineName)
 Remove an engine from the list of engines that can be opened.
Engine_Error Engine_setDesc (String name, Engine_Desc *desc)
 Set values for an Engine's descriptor. This function should only be called when the Engine has not yet been opened.
Int Engine_setTrace (Engine_Handle engine, String mask)
 Set Server's trace mask.

Variables

Engine_Attrs Engine_ATTRS
 Default engine attributes.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated