package ti.sysbios.hal |
|
Contains Hardware Abstraction Layer (HAL) modules for the SYS/BIOS kernel
SYS/BIOS provides services for configuration and management of interrupts,
cache, and timers. Unlike other SYS/BIOS services such as threading, these
modules directly program aspects of a device's hardware and are grouped
together in the Hardware Abstraction Layer (HAL) package. These modules
provide services such as enabling and disabling interrupts, plugging of
interrupt vectors, multiplexing of multiple interrupts to a single vector,
and cache invalidation or writeback.
[
more ... ]
package ti.sysbios.hal [2, 0, 0, 0] {
// Cache Manager Proxy
// Null Cache module
// "Global Proxy" for target specific Core implementations
// Null ICore implementation for default BIOS CoreDelegate
// Hardware Interrupt Manager Proxy
// Power Manager Proxy
// Seconds Manager
// A Seconds module that calls user-supplied callbacks
// Seconds module that uses Clock as its' time base
// Timer Manager Proxy
// Null Timer module
}
DETAILS
SYS/BIOS provides services for configuration and management of interrupts,
cache, and timers. Unlike other SYS/BIOS services such as threading, these
modules directly program aspects of a device's hardware and are grouped
together in the Hardware Abstraction Layer (HAL) package. These modules
provide services such as enabling and disabling interrupts, plugging of
interrupt vectors, multiplexing of multiple interrupts to a single vector,
and cache invalidation or writeback.
The HAL APIs fall into two categories:
- Generic APIs that are available across all targets and devices.
- Target/device-specific APIs that are available only for a specific device
or ISA family
The generic APIs are designed to cover the great majority of use cases.
If you are concerned with easy portability between
different TI devices, you should use the generic APIs as much
as possible. However, if the generic APIs cannot enable use of a
device-specific hardware feature that is advantageous to the software
application, you may choose to use the target/device-specific APIs.
The
ti.sysbios.hal.Hwi,
ti.sysbios.hal.Timer, and
ti.sysbios.hal.Cache modules require target/device-specific API
implementations to achieve their functionality. To provide a common set
of APIs for these modules across all supported families/devices, SYS/BIOS
uses the RTSC proxy-delegate module mechanism. That is, each of these
modules serves as a proxy for a corresponding
target/device-specific module implementation.
During the configuration step of the application build, the
modules in the ti.sysbios.hal package locate and bind themselves to
appropriate delegate module implementations based on the current target
and platform specified in your config.bld file. The delegate binding
process is done internally.
For example, if your config.bld file specifies that one of your build
targets is the C64P family, the
ti.sysbios.hal.Hwi knows to
bind itself to the
ti.sysbios.family.c64p.Hwi implementation.
generated on Tue, 18 Aug 2015 20:37:57 GMT