1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31
32 33 34 35
36
37 package ti.sysbios.family.arm.cc32xx;
38
39 import xdc.rov.ViewInfo;
40
41 import xdc.runtime.Types;
42 import xdc.runtime.Error;
43
44 import ti.sysbios.interfaces.ITimer;
45 import ti.sysbios.family.arm.m3.Hwi;
46 import ti.sysbios.knl.Clock;
47
48 /*!
49 * ======== Timer ========
50 * CC3200 Timer Peripheral Manager
51 *
52 * This module manages the 32Khz RTC timer available on CC3200 devices.
53 * The RTC timer uses 2 32-bit words, with the upper 16 bits of the MSW
54 * reserved, resulting in a 48-bit counter.
55 *
56 * The Timer module supports the timer in 'one shot', 'continuous', and
57 * 'dynamic' modes.
58 *
59 * In 'one shot' mode, a timer function will "fire" (run) when the timer
60 * period expires. In 'one shot' mode this will only happen once.
61 *
62 * In 'continuous' mode, the specified timer function will "fire" every
63 * time the period expires, throughout the lifetime of the program.
64 *
65 * In 'dynamic' mode, the specified timer function will "fire" every
66 * time the period expires. But the period of the timer can be changed
67 * dynamically, to correspond to the next tick interrupt needed from the
68 * timer. This mode is used by the SYS/BIOS
69 * {@link ti.sysbios.knl.Clock Clock} module for implementing
70 * dynamic tick suppression, to reduce the number of interrupts from the
71 * timer to the minimum required for currently scheduled timeouts.
72 *
73 * @a(Warning)
74 * Some of the RTC timer registers are accessed from the 32KHz clock
75 * domain, making reads/writes to these registers on the order of 100
76 * microseconds.
77 * If using the RTC timer for the {@link ti.sysbios.knl.Clock Clock}
78 * module's tick source, the interrupt latency will be as high as 200
79 * microseconds, as the {@link ti.sysbios.knl.Clock Clock} ISR makes two
80 * RTC register accesses on the 32KHz clock domain.
81 *
82 * @p(html)
83 * <h3> Calling Context </h3>
84 * <table border="1" cellpadding="3">
85 * <colgroup span="1"></colgroup> <colgroup span="5" align="center">
86 * </colgroup>
87 *
88 * <tr><th> Function </th><th> Hwi </th><th> Swi </th>
89 * <th> Task </th><th> Main </th><th> Startup </th></tr>
90 * <!-- -->
91 * <tr><td> {@link #getNumTimers} </td><td> Y </td>
92 * <td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
93 * <tr><td> {@link #getStatus} </td><td> Y </td>
94 * <td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
95 * <tr><td> {@link #Params_init} </td><td> N </td>
96 * <td> N </td><td> N </td><td> N </td><td> N </td></tr>
97 * <tr><td> {@link #construct} </td><td> N </td>
98 * <td> N </td><td> N </td><td> N </td><td> N </td></tr>
99 * <tr><td> {@link #create} </td><td> N </td>
100 * <td> N </td><td> N </td><td> N </td><td> N </td></tr>
101 * <tr><td> {@link #delete} </td><td> N </td>
102 * <td> N </td><td> N </td><td> N </td><td> N </td></tr>
103 * <tr><td> {@link #destruct} </td><td> N </td>
104 * <td> N </td><td> N </td><td> N </td><td> N </td></tr>
105 * <tr><td> {@link #getCount} </td><td> Y </td>
106 * <td> Y </td><td> Y </td><td> N </td><td> N </td></tr>
107 * <tr><td> {@link #getFreq} </td><td> Y </td>
108 * <td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
109 * <tr><td> {@link #getFunc} </td><td> Y </td>
110 * <td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
111 * <tr><td> {@link #getPeriod} </td><td> Y </td>
112 * <td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
113 * <tr><td> {@link #setFunc} </td><td> Y </td>
114 * <td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
115 * <tr><td> {@link #setPeriod} </td><td> Y </td>
116 * <td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
117 * <tr><td> {@link #setPeriodMicroSecs} </td><td> Y </td>
118 * <td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
119 * <tr><td> {@link #start} </td><td> Y </td>
120 * <td> Y </td><td> Y </td><td> N </td><td> N </td></tr>
121 * <tr><td> {@link #stop} </td><td> Y </td>
122 * <td> Y </td><td> Y </td><td> N </td><td> N </td></tr>
123 * <tr><td colspan="6"> Definitions: <br />
124 * <ul>
125 * <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
126 * <li> <b>Swi</b>: API is callable from a Swi thread. </li>
127 * <li> <b>Task</b>: API is callable from a Task thread. </li>
128 * <li> <b>Main</b>: API is callable during any of these phases: </li>
129 * <ul>
130 * <li> In your module startup after this module is started
131 * (e.g. Timer_Module_startupDone() returns TRUE). </li>
132 * <li> During xdc.runtime.Startup.lastFxns. </li>
133 * <li> During main().</li>
134 * <li> During BIOS.startupFxns.</li>
135 * </ul>
136 * <li> <b>Startup</b>: API is callable during any of these phases:</li>
137 * <ul>
138 * <li> During xdc.runtime.Startup.firstFxns.</li>
139 * <li> In your module startup before this module is started
140 * (e.g. Timer_Module_startupDone() returns FALSE).</li>
141 * </ul>
142 * </ul>
143 * </td></tr>
144 *
145 * </table>
146 * @p
147 */
148 @ModuleStartup
149 @InstanceInitStatic
150
151 module Timer inherits ti.sysbios.interfaces.ITimer
152 {
153 /*! override supportsDynamic - this Timer does support RunMode_DYNAMIC */
154 override metaonly config Bool supportsDynamic = true;
155
156 /*! override defaultMode - use RunMode_PERIODIC by default */
157 override metaonly config Bool defaultDynamic = true;
158
159 /*! Max value of Timer period for PeriodType_COUNTS */
160 const UInt64 MAX_PERIOD = 0xFFFFFFFFFFFF;
161
162
163 /*! @_nodoc */
164 @XmlDtd
165 metaonly struct BasicView {
166 Ptr halTimerHandle;
167 String label;
168 UInt id;
169 String startMode;
170 UInt64 period;
171 String tickFxn[];
172 UArg arg;
173 String hwiHandle;
174 };
175
176 /*! @_nodoc */
177 metaonly struct DeviceView {
178 UInt id;
179 String device;
180 String devAddr;
181 UInt intNum;
182 UInt64 period64;
183 UInt currCount;
184 UInt remainingCount;
185 UInt64 nextThreshold;
186 String state;
187 };
188
189 /*! @_nodoc */
190 metaonly struct ModuleView {
191 String availMask;
192 }
193
194 /*! @_nodoc */
195 @Facet
196 metaonly config ViewInfo.Instance rovViewInfo =
197 ViewInfo.create({
198 viewMap: [
199 [
200 'Basic',
201 {
202 type: ViewInfo.INSTANCE,
203 viewInitFxn: 'viewInitBasic',
204 structName: 'BasicView'
205 }
206 ],
207 [
208 'Device',
209 {
210 type: ViewInfo.INSTANCE,
211 viewInitFxn: 'viewInitDevice',
212 structName: 'DeviceView'
213 }
214 ],
215 [
216 'Module',
217 {
218 type: ViewInfo.MODULE,
219 viewInitFxn: 'viewInitModule',
220 structName: 'ModuleView'
221 }
222 ],
223 ]
224 });
225
226 /*!
227 * ======== E_invalidTimer ========
228 * Error raised when specified timer id is not supported
229 */
230 config Error.Id E_invalidTimer = {
231 msg: "E_invalidTimer: Invalid Timer Id %d"
232 };
233
234 /*!
235 * ======== E_notAvailable ========
236 * Error raised when requested timer is in use
237 */
238 config Error.Id E_notAvailable = {
239 msg: "E_notAvailable: Timer not available %d"
240 };
241
242 /*!
243 * ======== E_cannotSupport ========
244 * Error raised when requested period is not supported
245 */
246 config Error.Id E_cannotSupport = {
247 msg: "E_cannotSupport: Timer cannot support requested period %d"
248 };
249
250 /*!
251 * ======== anyMask ========
252 * Mask of available timers
253 *
254 * This mask is used to identify the timers that can be used when
255 * Timer_create() is called with an id equal to
256 * {@link Timer#ANY Timer_ANY}.
257 */
258 config UInt anyMask = 0x1;
259
260
261 /*!
262 * Period of a tick
263 *
264 * The RTC timer can take up to a 48-bit period.
265 * (The implementation of ITimer supports a period of UInt32
266 * timer counts).
267 */
268 config UInt64 period64 = 0;
269
270 /*!
271 * ======== dynamicStub ========
272 * @_nodoc
273 *
274 * @param(arg) Unused.
275 */
276 Void dynamicStub(UArg arg);
277
278 /*!
279 * ======== periodicStub ========
280 * @_nodoc
281 *
282 * @param(arg) Unused.
283 */
284 Void periodicStub(UArg arg);
285
286 /*!
287 * ======== getCount64 ========
288 * Read the 64-bit timer counter register
289 *
290 * @b(returns) timer counter value
291 */
292 UInt64 getCount64(Object * timer);
293
294 /*!
295 * ======== getAvailMask ========
296 * Returns the availMask.
297 *
298 * @b(returns) Mask of available timers
299 */
300 UInt getAvailMask();
301
302 /*!
303 * ======== setAvailMask ========
304 * Set the availMask to given mask.
305 *
306 * This function validates the given mask to ensure it does not mark
307 * any currently used timer as available. If validation is successful,
308 * the mask overwrites the current availMask and the function returns
309 * TRUE. Otherwise, the mask is discarded and the function returns
310 * FALSE.
311 *
312 * @param(mask) Mask used to write to availMask
313 */
314 Bool setAvailMask(UInt mask);
315
316 /*!
317 * ======== getHandle ========
318 * @_nodoc
319 * Used by TimestampProvider module to get hold of timer handle used by
320 * Clock.
321 *
322 * @param(id) timer Id.
323 */
324 Handle getHandle(UInt id);
325
326 /*!
327 * ======== setNextMaxTick ========
328 * @_nodoc
329 * Instead of using maxSkippable, this timer sets the next
330 * scheduled tick to the last tick just before the next rollover
331 * of the lower 32-bits of the counter.
332 */
333 Void setNextMaxTick(UArg arg);
334
335 instance:
336
337 /*! Hwi Params for Hwi Object. Default is null. */
338 config Hwi.Params *hwiParams = null;
339
340 internal:
341
342 /*!
343 * ======== noStartupNeeded ========
344 * Flag used to prevent misc code from being brought in
345 * un-necessarily
346 */
347 config UInt startupNeeded = false;
348
349 350 351 352
353 Void initDevice(Object *timer);
354
355 356 357 358
359 Int postInit(Object *timer, Error.Block *eb);
360
361 362 363 364
365 Void setThreshold(Object *timer, UInt64 next);
366
367 struct Instance_State {
368 Bool staticInst;
369 Int id;
370 ITimer.StartMode startMode;
371 UArg arg;
372 Hwi.FuncPtr tickFxn;
373 Types.FreqHz frequency;
374 Hwi.Handle hwi;
375 UInt64 period64;
376 UInt64 savedCurrCount;
377 UInt64 nextThreshold;
378 }
379
380 struct Module_State {
381 UInt availMask;
382 Handle handle;
383
384 385 386 387
388 Clock.Object clockObj;
389
390 391 392 393 394
395 UInt32 timeUpper;
396
397 398 399 400 401
402 UInt64 period64;
403 }
404 }