1    /* 
     2     * Copyright (c) 2011, Texas Instruments Incorporated
     3     * All rights reserved.
     4     *
     5     * Redistribution and use in source and binary forms, with or without
     6     * modification, are permitted provided that the following conditions
     7     * are met:
     8     *
     9     * *  Redistributions of source code must retain the above copyright
    10     *    notice, this list of conditions and the following disclaimer.
    11     *
    12     * *  Redistributions in binary form must reproduce the above copyright
    13     *    notice, this list of conditions and the following disclaimer in the
    14     *    documentation and/or other materials provided with the distribution.
    15     *
    16     * *  Neither the name of Texas Instruments Incorporated nor the names of
    17     *    its contributors may be used to endorse or promote products derived
    18     *    from this software without specific prior written permission.
    19     *
    20     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
    21     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
    22     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
    23     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
    24     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
    25     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
    26     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
    27     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
    28     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
    29     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
    30     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    31     * */
    32    /*
    33     *  ======== Hwi.xdc ========
    34     *
    35     */
    36    package ti.sysbios.hal;
    37    
    38    import xdc.runtime.Error;
    39    
    40    /*!
    41     *  ======== Hwi ========
    42     *  Hardware Interrupt Manager Proxy.
    43     *
    44     *  This module provides APIs for managing hardware interrupts. 
    45     *  These APIs are generic across all supported targets and devices 
    46     *  and should provide sufficient functionality for most applications.
    47     *
    48     *  The actual implementations of the Hwi module APIs are
    49     *  provided by the Hwi module delegates.
    50     *  Additional, family-specific Hwi module APIs may also be provided by
    51     *  the Hwi module delegates.
    52     *  See the list of 
    53     *  {@link ./../family/doc-files/delegates.html Delegate Mappings} 
    54     *  to determine which Hwi delegate is used
    55     *  for your target/device.
    56     *
    57     *  You can statically or dynamically assign functions that run when 
    58     *  specific hardware interrupts occur. Dynamic assignment of Hwi 
    59     *  functions to interrupts at run-time is done 
    60     *  using the {@link #create Hwi_create} function.
    61     *
    62     *  Interrupt routines can be written completely in C, completely in 
    63     *  assembly, or in a mix of C and assembly. In order to support interrupt
    64     *  routines
    65     *  written completely in C, an interrupt dispatcher is provided that performs
    66     *  the requisite prolog and epilog for an interrupt routine.
    67     *
    68     *  Some routines are assigned to interrupts by the other SYS/BIOS
    69     *  modules. For example, the 
    70     *  {@line ti.sysbios.knl.Clock} module configures its own timer interrupt
    71     *  handler. 
    72     *
    73     *  @p(html)
    74     *  <h3> Calling Context </h3>
    75     *  <table border="1" cellpadding="3">
    76     *    <colgroup span="1"></colgroup> <colgroup span="5" align="center">
    77     *    </colgroup>
    78     *
    79     *    <tr><th> Function                 </th><th>  Hwi   </th><th>  Swi   </th>
    80     *    <th>  Task  </th><th>  Main  </th><th>  Startup  </th></tr>
    81     *    <!--                                                         -->
    82     *    <tr><td> {@link #clearInterrupt}   </td><td>   Y    </td><td>   Y    </td>
    83     *    <td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
    84     *    <tr><td> {@link #create}           </td><td>   N    </td><td>   N    </td>
    85     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
    86     *    <tr><td> {@link #disable}          </td><td>   Y    </td><td>   Y    </td>
    87     *    <td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
    88     *    <tr><td> {@link #disableInterrupt} </td><td>   Y    </td><td>   Y    </td>
    89     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
    90     *    <tr><td> {@link #enable}           </td><td>   Y    </td><td>   Y    </td>
    91     *    <td>   Y    </td><td>   N    </td><td>   N    </td></tr>
    92     *    <tr><td> {@link #enableInterrupt}  </td><td>   Y    </td><td>   Y    </td>
    93     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
    94     *    <tr><td> {@link #Params_init}      </td><td>   Y    </td><td>   Y    </td>
    95     *    <td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
    96     *    <tr><td> {@link #restore}          </td><td>   Y    </td><td>   Y    </td>
    97     *    <td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
    98     *    <tr><td> {@link #restoreInterrupt} </td><td>   Y    </td><td>   Y    </td>
    99     *    <td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
   100     *    <tr><td> {@link #construct}        </td><td>   N    </td><td>   N    </td>
   101     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   102     *    <tr><td> {@link #delete}           </td><td>   N    </td><td>   N    </td>
   103     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   104     *    <tr><td> {@link #destruct}         </td><td>   N    </td><td>   N    </td>
   105     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   106     *    <tr><td> {@link #getHookContext}   </td><td>   Y    </td><td>   Y    </td>
   107     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   108     *    <tr><td> {@link #setFunc}          </td><td>   Y    </td><td>   Y    </td>
   109     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   110     *    <tr><td> {@link #setHookContext}   </td><td>   Y    </td><td>   Y    </td>
   111     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   112     *    <tr><td colspan="6"> Definitions: <br />
   113     *       <ul>
   114     *         <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
   115     *         <li> <b>Swi</b>: API is callable from a Swi thread. </li>
   116     *         <li> <b>Task</b>: API is callable from a Task thread. </li>
   117     *         <li> <b>Main</b>: API is callable during any of these phases: </li>
   118     *           <ul>
   119     *             <li> In your module startup after this module is started 
   120     *    (e.g. Hwi_Module_startupDone() returns TRUE). </li>
   121     *             <li> During xdc.runtime.Startup.lastFxns. </li>
   122     *             <li> During main().</li>
   123     *             <li> During BIOS.startupFxns.</li>
   124     *           </ul>
   125     *         <li> <b>Startup</b>: API is callable during any of these phases:</li>
   126     *           <ul>
   127     *             <li> During xdc.runtime.Startup.firstFxns.</li>
   128     *             <li> In your module startup before this module is started 
   129     *    (e.g. Hwi_Module_startupDone() returns FALSE).</li>
   130     *           </ul>
   131     *       </ul>
   132     *    </td></tr>
   133     *
   134     *  </table>
   135     *  @p
   136     *
   137     *  @a(Runtime Hwi Creation)
   138     *
   139     *  Below is an example that configures an interrupt at runtime. 
   140     *  Typically such code would be placed in main().
   141     *
   142     *  @p(code)
   143     *  #include <xdc/runtime/Error.h>
   144     *  #include <ti/sysbios/hal/Hwi.h>
   145     *  
   146     *  Hwi_Handle myHwi;
   147     *  
   148     *  Int main(Int argc, char* argv[])
   149     *  {
   150     *      Hwi_Params hwiParams;
   151     *      Error_Block eb;
   152     *   
   153     *      Hwi_Params_init(&hwiParams);
   154     *      Error_init(&eb);
   155     *  
   156     *      // set the argument you want passed to your ISR function
   157     *      hwiParams.arg = 1;        
   158     *   
   159     *      // set the event id of the peripheral assigned to this interrupt
   160     *      hwiParams.eventId = 10;   
   161     *   
   162     *      // don't allow this interrupt to nest itself
   163     *      hwiParams.maskSetting = Hwi_MaskingOption_SELF;
   164     *   
   165     *      // 
   166     *      // Configure interrupt 5 to invoke "myIsr".
   167     *      // Automatically enables interrupt 5 by default
   168     *      // set params.enableInt = FALSE if you want to control
   169     *      // when the interrupt is enabled using Hwi_enableInterrupt()
   170     *      //
   171     *   
   172     *      myHwi = Hwi_create(5, myIsr, &hwiParams, &eb);
   173     *   
   174     *      if (Error_check(&eb)) {
   175     *          // handle the error
   176     *      }
   177     *  }
   178     *   
   179     *  Void myIsr(UArg arg)
   180     *  {
   181     *      // this runs when interrupt #5 goes off
   182     *  }
   183     *  @p
   184     *
   185     *  @a(Hook Functions)
   186     *
   187     *  Sets of hook functions can be specified for the Hwi module
   188     *  using the configuration tool.  Each set contains these hook
   189     *  functions:
   190     *  @p(blist)
   191     *  -Register:  A function called before any statically-created Hwis
   192     *      are initialized at runtime.  The register hook is called at boot time
   193     *      before main() and before interrupts are enabled.
   194     *  -Create:    A function that is called when a Hwi is created.
   195     *      This includes hwis that are created statically and those
   196     *      created dynamically using {@link #create Hwi_create}.
   197     *  -Begin:     A function that is called just prior to running a Hwi.
   198     *  -End:       A function that is called just after a Hwi finishes.
   199     *  -Delete:    A function that is called when a Hwi is deleted at
   200     *      run-time with {@link #delete Hwi_delete}.
   201     *  @p
   202     *
   203     *  Register Function
   204     *
   205     *  The Register function is provided to allow a hook set to store its
   206     *  hookset ID.  This id can be passed to 
   207     *  {@link #setHookContext Hwi_setHookContext} and
   208     *  {@link #getHookContext Hwi_getHookContext} to set or get 
   209     *  hookset-specific context.  The
   210     *  Register function must be specified if the hook implementation
   211     *  needs to use {@link #setHookContext  Hwi_setHookContext} or 
   212     *  {@link #getHookContext  Hwi_getHookContext}.
   213     *  The registerFxn hook function is called during system initialization
   214     *  before interrupts have been enabled.
   215     *
   216     *  @p(code)
   217     *  Void myRegisterFxn(Int id);
   218     *  @p
   219     *
   220     *  Create and Delete Functions
   221     * 
   222     *  The create and delete functions are called whenever a Hwi is created
   223     *  or deleted.  They are called with interrupts enabled (unless called 
   224     *  at boot time or from main()).
   225     *
   226     *  @p(code)
   227     *  Void myCreateFxn(Hwi_Handle hwi, Error_Block *eb);
   228     *  @p
   229     *
   230     *  @p(code)
   231     *  Void myDeleteFxn(Hwi_Handle hwi);
   232     *  @p
   233     *
   234     *  Begin and End Functions
   235     *
   236     *  The beginFxn and endFxn function hooks are called with interrupts
   237     *  globally disabled, therefore any hook processing function will contribute
   238     *  to the overall system interrupt response latency.  In order to minimize
   239     *  this impact, carefully consider the processing time spent in an Hwi
   240     *  beginFxn or endFxn function hook.
   241     *
   242     *  @p(code)
   243     *  Void myBeginFxn(Hwi_Handle hwi);
   244     *  @p
   245     *
   246     *  @p(code)
   247     *  Void myEndFxn(Hwi_Handle hwi);
   248     *  @p
   249     *
   250     *  Hook functions can only be configured statically.
   251     *
   252     */
   253    
   254    @ModuleStartup      /* generate a call to startup function */
   255    
   256    @Template("./Hwi.xdt")
   257    
   258    module Hwi inherits ti.sysbios.interfaces.IHwi 
   259    {
   260        /*! 
   261         *  Error raised when a stack overflow (or corruption) is detected.
   262         *
   263         *  This error is raised by kernel's stack checking function.  This
   264         *  function checks the stacks before every task switch to make sure
   265         *  that reserved word at top of stack has not been modified.
   266         *
   267         *  The stack checking logic is enabled by the {@link #initStackFlag} and
   268         *  {@link #checkStackFlag} configuration parameters.  If both of these
   269         *  flags are set to true, the kernel will validate the stacks.
   270         */
   271        config Error.Id E_stackOverflow  = {
   272            msg: "E_stackOverflow: ISR stack overflow."
   273        };
   274    
   275        /*! 
   276         *  Initialize ISR stack with known value for stack checking at runtime
   277         *
   278         *  This is also useful for inspection of stack in debugger or core
   279         *  dump utilities.
   280         *
   281         *  Default is true.
   282         *  (see {@link #checkStackFlag}).
   283         */
   284        metaonly config Bool initStackFlag = true;
   285    
   286        /*! 
   287         *  Check for Hwi stack overrun during Idle loop.
   288         *  
   289         *  If true, then an idle function is added to the idle loop
   290         *  that checks for a Hwi stack overrun condition and raises
   291         *  an Error if one is detected.
   292         *
   293         *  The check consists of testing the top of stack value against
   294         *  its initial value (see {@link #initStackFlag}). If it is no
   295         *  longer at this value, the assumption is that the ISR stack
   296         *  has been overrun. If the test fails, then the 
   297         *  {@link #E_stackOverflow} error is raised.
   298         *
   299         *  Runtime stack checking is only performed if {@link #initStackFlag} is
   300         *  also true.
   301         *
   302         *  Default is true.
   303         *  (see {@link #initStackFlag}).
   304         *
   305         *  To enable or disable full stack checking, you should set both this
   306         *  flag and the {@link ti.sysbios.knl.Task#checkStackFlag}.
   307         */
   308        metaonly config Bool checkStackFlag = true;
   309    
   310        /*!
   311         *  ======== disable ========
   312         */
   313        @Macro
   314        override UInt disable();
   315    
   316        /*!
   317         *  ======== enable ========
   318         */
   319        @Macro
   320        override UInt enable();
   321    
   322        /*!
   323         *  ======== restore ========
   324         */
   325        @Macro
   326        override Void restore(UInt key);
   327    
   328        /*!
   329         *  ======== viewGetHandle ========
   330         *  @_nodoc
   331         *  Returns the corresponding hal Hwi handle for a delegate Hwi handle
   332         *
   333         *  @b(returns)     hal Hwi handle
   334         */
   335        metaonly Handle viewGetHandle(Ptr pi);
   336    
   337    instance:
   338    
   339        /*!
   340         *  ======== create ========
   341         *  Create a dispatched interrupt.
   342         *
   343         *  To cause a C function to run in response to a particular system
   344         *  interrupt, you create a Hwi object that encapsulates information
   345         *  regarding the interrupt required by the Hwi module.
   346         *  
   347         *  The standard static and dynamic forms of the "create" function are
   348         *  supported by the ti.sysbios.hal.Hwi module. 
   349         *  The following C code configures interrupt 5 with the "myIsr"
   350         *  C function. 
   351         *  
   352         *  @p(code)
   353         *  #include <ti/sysbios/hal/Hwi>
   354         *  
   355         *  Hwi_create(5, myIsr, NULL, NULL);
   356         *  @p
   357         *  
   358         *  The NULL, NULL arguments are used when the default instance 
   359         *  parameters and generic error handling is satisfactory for creating 
   360         *  a Hwi object.  
   361         *  
   362         *  A Hwi dispatcher table entry is created and filled with the 
   363         *  function specified by the fxn parameter and the attributes 
   364         *  specified by the params parameter.
   365         *
   366         *  If params is NULL, the Hwi's dispatcher properties are assigned a 
   367         *  default set of values. Otherwise, the following properties
   368         *  are specified by a structure of type Hwi_Params.
   369         *
   370         *  @p(blist)
   371         *  - The arg element is a generic argument that is passed to the plugged
   372         *  function as its only parameter. The default value is 0.
   373         *  - The enableInt element determines whether the interrupt should be
   374         *  enabled in the IER by create.
   375         *  - The maskSetting element defines the dispatcherAutoNestingSupport 
   376         *  behavior of the interrupt.
   377         *  @p
   378         *  
   379         *  Hwi_create returns a pointer to the created Hwi object.
   380         *
   381         *  @param(intNum)  interrupt number
   382         *  @param(hwiFxn)  pointer to ISR function
   383         */
   384        @DirectCall
   385        override create(Int intNum, FuncPtr hwiFxn);
   386    
   387        /*!
   388         *  ======== getHookContext ========
   389         *  Get hook instance's context for a Hwi.
   390         *
   391         *  The Handle passed to this API must be the handle passed 
   392         *  to any of the Hook functions, not the one returned by
   393         *  {@link #create Hwi_create}.
   394         *
   395         *  @b(returns)     hook instance's context for hwi
   396         */
   397        @DirectCall
   398        override Ptr getHookContext(Int id);
   399    
   400        /*!
   401         *  ======== setHookContext ========
   402         *  Set hook instance's context for a Hwi.
   403         *
   404         *  The Handle passed to this API must be the handle passed 
   405         *  to any of the Hook functions, not the one returned by
   406         *  {@link #create Hwi_create}.
   407         *
   408         *  @param(id)            hook instance's ID
   409         *  @param(hookContext)   value to write to context
   410         */
   411        @DirectCall
   412        override Void setHookContext(Int id, Ptr hookContext);
   413    
   414    internal:   /* not for client use */
   415    
   416        /* keep track of the number of hooks defined */
   417        metaonly config UInt numHooks = 0;
   418    
   419        /*! target/device-specific Hwi implementation. */
   420        proxy HwiProxy inherits ti.sysbios.interfaces.IHwi;
   421    
   422        struct Instance_State {
   423            HwiProxy.Handle pi;
   424        };
   425    }
   426    /*
   427     *  @(#) ti.sysbios.hal; 2, 0, 0, 0,505; 7-20-2011 07:23:31; /db/vtree/library/trees/avala/avala-p45x/src/ xlibrary
   428    
   429     */
   430