1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Memory.xdc ========
    15     */
    16    
    17    /*!
    18     *  ======== Memory ========
    19     *  Static and run-time memory manager
    20     *
    21     *  All memory allocations are executed via `staticPlace()` at the
    22     *  config time or through `Memory_alloc()` (or `Memory_calloc()` or
    23     *  `Memory_valloc()`) at run-time. 
    24     *
    25     *  The actual memory management is performed by modules that
    26     *  implement `{@link xdc.runtime.IHeap}`.  Heap instances are created
    27     *  statically or dynamically via the heap specific create functions and 
    28     *  these instances are then passed as input parameters to the `Memory` 
    29     *  calls with `{@link xdc.runtime.IHeap#Handle}` parameters.
    30     */
    31    module Memory {
    32    
    33        /*!
    34         *  ======== Q_BLOCKING ========
    35         *  Blocking quality
    36         *
    37         *  `{@link xdc.runtime.IHeap}`s with this "quality" may cause the
    38         *  calling thread to block; i.e., suspend execution until another thread
    39         *  leaves the gate.
    40         */
    41        const Int Q_BLOCKING = 1;
    42        
    43        /*!
    44         *  ======== Size ========
    45         *  Type to be used to specify heap buffer sizes
    46         */
    47        typedef UArg Size;
    48    
    49        /*!
    50         *  ======== Stats ========
    51         *  Memory heap statistics
    52         *
    53         *  This structure defines generic statistics that must be supplied
    54         *  by each module that implements the `{@link xdc.runtime.IHeap}`
    55         *  interface.
    56         *
    57         *  @field(totalSize)         total size (in MADUs) of heap.
    58         *  @field(totalFreeSize)     current size (in MADUs) of free memory in 
    59         *                            the heap
    60         *  @field(largestFreeSize)   current largest contiguous free block 
    61         *                            (in MADUs)
    62         */
    63        struct Stats {
    64            Size totalSize;
    65            Size totalFreeSize;
    66            Size largestFreeSize;
    67         }
    68         
    69        /*! @_nodoc */
    70        @XmlDtd
    71        metaonly struct Module_View {
    72            SizeT maxDefaultTypeAlignment;
    73        };
    74    
    75        /*!
    76         *  ======== defaultHeapInstance ========
    77         *  The default heap.
    78         *
    79         *  If no heap is specified in the `Memory` module's methods (i.e.
    80         *  heap == `NULL`) `defaultHeapInstance` is used. If
    81         *  `defaultHeapInstance` is not set (or set to `null`), a
    82         *  `{@link xdc.runtime.HeapStd}` heap instance is created and assigned
    83         *  to this configuration parameter. The size of the heap is determined
    84         *  by the `{@link #defaultHeapSize}` parameter.
    85         *
    86         *  By default, all modules are configured with a `null` instance heap.
    87         *  Instances created by modules with a `null` instance heap are
    88         *  allocated from the `defaultHeapInstance` heap.
    89         */
    90        config IHeap.Handle defaultHeapInstance;
    91    
    92        /*!
    93         *  ======== defaultHeapSize ========
    94         *  The size (in target MADUs) of the `defaultHeapInstance`.
    95         *
    96         *  This parameters is used when the `{@link #defaultHeapInstance}`
    97         *  is not configured. 
    98         */
    99        metaonly config int defaultHeapSize = 0x1000;
   100    
   101        /*!
   102         *  ======== alloc ========
   103         *  Allocate a block of memory from a heap.
   104         *
   105         *  @param(heap)    heap from which the memory is allocated
   106         *
   107         *                  The `heap` is created by a module that implements
   108         *                  the `{@link xdc.runtime.IHeap}` interface.
   109         *                  If `heap` is `NULL`, the 
   110         *                  `{@link #defaultHeapInstance}` is used.
   111         *
   112         *  @param(size)    requested memory block size (in MADUs)
   113         *  @param(align)   alignment (in MADUs) of the block of memory
   114         *
   115         *                  A value of 0 denotes maximum default type alignment.
   116         *
   117         *  @param(eb)      pointer to error block
   118         *
   119         *  @a(returns)     
   120         *  If the allocation was successful, `Memory_alloc()` returns non-`NULL` 
   121         *  pointer to the allocated and uninitialized block; otherwise it returns 
   122         *  `NULL` and the error block will indicate the cause of the error.     
   123         */
   124        Ptr alloc(IHeap.Handle heap, SizeT size, SizeT align, Error.Block *eb);
   125    
   126        /*!
   127         *  ======== calloc ========
   128         *  Allocate a block of memory from a heap and zero out the contents.
   129         *
   130         *  @param(heap)    heap from which the memory is allocated
   131         *
   132         *                  The `heap` is created by a module that implements
   133         *                  the `{@link xdc.runtime.IHeap}` interface.
   134         *                  If `heap` is `NULL`, the 
   135         *                  `{@link #defaultHeapInstance}` is used.
   136         *
   137         *  @param(size)    requested memory block size (in MADUs)
   138         *  @param(align)   alignment (in MADUs) of the block of memory
   139         *
   140         *                  A value of 0 denotes maximum default type alignment.
   141         *
   142         *  @param(eb)      pointer to error block
   143         *
   144         *  @a(returns)
   145         *  If the allocation was successful, `Memory_calloc()` returns non-`NULL` 
   146         *  pointer to the allocated and initialized block; otherwise it returns 
   147         *  `NULL` and the error block will indicate the cause of the error.     
   148         */
   149        Ptr calloc(IHeap.Handle heap, SizeT size, SizeT align, Error.Block *eb);
   150    
   151        /*!
   152         *  ======== free ========
   153         *  Frees the space if the heap manager offers such functionality.
   154         *
   155         *  @param(heap)   heap that the block of memory will be freed back to.
   156         *
   157         *                 The `heap` is created by a module that implements
   158         *                 the `{@link xdc.runtime.IHeap}` interface.
   159         *                 If `heap` is `NULL`, the 
   160         *                 `{@link #defaultHeapInstance}` is used.
   161         *
   162         *  @param(block)  block of memory to free back to the heap
   163         *  @param(size)   size (in MADUs) of the block of memory to free.
   164         *
   165         */
   166        Void free(IHeap.Handle heap, Ptr block, SizeT size);
   167        
   168        /*!
   169         *  ======== getStats ========
   170         *  Obtain statistics from a heap.
   171         *
   172         *  @param(heap)    the heap to get the statistics from
   173         *
   174         *                  The `heap` is created by a module that implements
   175         *                  the `{@link xdc.runtime.IHeap}` interface.
   176         *                  If `heap` is `NULL`, the 
   177         *                  `{@link #defaultHeapInstance}` is used.
   178         *
   179         *  @param(stats)   the output buffer for the returned statistics
   180         */
   181        Void getStats(IHeap.Handle heap, Stats *stats);
   182        
   183        /*!
   184         *  ======== query ========
   185         *  Test for a particular `{@link xdc.runtime.IHeap}` quality.
   186         *
   187         *  There currently is only one quality, namely `{@link #Q_BLOCKING}`.
   188         *
   189         *  @param(heap)    the heap to query
   190         *
   191         *                  The `heap` is created by a module that implements
   192         *                  the `{@link xdc.runtime.IHeap}` interface.  If `heap`
   193         *                  is `NULL`, the `{@link #defaultHeapInstance}`
   194         *                  is queried
   195         *
   196         *  @param(qual)    quality to test
   197         *
   198         *                   For example: `{@link #Q_BLOCKING}`.
   199         *
   200         *  @a(returns)
   201         *  If `heap` has the `qual` quality, this method returns `TRUE`,
   202         *  otherwise it returns `FALSE`.
   203         */
   204        Bool query(IHeap.Handle heap, Int qual);
   205    
   206        /*!
   207         *  ======== getMaxDefaultTypeAlignMeta ========
   208         *  Return the largest alignment required by the target
   209         *
   210         *  This method scans the standard base types supported by the current
   211         *  configuration's target
   212         *  (`{@link xdc.cfg.Program#build Program.build.target}`) and returns
   213         *  the largest alignment required for these types.
   214         *
   215         *  @a(returns)     Returns target-specific alignment in MADUs. 
   216         *
   217         *  @see xdc.bld.ITarget#stdTypes
   218         */
   219        metaonly SizeT getMaxDefaultTypeAlignMeta();
   220        
   221        /*!
   222         *  ======== getMaxDefaultTypeAlign ========
   223         *  Return the largest alignment required by the target
   224         *
   225         *  `getMaxDefaultTypeAlign` returns the largest alignment
   226         *   required for all the standard base types supported by the current
   227         *  configuration's target
   228         *  (`{@link xdc.cfg.Program#build Program.build.target}`) 
   229         *
   230         *  This is the runtime version of the
   231         *  `{@link #getMaxDefaultTypeAlignMeta}` function.      
   232         *
   233         *  @a(returns)     Returns target-specific alignment in MADUs. 
   234         *
   235         *  @see #getMaxDefaultTypeAlignMeta
   236         */
   237        SizeT getMaxDefaultTypeAlign();
   238    
   239        /*!
   240         *  ======== staticPlace ========
   241         *  Statically places buffers.
   242         *
   243         *  This function places the object specified by `obj` into the specified
   244         *  memory section. The section string is a target-specific name that is
   245         *  interpreted by the underlying target tool-chain.  In the case of TI
   246         *  tool-chains, this section can be a subsection (e.g.
   247         *  ".data:someSection").
   248         *
   249         *  The amount of memory that is created for `obj` is dependent on its
   250         *  size and the value of the property `length`. The length (number
   251         *  of elements in an array) is set before the `staticPlace()` is called.
   252         *  For example, setting `obj.length = 5;` before calling `staticPlace()`,
   253         *  will create `5 * sizeof (obj)` MADUs of memory.
   254         *
   255         *  If 0 is specified for the alignment, the allocated buffer is aligned 
   256         *  as determined by the target toolchain. For instance, if `obj` is an
   257         *  array of structs that have only 16-bit integers, the alignment would
   258         *  be on a 16-bit boundary. 
   259         *
   260         *  All non-zero alignments must be a power of 2. Not all targets support
   261         *  directives that allow one to specify alignment. The readonly config
   262         *  parameter
   263         *  `{@link xdc.cfg.Program#build Program.build.target.alignDirectiveSupported}`
   264         *  can be used to determine if the target supports alignment directives. 
   265         *
   266         *  @param(obj)     object to place
   267         *
   268         *      This object always has the `length` property; `obj.length`
   269         *      determines the size of the allocated buffer for `obj`
   270         *
   271         *  @param(align)   the alignment required by `obj`
   272         *
   273         *  @param(section) section name to contain `obj`
   274         *
   275         *      This parameter names the section where `obj` will be placed.  If
   276         *      this parameter is `null`, no explicit placement is done.
   277         *
   278         *  @a(returns)
   279         *  Returns `false` if the alignment request cannot be honored. The `obj` 
   280         *  is still placed regardless of the return code.
   281         */
   282        metaonly Bool staticPlace(any obj, SizeT align, String section);
   283    
   284        /*!
   285         *  ======== valloc ========
   286         *  Allocate a block of memory from a heap and initialize the contents
   287         *  to the value specified.
   288         *
   289         *  @param(heap)    heap from which the memory is allocated
   290         *
   291         *                  The `heap` is created by a module that implements
   292         *                  the `{@link xdc.runtime.IHeap}` interface.
   293         *                  If `heap` is `NULL`, the 
   294         *                  `{@link #defaultHeapInstance}` is used.
   295         *
   296         *  @param(size)    requested memory block size (in MADUs)
   297         *  @param(align)   alignment (in MADUs) of the block of memory
   298         *
   299         *                  A value of 0 denotes maximum default type alignment.
   300         *
   301         *  @param(value)   value to initialize the contents of the block
   302         *  @param(eb)      pointer to error block
   303         *
   304         *  @a(returns)
   305         *  If the allocation was successful, `Memory_valloc()` returns non-`NULL` 
   306         *  pointer to the allocated and initialized block; otherwise it returns 
   307         *  `NULL` and the error block will indicate the cause of the error.     
   308         */
   309        Ptr valloc(IHeap.Handle heap, SizeT size, SizeT align, Char value, 
   310                   Error.Block *eb);
   311    
   312    internal:
   313    
   314        proxy HeapProxy inherits IHeap;
   315    
   316        struct Module_State {
   317            SizeT maxDefaultTypeAlign;
   318        }
   319    }
   320    /*
   321     *  @(#) xdc.runtime; 2, 1, 0,298; 1-12-2011 10:12:29; /db/ztree/library/trees/xdc/xdc-v55x/src/packages/
   322     */
   323