Id |
Component |
Affected
Targets |
Headline |
Additional Details |
Workaround (if applicable) |
SDSCM00043761 |
DVT |
ALL |
The "Display Data Size" parameter of the graph tool seems
limited to 512 |
Setting a value greater than 512 for the "Display Data Size"
distorts the displayed data in the graph display. |
Use a value smaller than 512 |
SDSCM00043762 |
DVT |
ALL |
The format display for Y axis does not show 64-bit values
correctly |
When displaying graphs with 64-bit data, the Y axis shows
invalid data when using Display Format as General, Decimal or
Scientif... |
Use Hexadecimal format instead. Right-click on the graph view
and select Display Properties --> Axes --> Y-axis --> set the
val... |
SDSCM00045320 |
DVT |
ALL |
Show Coverage option in CodeGen Coverage DVT view does not work |
The show Coverage option in CodeGen Coverage DVT view does not
work. The tooltip description says it will highlight coverage
inf... |
|
SDSCM00046280 |
DVT |
ALL |
Image Analyzer does not process 8bit data read in big endian for
RGB correctly |
Ther is a problem with viewing RGB data with 8bit Data Read. See
forum post for details.
http://e2e.ti.com/support/development_... |
Customer was able to workaround this using 32bit Data Read. See
Forum Post for details: http://e2e.ti.com/support/development_t... |
SDSCM00046965 |
DVT |
ALL |
Analysis (DVT) table views are slow to scroll on Linux |
When displaying a large amount of data (> 500 000 records) the
DVT table view can be slow scrolling. This affects features such
... |
There are no known workarounds to this issue. |
SDSCM00043147 |
Emulation |
ALL |
TMS570LS3137 device xml files are missing Access Port
Designation setting |
Device files for TMS570LS3137 is missing Access Port Designation
setting. It should be set to 0x02000100. Without this setting,
... |
In the 'Advanced' tab of the Target Configuration editor, set
the Access Port Designation setting to 0x02000100 (make sure the
C... |
SDSCM00043910 |
Emulation |
ALL |
MSP430 REGISTER view descriptions for SR.SCG0 and SR.SCG1
incorrect in CCSv5.1 |
|
|
SDSCM00044322 |
Emulation |
ALL |
Disassembly shows branch to wrong label |
|
|
SDSCM00044689 |
Emulation |
ALL |
When connecting OMAP5430 using cjtag on first try you have an
Icepick error that occurs |
|
|
SDSCM00044691 |
Emulation |
ALL |
OMAP5430 CJTAG connection. First memory access is performing a
consol error display on console. |
|
|
SDSCM00044821 |
Emulation |
ALL |
CCSv5 is loading emulation DLLs from v3.3 |
CCSv5 is loading emulation DLLs from CCSv3.3. |
Remove any references to CCSv3 from the system path |
SDSCM00044859 |
Emulation |
ALL |
CCS hangs when coming out of Windows 7 'Sleep' mode when using
XDS560 PCI |
CCS hangs when coming out of Windows 7 'Sleep' mode when
connected to a target with the XDS560 PCI. Issue does not seem
to happ... |
|
SDSCM00045482 |
Emulation |
ALL |
CCSv5.1 f2811.gel typo |
|
|
SDSCM00045778 |
Emulation |
ALL |
CP14 register set of Cortex A8 core is not implemented |
The file ccsv5/ccs_base/common/targetdb/Modules/cortexA8_NotVisible.xml
does not have CP14 registers defined. Cortex A7, A9 and... |
N/A. |
SDSCM00038571 |
IDE |
ALL |
Need excluded files filter for the Project Explorer |
In the Project Explorer, which will be the default project view
in CCSv5 instead of the C/C++ Projects View, there is a list of
... |
|
SDSCM00040028 |
IDE |
ALL |
Import wizard should prompt user to change compiler version if
needed |
If I am importing a project that uses a different version of the
compiler than what I have installed the wizard should inform
me... |
|
SDSCM00040045 |
IDE |
ALL |
NullPointerException when renaming project |
Sometimes when renaming an imported project you will get a
dialog complaining of a null pointer exception. |
|
SDSCM00040262 |
IDE |
ALL |
MMU Page table view should be listed on the view menu |
The MMU Page Table View should be listed on the view menu. |
|
SDSCM00040708 |
IDE |
ALL |
For header files outside the project folder double clicking on
compile errors in the Problems view does not jump to error |
When a compilation error occurs in a header file that is outside
the project (e.g. system header file or even user header file
l... |
|
SDSCM00040717 |
IDE |
ALL |
DVT graph button should be disabled if the features are not
available |
In the Debug perspective there is a button to open DVT analysis
views. If you click on this button before launching a debug ses... |
|
SDSCM00041325 |
IDE |
ALL |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension. The default 'Debug' and 'Relea... |
|
SDSCM00041406 |
IDE |
ALL |
US: Project properties is disabled even when there is a project
highlighted |
When you look at the project explorer there is a project
highlighted, but when you to to the project menu, properties
(and many ... |
You need to click again in the project explorer on the project
and then the menu items are enabled. |
SDSCM00042329 |
IDE |
ALL |
Support ISA aware dynamic support for view menu |
The MMU Page Table View should be listed on the view menu. |
|
SDSCM00043134 |
IDE |
ALL |
File shows thumb tack icon indicating file specific options even
when none has been set |
If you right-click on a source file in a project, go into
Properties (or Build Options) and simply click OK (instead of
Cancel),... |
|
SDSCM00043464 |
IDE |
ALL |
Differentiate between Standard Eclipse / CDT help and CCS IDE
help |
Standard Eclipse and CDT help content has screenshots and
instructions that contradict CCS specific documentation. We
should rem... |
|
SDSCM00044371 |
IDE |
ALL |
CCS5.2.0.00069_linux crash shortly after startup when welcome
screen displayed - Resource explorer/browser collides ds' xul |
|
|
SDSCM00044374 |
IDE |
ALL |
CCS Editor: The parallel instruction syntax ('ll') is considered
as a syntax for commenting for assembly files |
The parallel instruction syntax ('ll') is considered as a syntax
for commenting for assembly files with the CCS editor. Hence th... |
|
SDSCM00044793 |
IDE |
ALL |
Any user interface features contributed by a RTSC product (BIOS,
XDAIS, etc) cannot be rolled back to a lower version |
Whenever an existing RTSC-based component is downgraded, the
user interface does not recognize the previous version and fails
to... |
At this moment there is no workaround other than reinstall the
tool and add the RTSC component separately (if the required
versi... |
SDSCM00045301 |
IDE |
ALL |
CCS refresh compiler options GUI for each new compiler patch
release (only currently for major/minor releases) |
CCS currently only refreshes the compiler options GUI for each
major or minor compiler release (X or Y changing in compiler
vers... |
|
SDSCM00045487 |
IDE |
ALL |
Request to add support for creating virtual folders when using
command line project create |
Request to add option for creating virtual folders when using
command line to create projects |
|
SDSCM00045764 |
IDE |
ALL |
Renaming linked files causes invalid duplicate links in another
workspace that is sharing the same file |
When the file is renamed in CCS (hence updating the .project
file), the rename is not getting handled properly by other
workspac... |
Remove the project from the workspaces that exhibit the issue
and re-import it. This will correctly update the Project
Explorer ... |
SDSCM00045853 |
IDE |
ALL |
RTSC Product Discovery should allow you to not be reminded for
specific products |
When you run CCS it brings up a dialog that shows all the RTSC
products that it has discovered that are not currently
configured... |
|
SDSCM00045895 |
IDE |
ALL |
Uninstaller hangs |
When trying to uninstall CCSv5 using the uninstaller (either
Windows Add/Remove programs or running the exe directly), The
unins... |
|
SDSCM00045932 |
IDE |
ALL |
Linux: CCS crash when install GUI app or export app from GUI
Composer |
|
|
SDSCM00045990 |
IDE |
ALL |
Building project using keyboard shortcut does not honor settings
of dependent projects |
If "Build Project" is bound to a keyboard shortcut like F7,
there is a bug where invoking Build Project via keystroke
results in... |
|
SDSCM00046042 |
IDE |
ALL |
CCS should automatically create the CGT built-in macros
according to the project settings |
CCS environment does not properly recognize all the built-in
macros of the compiler tools, thus causing confusion when
browsing ... |
N/A. |
SDSCM00046736 |
IDE |
ALL |
Eclipse won't start when there are unusual characters in the
platform path |
Eclipse and hence CCS will not start if a folder contains #!$
characters in the path. As a workaround CCS installer is
detecting... |
Don't use a User or Install path that includes characters like #
or $. |
SDSCM00046779 |
IDE |
ALL |
Product Autodiscover shut off |
|
|
SDSCM00047039 |
IDE |
ALL |
Project fails to link after creating "Source Folder"s |
Add a folder that is a "Source Folder" under another "Source
Folder" leads to linking errors. |
Create regular folders instead of "Source" folders |
SDSCM00041210 |
Simulation |
ALL |
C6678 Device Functional Simulator is missing a dll file |
The C6678 Device Functional Simulator has been found to be
missing a dll in CCS 5.1 release M6. The error message shown
is: TMS... |
N/A |
SDSCM00041211 |
Simulation |
ALL |
Second Launch of C6678 Device Cycle Approximate Simulator locks
CCS |
In CCS v5.1 M6 it was found that launching a target
configuration a second time locks up CCS. After launching a
debug session ... |
Close CCS before a second launch of the configuration |
SDSCM00043153 |
Simulation |
ALL |
Debug Server Scripting creates EP trace files with duplicate .ept
extensions |
Whenever EP trace on a simulator is enabled, it creates a file
with extension .ept in the same directory as the executable.
How... |
N/A |
SDSCM00043725 |
Simulation |
ALL |
674 simulator does not flush out pipeline when debugger writes
to the PC |
This issue potentially can occur on any C6000 based simulator
and not just C674 simulator. |
Before doing reload, do a reset in order to workaround this
issue. |
SDSCM00043926 |
Simulation |
ALL |
TCI6616 simulator cache tag-RAM viewer displays zero L2 Cache
lines when L2CFG.mode == 0x7 |
|
L2CFG.mode = 0x7 and L2CFG.mode == 0x6 both configure the cache
to 1MB. A workaround is to configure the L!CFG.mode to 0x6. The
... |
SDSCM00044351 |
Simulation |
ALL |
A functionality bug in Nyquist Cycle Approximate Simulator when
SPLOOP buffer is enabled |
|
|
SDSCM00045262 |
Simulation |
ALL |
C674x Simulator crashes CCS |
|
|
SDSCM00044490 |
Trace |
ALL |
Need to load installed libbz2.dll and not the first one found on
the windows path |
|
Remove the other version of the library from the windows path |
SDSCM00045277 |
Trace |
ALL |
ETB is not working on DM365 and DM368 |
The necessary files to make ETB work are not present. |
Instructions and the missing files are available here: https://processors.wiki.ti.com/index.php/DM36x_Trace#ETB |
SDSCM00046966 |
DVT |
ARM Cortex A8 |
Trace Analyzer delta cycle count is one row off on ARM targets |
On all ARM targets the delta cycle shown in Trace Analyzer Log
view is off by 1 row. The delta cycle for the current record is
a... |
To know how many cycles is spent on the current instruction,
look at the delta cycle shown for the previous instruction. |
SDSCM00045827 |
DVT |
ARM Cortex M3 |
Using JTAGRunMode with stairstep example on LM4F232 results in
"trouble reading memory block" error |
RTA does not work reliably when using JTAGRunMode on LM4F232 and
results in "trouble reading memory block" errors. |
|
SDSCM00041464 |
IDE |
ARM Cortex M3 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds th... |
Simply remove the file TMS320F28335.cmd from the project |
SDSCM00045031 |
IDE |
ARM Cortex M3 |
CCS loaders on Concerto should restore clock settings after
loading a program |
|
|
SDSCM00046163 |
IDE |
ARM Cortex M3 |
Helloworld template does not work for Stellaris |
The hello world template in the project wizard is not compatible
with Stellaris devices as they require additional initializatio... |
There is a hello world project as part of StellarisWare that
uses the UART. Note that you will need to use a program like
TeraT... |
SDSCM00046393 |
IDE |
ARM Cortex M3 |
Unable to connect to Stellaris Launchpad on Linux |
Not able to connect to the Stellaris Launchpad on Ubuntu 12.04. |
|
SDSCM00046884 |
IDE |
ARM Cortex M3 |
Breakpoint on a single source line causes the debugger to break
twice before resuming execution |
Breakpoint on a single source line causes the debugger to break
twice at the same line before resuming execution |
|
SDSCM00046465 |
Emulation |
ARM Cortex R4 |
Hardware watchpoint set on a 32-bit variable halts the CPU for
16-bit access width when it should not |
Hardware watchpoint set on a 32-bit variable halts the CPU also
for 16-bit access width |
|
SDSCM00046183 |
Simulation |
ARP32 |
CCS 5.3 crashes when simulator is brought up after a session is
terminated in win7 |
|
|
SDSCM00046754 |
Simulation |
ARP32 |
C6800 Crash on Connect->Termintate->(again) Connect - Duplicate
of SDSCM00046183 |
|
|
SDSCM00044049 |
DVT |
C2800 |
Execution graph cuts off the symbol names |
Execution graph does not display full symbol names, it seems to
be cut off after a certain number of characters. |
|
SDSCM00034673 |
IDE |
C2800 |
CCS v4 allows usage of 1 hardware breakpoint less than CCS 3.3
for BIOS programs |
CCS v4.0x allows user to set only 1 hardware breakpoint when
debugging BIOS programs in Flash |
|
SDSCM00041464 |
IDE |
C2800 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds th... |
Simply remove the file TMS320F28335.cmd from the project |
SDSCM00045031 |
IDE |
C2800 |
CCS loaders on Concerto should restore clock settings after
loading a program |
|
|
SDSCM00046162 |
IDE |
C2800 |
Hide hello world template for C2000 devices that don't have
enough memory |
The helloworld template needs to be hidden for devices that it
will not work on due to limited memory availability. |
|
SDSCM00046908 |
Emulation |
C6416 |
CCS hangs for long moments when debugging BIOS programs with
RTDX enabled |
CCS will hang for long moments when debugging a BIOS program
with RTDX enabled. It is very noticeable when loading programs/symb... |
Disable RTDX |
SDSCM00041366 |
DVT |
C64x Plus Emulator |
Code Coverage coloring does not work for files that do not have
a CCS Project |
Line coloring works if coverage is done for an executable from a
CCS Project. Does not work E.g. if a .out file is directly loa... |
|
SDSCM00046183 |
Simulation |
C66XP |
CCS 5.3 crashes when simulator is brought up after a session is
terminated in win7 |
|
|
SDSCM00046754 |
Simulation |
C66XP |
C6800 Crash on Connect->Termintate->(again) Connect - Duplicate
of SDSCM00046183 |
|
|
SDSCM00045253 |
Simulation |
C6713 |
CCS crashes when enabling multiple L1P and L1D events for code
coverage on a C6713 simulator |
CCS crashes when enabling multiple L1P and L1D events for code
coverage on a C6713 simulator. The crash occurs after the
profile... |
|
SDSCM00045780 |
IDE |
MSP430 |
Full Verification of Code Download to MSP430 BSL fails |
|
|
SDSCM00046166 |
IDE |
MSP430 |
Helloworld template doesn't work for common MSP devices |
On small MSP devices like Gxxxx devices that do not have much
memory it is not possible to build a program using the hello
world... |
Don't use printf on these devices. |
SDSCM00046440 |
IDE |
MSP430 |
Bitfield Structure Debugger Display Issue - Incorrect Index
Shown |
|
|