|
Id |
Component |
Affected
Targets |
Headline |
Additional Details |
Workaround (if applicable) |
|
SDSCM00045588 |
IDE |
ALL |
Memory browser loses symbols when resized |
Variables displayed in the Memory Browser view sometimes
disappear if this view is resized horizontally (which changes
the numbe... |
Experiment resizing the view until all the symbols appear |
|
SDSCM00045541 |
IDE |
ALL |
can not disable line numbering |
|
|
|
SDSCM00045487 |
IDE |
ALL |
Request to add support for creating virtual folders when using
command line project create |
Request to add option for creating virtual folders when using
command line to create projects |
|
|
SDSCM00045440 |
IDE |
ALL |
Rebuilding a project does not rebuild index for updating macro
expansions |
Rebuilding a project does not rebuild index for updating macro
expansions |
Manually do Index->Rebuild before rebuilding the project |
|
SDSCM00045434 |
IDE |
ALL |
Welcome page in resource explorer does not appear after a
restart |
Start CCS with a new workspace. The resource explorer opens
with the welcome page active. Close CCS. Start CCS with the same
wo... |
Click on Welcome on the list on the left hand side. |
|
SDSCM00045415 |
IDE |
ALL |
Load Program: Disable 'OK' button if valid program is not
selected (like it was in 5.1) |
In CCSv5.1, when loading a program via 'Run->Load->Load Program'
and using the option to 'Browse Project', the 'OK' button to di... |
Make sure the actual executable is selected |
|
SDSCM00045399 |
IDE |
ALL |
Pre-build steps are not completely executed before main build
when using parallel build |
Pre build steps do not always complete before the main build
starts when using parallel builds. |
|
|
SDSCM00045348 |
IDE |
ALL |
Command line build does not return an error if an invalid Build
Configuration is specified |
The command-line project build fails to properly return an error
code to the OS if an invalid build configuration is passed as
a... |
N/A |
|
SDSCM00045301 |
IDE |
ALL |
CCS needs to update options cache for each new compiler release |
|
|
|
SDSCM00044793 |
IDE |
ALL |
Any user interface features contributed by a RTSC product (BIOS,
XDAIS, etc) cannot be rolled back to a lower version |
Whenever an existing RTSC-based component is downgraded, the
user interface does not recognize the previous version and fails
to... |
At this moment there is no workaround other than reinstall the
tool and add the RTSC component separately (if the required
versi... |
|
SDSCM00044374 |
IDE |
ALL |
CCS Editor: The parallel instruction syntax ('ll') is considered
as a syntax for commenting for assembly files |
The parallel instruction syntax ('ll') is considered as a syntax
for commenting for assembly files with the CCS editor. Hence th... |
|
|
SDSCM00044371 |
IDE |
ALL |
CCS5.2.0.00069_linux crash shortly after startup when welcome
screen displayed - Resource explorer/browser collides ds' xul |
|
|
|
SDSCM00043464 |
IDE |
ALL |
Differentiate between Standard Eclipse / CDT help and CCS IDE
help |
Standard Eclipse and CDT help content has screenshots and
instructions that contradict CCS specific documentation. We
should rem... |
|
|
SDSCM00042750 |
IDE |
ALL |
Linux installer gets stuck if identical target content
components are already installed |
On Linux if you already have a version of a target contect
package such as IPC that is exactly the same as what CCS is
trying to... |
Uninstall the existing copy of IPC first or tell CCS not to
install IPC. |
|
SDSCM00042329 |
IDE |
ALL |
Support ISA aware dynamic support for view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
SDSCM00042270 |
IDE |
ALL |
Linker - Cmd mapping should be introduced when a user changes
defaults for RTSC projects. |
|
|
|
SDSCM00041417 |
IDE |
ALL |
US: StellarisWare examples are not expanded properly in the
Resource Explorer |
StellarisWare should be fully expanded to show the examples in
Resource Explorer |
|
|
SDSCM00041406 |
IDE |
ALL |
US: Project properties is disabled even when there is a project
highlighted |
When you look at the project explorer there is a project
highlighted, but when you to to the project menu, properties
(and many ... |
You need to click again in the project explorer on the project
and then the menu items are enabled. |
|
SDSCM00041325 |
IDE |
ALL |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension. The default 'Debug' and 'Relea... |
|
|
SDSCM00040737 |
IDE |
ALL |
Installer fails if user folder is linked to another location |
If your user folder or temp folder is symbolically linked to a
different location (called a Junction) you will get an error
when... |
Change your temporary folder to be a different folder that is
not linked. |
|
SDSCM00040717 |
IDE |
ALL |
DVT graph button should be disabled if the features are not
available |
In the Debug perspective there is a button to open DVT analysis
views. If you click on this button before launching a debug ses... |
|
|
SDSCM00040708 |
IDE |
ALL |
For header files outside the project folder double clicking on
compile errors in the Problems view does not jump to error |
When a compilation error occurs in a header file that is outside
the project (e.g. system header file or even user header file
l... |
|
|
SDSCM00040262 |
IDE |
ALL |
MMU Page table view should be listed on the view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
SDSCM00040045 |
IDE |
ALL |
NullPointerException when renaming project |
Sometimes when renaming an imported project you will get a
dialog complaining of a null pointer exception. |
|
|
SDSCM00040028 |
IDE |
ALL |
Import wizard should prompt user to change compiler version if
needed |
If I am importing a project that uses a different version of the
compiler than what I have installed the wizard should inform
me... |
|
|
SDSCM00038571 |
IDE |
ALL |
Need excluded files filter for the Project Explorer |
In the Project Explorer, which will be the default project view
in CCSv5 instead of the C/C++ Projects View, there is a list of
... |
|
|
SDSCM00045657 |
DVT |
ALL |
NullPointerException when closing CCS with debug perspective
open |
|
Close all Image Analyzer views in all perspectives before
closing CCS. |
|
SDSCM00045618 |
DVT |
ALL |
Setting the graph description property does not affect its tab
title |
Any attempts to modify a title to a graph by setting its
Description parameter have no effect. The default title always
remains... |
N/A. |
|
SDSCM00045516 |
DVT |
ALL |
Trace Viewer Preferences Page generates an error |
If you go to Window->Preferences->Code Composer
Studio->Advanced->Trace Viewer an error is generated. |
The Trace Viewer preference does does not contain any relevant
fields. Please use the Trace Analyzer for Trace related
preferenc... |
|
SDSCM00045353 |
DVT |
ALL |
System Analyzer welcome pops up and says my app is not
instrumented when it is |
If I have RTOS analyzer open and I do something that causes it
to lose its connection (like reloading my program, or launching
a... |
|
|
SDSCM00045351 |
DVT |
ALL |
RTOS Analyzer does not survive a reload program |
If I reload my program because I have made a change or want to
refresh the image I lose all functionality and have to manually
c... |
close all the views and open them again to establish the
connection. |
|
SDSCM00045320 |
DVT |
ALL |
Show Coverage option in CodeGen Coverage DVT view does not work |
The show Coverage option in CodeGen Coverage DVT view does not
work. The tooltip description says it will highlight coverage
inf... |
|
|
SDSCM00043762 |
DVT |
ALL |
The format display for Y axis does not show 64-bit values
correctly |
When displaying graphs with 64-bit data, the Y axis shows
invalid data when using Display Format as General, Decimal or
Scientif... |
Use Hexadecimal format instead. Right-click on the graph view
and select Display Properties --> Axes --> Y-axis --> set the
val... |
|
SDSCM00043761 |
DVT |
ALL |
The "Display Data Size" parameter of the graph tool seems
limited to 512 |
Setting a value greater than 512 for the "Display Data Size"
distorts the displayed data in the graph display. |
Use a value smaller than 512 |
|
SDSCM00043256 |
DVT |
ALL |
System Analyzer does not autodetect UIA projects when using JTAG
transport and multiple DSF sessions active |
System Analyzer sometimes does not autodetect that a UIA project
has been loaded when using JTAG as a transport. Once this cond... |
|
|
SDSCM00039329 |
DVT |
ALL |
Profiling help topic is missing screen captures |
When you open the help for profiling it has some red X's where
the help references a screen capture but the screen capture is
mi... |
|
|
SDSCM00038605 |
DVT |
ALL |
STS and CPU Load views should indicate that they are not
supported in stop mode RTA |
Some functionality is not supported when running stop-mode RTA.
Such as the statistics and CPU load views. Ideally we should
d... |
|
|
SDSCM00044859 |
Emulation |
ALL |
CCS hangs when coming out of Windows 7 'Sleep' mode when using
XDS560 PCI |
CCS hangs when coming out of Windows 7 'Sleep' mode when
connected to a target with the XDS560 PCI. Issue does not seem
to happ... |
|
|
SDSCM00044821 |
Emulation |
ALL |
CCSv5 is loading emulation DLLs from v3.3 |
CCSv5 is loading emulation DLLs from CCSv3.3. |
Remove any references to CCSv3 from the system path |
|
SDSCM00045031 |
IDE |
ARM Cortex M3 |
CCS loaders on Concerto should restore clock settings after
loading a program |
|
|
|
SDSCM00043593 |
IDE |
ARM Cortex M3 |
Stellaris driver xmls point to the windows driver on Linux |
Unable to launch debug sessions using Stellaris ICDI on Linux. |
|
|
SDSCM00041464 |
IDE |
ARM Cortex M3 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds th... |
Simply remove the file TMS320F28335.cmd from the project |
|
SDSCM00040875 |
Emulation |
ARM Cortex R4 |
Memory mapping for LIN peripheral register in GEL file needs
updating |
Memory mapping for LIN peripheral register in TMS570 GEL file
needs to be updated to a length of 0x200 instead of 0x100. |
|
|
SDSCM00042185 |
Simulation |
ARM Cortex R4 |
Disassembly view of Cortex R4 Functional Simulator BE32 shows
incorrect instructions due to incorrect endianness |
Disassembly view of Cortex R4 Functional Simulator BE32 shows
incorrect instructions due to incorrect endianness |
|
|
SDSCM00045336 |
IDE |
ARM926 |
Changing compiler version turns on little endian code option |
Changing compiler version turns on little endian code option
even if it was off before. |
|
|
SDSCM00045594 |
IDE |
C2800 |
Cannot program flash for the second device in an hetero
multi-target configuration |
If there are two (or more) targets (boards) in a single target
configuration file, the second target cannot be flashed with the
... |
Flash the device using a different target configuration file
with only the second target specified. |
|
SDSCM00045031 |
IDE |
C2800 |
CCS loaders on Concerto should restore clock settings after
loading a program |
|
|
|
SDSCM00041464 |
IDE |
C2800 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds th... |
Simply remove the file TMS320F28335.cmd from the project |
|
SDSCM00034673 |
IDE |
C2800 |
CCS v4 allows usage of 1 hardware breakpoint less than CCS 3.3
for BIOS programs |
CCS v4.0x allows user to set only 1 hardware breakpoint when
debugging BIOS programs in Flash |
|
|
SDSCM00044049 |
DVT |
C2800 |
Execution graph cuts off the symbol names |
Execution graph does not display full symbol names, it seems to
be cut off after a certain number of characters. |
|
|
SDSCM00038672 |
DVT |
C6416 |
CCSv4.2 RC1 profiler doesn’t correctly report the type of
cycles, cycle.CPU versus cycle.Total |
CCSv4.2 RC1 profiler doesn’t correctly report the type of
cycles, cycle.CPU versus cycle.Total , Simulator used: C6416
device si... |
|
|
SDSCM00041366 |
DVT |
C64x Plus Emulator |
Code Coverage coloring does not work for files that do not have
a CCS Project |
Line coloring works if coverage is done for an executable from a
CCS Project. Does not work E.g. if a .out file is directly loa... |
|
|
SDSCM00044891 |
Simulation |
C64x Plus Simulator |
The IPC Notify example code fails to properly run in the C6472
(Tomahawk) device cycle accurate simulator |
The IPC example code "C6472: Notify (single image for all
cores)" does not finish its proper execution when running from
the six... |
Insert a breakpoint at line 175. |
|
SDSCM00045253 |
Simulation |
C6713 |
CCS crashes when enabling multiple L1P and L1D events for code
coverage on a C6713 simulator |
CCS crashes when enabling multiple L1P and L1D events for code
coverage on a C6713 simulator. The crash occurs after the
profile... |
|
|
SDSCM00044818 |
IDE |
MSP430 |
MSP430 clock control settings |
|
|
|
SDSCM00045724 |
Emulation |
ALL |
CCS disassembles FMRX and FMXR instructions incorrectly on
CortexR4 |
CCS disassembles FMRX instruction as FMXR and FMXR instruction
as FMRX on CortexR4 |
|
|
SDSCM00045576 |
Emulation |
ALL |
Spectrum Digital XDS PRO Trace connection files should only be
installed when installing Spectrum Digital support |
Even though I did not install support for Spectrum Digital
emulators I still get two Spectrum Digital connection files for
the P... |
Just ignore them and don't try to use them. |
|
SDSCM00045552 |
Emulation |
ALL |
Relaunching Debug Session Hangs with XDS100v1 connections |
CCS can hang if you click on the bug button while in a debug
session |
Unplug the usbstick |
|
SDSCM00045482 |
Emulation |
ALL |
CCSv5.1 f2811.gel typo |
|
|
|
SDSCM00044691 |
Emulation |
ALL |
OMAP5430 CJTAG connection. First memory access is performing a
consol error display on console. |
|
|
|
SDSCM00044689 |
Emulation |
ALL |
When connecting OMAP5430 using cjtag on first try you have an
Icepick error that occurs |
|
|
|
SDSCM00044322 |
Emulation |
ALL |
Disassembly shows branch to wrong label |
|
|
|
SDSCM00044274 |
Emulation |
ALL |
Realtime difficult to use with reset and program load |
With C2000 devices it is necessary to disable real-time mode to
perform certain actions like loading a program or resetting the
... |
|
|
SDSCM00043910 |
Emulation |
ALL |
MSP430 REGISTER view descriptions for SR.SCG0 and SR.SCG1
incorrect in CCSv5.1 |
|
|
|
SDSCM00043147 |
Emulation |
ALL |
TMS570LS3137 device xml files are missing Access Port
Designation setting |
Device files for TMS570LS3137 is missing Access Port Designation
setting. It should be set to 0x02000100. Without this setting,
... |
In the 'Advanced' tab of the Target Configuration editor, set
the Access Port Designation setting to 0x02000100 (make sure the
C... |
|
SDSCM00042334 |
Emulation |
ALL |
Need to be able to see CP15 registers |
Developers using ARM cores at a very low-level usually require
viewing CP15 and other registers that are hidden by default in
th... |
All registers can be viewed in the Expressions view of CCSv5.1.
Simply type the name of the register with upper case. For exampl... |
|
SDSCM00045262 |
Simulation |
ALL |
C674x Simulator crashes CCS |
|
|
|
SDSCM00043725 |
Simulation |
ALL |
674 simulator does not flush out pipeline when debugger writes
to the PC |
This issue potentially can occur on any C6000 based simulator
and not just C674 simulator. |
Before doing reload, do a reset in order to workaround this
issue. |
|
SDSCM00041211 |
Simulation |
ALL |
Second Launch of C6678 Device Cycle Approximate Simulator locks
CCS |
In CCS v5.1 M6 it was found that launching a target
configuration a second time locks up CCS. After launching a
debug session ... |
Close CCS before a second launch of the configuration |
|
SDSCM00041210 |
Simulation |
ALL |
C6678 Device Functional Simulator is missing a dll file |
The C6678 Device Functional Simulator has been found to be
missing a dll in CCS 5.1 release M6. The error message shown
is: TMS... |
N/A |
|
SDSCM00044351 |
Simulation |
ALL |
A functionality bug in Nyquist Cycle Approximate Simulator when
SPLOOP buffer is enabled |
|
|
|
SDSCM00043926 |
Simulation |
ALL |
TCI6616 simulator cache tag-RAM viewer displays zero L2 Cache
lines when L2CFG.mode == 0x7 |
|
L2CFG.mode = 0x7 and L2CFG.mode == 0x6 both configure the cache
to 1MB. A workaround is to configure the L!CFG.mode to 0x6. The
... |
|
SDSCM00043153 |
Simulation |
ALL |
Debug Server Scripting creates EP trace files with duplicate .ept
extensions |
Whenever EP trace on a simulator is enabled, it creates a file
with extension .ept in the same directory as the executable.
How... |
N/A |
|
SDSCM00045277 |
Trace |
ALL |
ETB is not working on DM365 and DM368 |
The necessary files to make ETB work are not present. |
Instructions and the missing files are available here: https://processors.wiki.ti.com/index.php/DM36x_Trace#ETB |
|
SDSCM00044490 |
Trace |
ALL |
Need to load installed libbz2.dll and not the first one found on
the windows path |
|
Remove the other version of the library from the windows path |
|
SDSCM00044173 |
Trace |
ALL |
CCS application shuts down when hibernation code running on the
device is terminated |
CCS application shuts down when hibernation code running on the
device is terminated. |
|