|
Id |
Component |
Affected
Targets |
Headline |
Additional Details |
Workaround (if applicable) |
|
SDSCM00038605 |
DVT |
ALL |
STS and CPU Load views should indicate that they are not
supported in stop mode RTA |
Some functionality is not supported when running stop-mode RTA.
Such as the statistics and CPU load views. Ideally we should
d... |
|
|
SDSCM00039329 |
DVT |
ALL |
Profiling help topic is missing screen captures |
When you open the help for profiling it has some red X's where
the help references a screen capture but the screen capture is
mi... |
|
|
SDSCM00043256 |
DVT |
ALL |
System Analyzer does not autodetect UIA projects when using JTAG
transport and multiple DSF sessions active |
System Analyzer sometimes does not autodetect that a UIA project
has been loaded when using JTAG as a transport. Once this cond... |
|
|
SDSCM00043761 |
DVT |
ALL |
The "Display Data Size" parameter of the graph tool seems
limited to 512 |
Setting a value greater than 512 for the "Display Data Size"
distorts the displayed data in the graph display. |
Use a value smaller than 512 |
|
SDSCM00043762 |
DVT |
ALL |
The format display for Y axis does not show 64-bit values
correctly |
When displaying graphs with 64-bit data, the Y axis shows
invalid data when using Display Format as General, Decimal or
Scientif... |
Use Hexadecimal format instead. Right-click on the graph view
and select Display Properties --> Axes --> Y-axis --> set the
val... |
|
SDSCM00039615 |
Emulation |
ALL |
CCS reports incorrect cycles for POPM.A PUSHM.A instructions |
When viewing the clock in CCS it reports an incorrect number of
cycles for POPM.A and PUSHM.A instructions. It reports them as
... |
|
|
SDSCM00041300 |
Emulation |
ALL |
XDS100 conflicts with USB to Serial cables |
It is possible for there to be a conflict between XDS100 and
Serial to USB cables. |
|
|
SDSCM00042138 |
Emulation |
ALL |
Emulation components and libraries should not rely on PATH
environment variable |
Certain emulation components and libraries get confused if an
older version of CCS (3.3 or 3.1) has certain bin directories
set ... |
Remove all references to CCS3.1 or 3.3 from the system path. |
|
SDSCM00042334 |
Emulation |
ALL |
Need to be able to see CP15 registers |
Developers using ARM cores at a very low-level usually require
viewing CP15 and other registers that are hidden by default in
th... |
All registers can be viewed in the Expressions view of CCSv5.1.
Simply type the name of the register with upper case. For exampl... |
|
SDSCM00043147 |
Emulation |
ALL |
TMS570LS3137 device xml files are missing Access Port
Designation setting |
Device files for TMS570LS3137 is missing Access Port Designation
setting. It should be set to 0x02000100. Without this setting,
... |
In the 'Advanced' tab of the Target Configuration editor, set
the Access Port Designation setting to 0x02000100 (make sure the
C... |
|
SDSCM00043783 |
Emulation |
ALL |
IERR register not visible for C64xx devices |
The IERR register doesn't show up in the register view. |
Open the expressions view and enter IERR. |
|
SDSCM00044168 |
Emulation |
ALL |
Crash when connecting to XDS100 |
On some Win7 systems connecting to a BeagleBone will crash CCS. |
|
|
SDSCM00044322 |
Emulation |
ALL |
Disassembly shows branch to wrong label |
|
|
|
SDSCM00038571 |
IDE |
ALL |
Need excluded files filter for the Project Explorer |
In the Project Explorer, which will be the default project view
in CCSv5 instead of the C/C++ Projects View, there is a list of
... |
|
|
SDSCM00040028 |
IDE |
ALL |
Import wizard should prompt user to change compiler version if
needed |
If I am importing a project that uses a different version of the
compiler than what I have installed the wizard should inform
me... |
|
|
SDSCM00040045 |
IDE |
ALL |
NullPointerException when renaming project |
Sometimes when renaming an imported project you will get a
dialog complaining of a null pointer exception. |
|
|
SDSCM00040262 |
IDE |
ALL |
MMU Page table view should be listed on the view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
SDSCM00040708 |
IDE |
ALL |
For header files outside the project folder double clicking on
compile errors in the Problems view does not jump to error |
When a compilation error occurs in a header file that is outside
the project (e.g. system header file or even user header file
l... |
|
|
SDSCM00040717 |
IDE |
ALL |
DVT graph button should be disabled if the features are not
available |
In the Debug perspective there is a button to open DVT analysis
views. If you click on this button before launching a debug ses... |
|
|
SDSCM00040737 |
IDE |
ALL |
Installer fails if user folder is linked to another location |
If your user folder or temp folder is symbolically linked to a
different location (called a Junction) you will get an error
when... |
Change your temporary folder to be a different folder that is
not linked. |
|
SDSCM00041182 |
IDE |
ALL |
Need ability to verify program at any time |
Right now CCS will verify memory as it loads a program. A great
feature would be to allow that same capability to be used indepe... |
|
|
SDSCM00041325 |
IDE |
ALL |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension. The default 'Debug' and 'Relea... |
|
|
SDSCM00041406 |
IDE |
ALL |
US: Project properties is disabled even when there is a project
highlighted |
When you look at the project explorer there is a project
highlighted, but when you to to the project menu, properties
(and many ... |
You need to click again in the project explorer on the project
and then the menu items are enabled. |
|
SDSCM00041417 |
IDE |
ALL |
US: StellarisWare examples are not expanded properly in the
Resource Explorer |
StellarisWare should be fully expanded to show the examples in
Resource Explorer |
|
|
SDSCM00041425 |
IDE |
ALL |
Importing project should shrink the Editor area |
If I import a project from the project menu it does not make the
Project Explorer visible. The resource explorer and grace welc... |
Double click on a tab in the editor area to make it smaller |
|
SDSCM00041649 |
IDE |
ALL |
After installing CCS, starting the setup program again causes
"Program Compatibility Assistant" dialog |
|
|
|
SDSCM00042270 |
IDE |
ALL |
Linker - Cmd mapping should be introduced when a user changes
defaults for RTSC projects. |
|
|
|
SDSCM00042329 |
IDE |
ALL |
Support ISA aware dynamic support for view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
SDSCM00042750 |
IDE |
ALL |
Linux installer gets stuck if identical target content
components are already installed |
On Linux if you already have a version of a target contect
package such as IPC that is exactly the same as what CCS is
trying to... |
Uninstall the existing copy of IPC first or tell CCS not to
install IPC. |
|
SDSCM00043063 |
IDE |
ALL |
Switching stackframe in breadcrumb mode causes 'Run to line' to
disappear in the editor |
|
|
|
SDSCM00043161 |
IDE |
ALL |
Include terminal plugins as part of installation |
Request to include the terminal plug-in in the CCS installation |
Add the terminal plug-in according to the instructions here:
https://processors.wiki.ti.com/index.php/How_to_install_the_terminal... |
|
SDSCM00043384 |
IDE |
ALL |
Installation fails to run on Ubuntu 11.10 64bit |
Installation fails to run on Ubuntu 11.10 Desktop 64bit |
|
|
SDSCM00043435 |
IDE |
ALL |
Active target configuration settings not kept |
When creating a project, if you select a connection type a
target configuration file (ccxml) gets autogenerated. If you
later... |
Manually set the active configuration |
|
SDSCM00043464 |
IDE |
ALL |
Differentiate between Standard Eclipse / CDT help and CCS IDE
help |
Standard Eclipse and CDT help content has screenshots and
instructions that contradict CCS specific documentation. We
should rem... |
|
|
SDSCM00044160 |
IDE |
ALL |
CCS installation into a directory path with a comma fails |
CCS installation will fail if its install path contains a comma. |
Avoid commas in installation paths. |
|
SDSCM00044262 |
IDE |
ALL |
loadti does not work when invoked with the the launch method |
When a loadti script is invoked from within a CCS install in
v5.2, the script will print the loadti help and exit. |
The problem is caused by the new invocation method for DSS
scripts. The new method is required when you want to attach the
eclip... |
|
SDSCM00044278 |
IDE |
ALL |
Install size reported is inflated |
Depending on what device and feature combination you select the
install size that CCS reports may be inflated and the installati... |
|
|
SDSCM00044301 |
IDE |
ALL |
Importing or building project that has a file with custom build
step defined throws NullPointerException |
Importing or building project that has a file with custom build
step defined throws Java NullPointerExceptions. |
|
|
SDSCM00044371 |
IDE |
ALL |
CCS5.2.0.00069_linux crash shortly after startup when welcome
screen displayed - Resource explorer/browser collides ds' xul |
|
|
|
SDSCM00044374 |
IDE |
ALL |
CCS Editor: The parallel instruction syntax ('ll') is considered
as a syntax for commenting for assembly files |
The parallel instruction syntax ('ll') is considered as a syntax
for commenting for assembly files with the CCS editor. Hence th... |
|
|
SDSCM00041210 |
Simulation |
ALL |
C6678 Device Functional Simulator is missing a dll file |
The C6678 Device Functional Simulator has been found to be
missing a dll in CCS 5.1 release M6. The error message shown
is: TMS... |
N/A |
|
SDSCM00041211 |
Simulation |
ALL |
Second Launch of C6678 Device Cycle Approximate Simulator locks
CCS |
In CCS v5.1 M6 it was found that launching a target
configuration a second time locks up CCS. After launching a
debug session ... |
Close CCS before a second launch of the configuration |
|
SDSCM00041861 |
Simulation |
ALL |
Incorrect processor ID in driver xml file causes device to show
up twice in project wizard |
If you have a device file with at C674x core and it has options
for the project wizard it shows up twice in the project wizard. |
Pick either device and it works fine |
|
SDSCM00043153 |
Simulation |
ALL |
Debug Server Scripting creates EP trace files with duplicate .ept
extensions |
Whenever EP trace on a simulator is enabled, it creates a file
with extension .ept in the same directory as the executable.
How... |
N/A |
|
SDSCM00043725 |
Simulation |
ALL |
674 simulator does not flush out pipeline when debugger writes
to the PC |
This issue potentially can occur on any C6000 based simulator
and not just C674 simulator. |
Before doing reload, do a reset in order to workaround this
issue. |
|
SDSCM00043926 |
Simulation |
ALL |
TCI6616 simulator cache tag-RAM viewer displays zero L2 Cache
lines when L2CFG.mode == 0x7 |
|
L2CFG.mode = 0x7 and L2CFG.mode == 0x6 both configure the cache
to 1MB. A workaround is to configure the L!CFG.mode to 0x6. The
... |
|
SDSCM00044351 |
Simulation |
ALL |
A functionality bug in Nyquist Cycle Approximate Simulator when
SPLOOP buffer is enabled |
|
|
|
SDSCM00044173 |
Trace |
ALL |
CCS application shuts down when hibernation code running on the
device is terminated |
CCS application shuts down when hibernation code running on the
device is terminated. |
|
|
SDSCM00044458 |
Trace |
ALL |
CCSv5.2.0: Cannot configure watchdog timer AET job on a C6000
target |
|
|
|
SDSCM00042994 |
IDE |
ARM Cortex A8 |
OMAP5430 : Problem when loading symbol on cortexM4 and CortexA15
CPU0 |
|
|
|
SDSCM00041464 |
IDE |
ARM Cortex M3 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds th... |
Simply remove the file TMS320F28335.cmd from the project |
|
SDSCM00042994 |
IDE |
ARM Cortex M3 |
OMAP5430 : Problem when loading symbol on cortexM4 and CortexA15
CPU0 |
|
|
|
SDSCM00043593 |
IDE |
ARM Cortex M3 |
Stellaris driver xmls point to the windows driver on Linux |
Unable to launch debug sessions using Stellaris ICDI on Linux. |
|
|
SDSCM00040875 |
Emulation |
ARM Cortex R4 |
Memory mapping for LIN peripheral register in GEL file needs
updating |
Memory mapping for LIN peripheral register in TMS570 GEL file
needs to be updated to a length of 0x200 instead of 0x100. |
|
|
SDSCM00044221 |
IDE |
ARM Cortex R4 |
CCS Loader fails to load code to the TMS570 EEPROM memory area |
When trying to load code to the EEPROM memory area of a TMS570
device (TMS570LS2125 and TMS570LS3137 were tested), the loader
fa... |
Use the nowFlash tool instead https://www.ti.com/tool/nowFlash |
|
SDSCM00042185 |
Simulation |
ARM Cortex R4 |
Disassembly view of Cortex R4 Functional Simulator BE32 shows
incorrect instructions due to incorrect endianness |
Disassembly view of Cortex R4 Functional Simulator BE32 shows
incorrect instructions due to incorrect endianness |
|
|
SDSCM00044049 |
DVT |
C2800 |
Execution graph cuts off the symbol names |
Execution graph does not display full symbol names, it seems to
be cut off after a certain number of characters. |
|
|
SDSCM00034673 |
IDE |
C2800 |
CCS v4 allows usage of 1 hardware breakpoint less than CCS 3.3
for BIOS programs |
CCS v4.0x allows user to set only 1 hardware breakpoint when
debugging BIOS programs in Flash |
|
|
SDSCM00041464 |
IDE |
C2800 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds th... |
Simply remove the file TMS320F28335.cmd from the project |
|
SDSCM00042703 |
IDE |
C2800 |
C2000 Device Support Feature needs to be renamed |
When you check for updates in CCS you may see an update called
"C2000 Emulators". This feature name is not clear. The updated
... |
|
|
SDSCM00044274 |
IDE |
C2800 |
Realtime difficult to use with reset and program load |
With C2000 devices it is necessary to disable real-time mode to
perform certain actions like loading a program or resetting the
... |
|
|
SDSCM00044276 |
IDE |
C2800 |
Using GEL to write a float value to a floating point register,
the value cannot be correctly written. |
A number of C28x devices have floating point registers as do
Cortex-M4F and Cortex-R4F devices. In the register view there
is n... |
Use the memory view |
|
SDSCM00038672 |
DVT |
C6416 |
CCSv4.2 RC1 profiler doesn’t correctly report the type of
cycles, cycle.CPU versus cycle.Total |
CCSv4.2 RC1 profiler doesn’t correctly report the type of
cycles, cycle.CPU versus cycle.Total , Simulator used: C6416
device si... |
|
|
SDSCM00041366 |
DVT |
C64x Plus Emulator |
Code Coverage coloring does not work for files that do not have
a CCS Project |
Line coloring works if coverage is done for an executable from a
CCS Project. Does not work E.g. if a .out file is directly loa... |
|
|
SDSCM00042038 |
Emulation |
MSP430 |
MSP 430 Write Register Breakpoint does not work |
Register Write Breakpoints are not functional for MSP430F2xx and
MSP430F4xx derivatives with >64kB Flash memory. |
None, the problem will be addressed in next CCSv5.1 service
release. |
|
SDSCM00043540 |
IDE |
MSP430 |
Re-enable Trace Buffer Support on MSP430 |
Trace support on MSP430 is missing. |
Use CCSv4. |
|
SDSCM00043910 |
IDE |
MSP430 |
MSP430 REGISTER view descriptions for SR.SCG0 and SR.SCG1
incorrect in CCSv5.1 |
|
|
|
SDSCM00043918 |
IDE |
MSP430 |
ULP Advisor is too intrusive on workflow, disabling the dialogs
needs to be global not per project |
This was pretty apparent when running our MSP430 workshop. I
understand the need to prompt the ULP Advisor tool as otherwise
pe... |
|
|
SDSCM00044133 |
IDE |
MSP430 |
double types not displayed properly in the Locals/Expressions
view for hexadecimal formats |
double types not displayed properly in the Locals/Expressions
view for hexadecimal format view. It simply displays it as '0'.
Wh... |
|
|
SDSCM00044279 |
IDE |
MSP430 |
Use of __TI_COMPILER_VERSION__ results in code incorrectly being
grayed out |
|
|
|
SDSCM00043412 |
Simulation |
Shannon Device Functional Simulator |
Error message when starting a debug session for a 6678 device
functional simulator |
When starting a debug session for the 6678 device functional
simulator, the below error occurs for each CPU: Trouble Reading
PC... |
|