|
Id |
Component |
Affected
Targets |
Headline |
Additional Details |
Workaround (if applicable) |
|
SDSCM00038605 |
DVT |
ALL |
STS and CPU Load views should indicate that they are not
supported in stop mode RTA |
Some functionality is not supported when running stop-mode RTA.
Such as the statistics and CPU load views. Ideally we should
d... |
|
|
SDSCM00039329 |
DVT |
ALL |
Profiling help topic is missing screen captures |
When you open the help for profiling it has some red X's where
the help references a screen capture but the screen capture is
mi... |
|
|
SDSCM00042046 |
DVT |
ALL |
Add Tools main menu in CCS Edit perspective |
Tools menu is only available in CCS Debug perspective |
|
|
SDSCM00043256 |
DVT |
ALL |
System Analyzer does not autodetect UIA projects when using JTAG
transport and multiple DSF sessions active |
System Analyzer sometimes does not autodetect that a UIA project
has been loaded when using JTAG as a transport. Once this cond... |
|
|
SDSCM00043761 |
DVT |
ALL |
The "Display Data Size" parameter of the graph tool seems
limited to 512 |
Setting a value greater than 512 for the "Display Data Size"
distorts the displayed data in the graph display. |
Use a value smaller than 512 |
|
SDSCM00043762 |
DVT |
ALL |
The format display for Y axis does not show 64-bit values
correctly |
When displaying graphs with 64-bit data, the Y axis shows
invalid data when using Display Format as General, Decimal or
Scientif... |
Use Hexadecimal format instead. Right-click on the graph view
and select Display Properties --> Axes --> Y-axis --> set the
val... |
|
SDSCM00039615 |
Emulation |
ALL |
CCS reports incorrect cycles for POPM.A PUSHM.A instructions |
When viewing the clock in CCS it reports an incorrect number of
cycles for POPM.A and PUSHM.A instructions. It reports them as
... |
|
|
SDSCM00041300 |
Emulation |
ALL |
XDS100 conflicts with USB to Serial cables |
It is possible for there to be a conflict between XDS100 and
Serial to USB cables. |
|
|
SDSCM00042138 |
Emulation |
ALL |
Emulation components and libraries should not rely on PATH
environment variable |
Certain emulation components and libraries get confused if an
older version of CCS (3.3 or 3.1) has certain bin directories
set ... |
Remove all references to CCS3.1 or 3.3 from the system path. |
|
SDSCM00042334 |
Emulation |
ALL |
Need to be able to see CP15 registers |
Developers using ARM cores at a very low-level usually require
viewing CP15 and other registers that are hidden by default in
th... |
All registers can be viewed in the Expressions view of CCSv5.1.
Simply type the name of the register with upper case. For exampl... |
|
SDSCM00043147 |
Emulation |
ALL |
TMS570LS3137 device xml files are missing Access Port
Designation setting |
Device files for TMS570LS3137 is missing Access Port Designation
setting. It should be set to 0x02000100. Without this setting,
... |
In the 'Advanced' tab of the Target Configuration editor, set
the Access Port Designation setting to 0x02000100 (make sure the
C... |
|
SDSCM00043783 |
Emulation |
ALL |
IERR register not visible for C64xx devices |
The IERR register doesn't show up in the register view. |
Open the expressions view and enter IERR. |
|
SDSCM00038571 |
IDE |
ALL |
Need excluded files filter for the Project Explorer |
In the Project Explorer, which will be the default project view
in CCSv5 instead of the C/C++ Projects View, there is a list of
... |
|
|
SDSCM00040028 |
IDE |
ALL |
Import wizard should prompt user to change compiler version if
needed |
If I am importing a project that uses a different version of the
compiler than what I have installed the wizard should inform
me... |
|
|
SDSCM00040045 |
IDE |
ALL |
NullPointerException when renaming project |
Sometimes when renaming an imported project you will get a
dialog complaining of a null pointer exception. |
|
|
SDSCM00040262 |
IDE |
ALL |
MMU Page table view should be listed on the view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
SDSCM00040708 |
IDE |
ALL |
For header files outside the project folder double clicking on
compile errors in the Problems view does not jump to error |
When a compilation error occurs in a header file that is outside
the project (e.g. system header file or even user header file
l... |
|
|
SDSCM00040717 |
IDE |
ALL |
DVT graph button should be disabled if the features are not
available |
In the Debug perspective there is a button to open DVT analysis
views. If you click on this button before launching a debug
ses... |
|
|
SDSCM00040737 |
IDE |
ALL |
Installer fails if user folder is linked to another location |
If your user folder or temp folder is symbolically linked to a
different location (called a Junction) you will get an error
when... |
Change your temporary folder to be a different folder that is
not linked. |
|
SDSCM00041325 |
IDE |
ALL |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension. The default 'Debug' and
'Relea... |
|
|
SDSCM00041406 |
IDE |
ALL |
US: Project properties is disabled even when there is a project
highlighted |
When you look at the project explorer there is a project
highlighted, but when you to to the project menu, properties
(and many ... |
You need to click again in the project explorer on the project
and then the menu items are enabled. |
|
SDSCM00041417 |
IDE |
ALL |
US: StellarisWare examples are not expanded properly in the
Resource Explorer |
StellarisWare should be fully expanded to show the examples in
Resource Explorer |
|
|
SDSCM00041425 |
IDE |
ALL |
Importing project should shrink the Editor area |
If I import a project from the project menu it does not make the
Project Explorer visible. The resource explorer and grace
welc... |
Double click on a tab in the editor area to make it smaller |
|
SDSCM00041649 |
IDE |
ALL |
After installing CCS, starting the setup program again causes
"Program Compatibility Assistant" dialog |
|
|
|
SDSCM00042212 |
IDE |
ALL |
ASM [Wxxxx] warning options treated as errors in problems view |
Warning [W9999] is displayed as an error in the problems tab. |
|
|
SDSCM00042270 |
IDE |
ALL |
Linker - Cmd mapping should be introduced when a user changes
defaults for RTSC projects. |
|
|
|
SDSCM00042271 |
IDE |
ALL |
source level debugging assembly code is not working. |
CCS organize the debug line info by functions. Most assemblers
have special directives to mark the begin or end of function in
a... |
|
|
SDSCM00042297 |
IDE |
ALL |
Emulation Updates Trigger Errors |
Emulator Updates currently trigger problems in CCS. |
Do not install the updates until a fix is implemented. |
|
SDSCM00042329 |
IDE |
ALL |
Support ISA aware dynamic support for view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
SDSCM00042750 |
IDE |
ALL |
Linux installer gets stuck if identical target content
components are already installed |
On Linux if you already have a version of a target contect
package such as IPC that is exactly the same as what CCS is
trying to... |
Uninstall the existing copy of IPC first or tell CCS not to
install IPC. |
|
SDSCM00043063 |
IDE |
ALL |
Switching stackframe in breadcrumb mode causes 'Run to line' to
disappear in the editor |
|
|
|
SDSCM00043161 |
IDE |
ALL |
Include terminal plugins as part of installation |
Request to include the terminal plug-in in the CCS installation |
Add the terminal plug-in according to the instructions here:
https://processors.wiki.ti.com/index.php/How_to_install_the_terminal... |
|
SDSCM00043248 |
IDE |
ALL |
Installer can not handle double byte/accented/special characters
giving no warning or error |
CCS will not install properly in a directory containing double
byte/special/accented characters. |
None |
|
SDSCM00043340 |
IDE |
ALL |
Files that are written when project properties (e.g. Debug
settings) are modified need to be checked out |
Some changes to project properties (e.g. Debugger settings) may
result in files being accessed. If they are under source
control... |
check out necessary file manually (.e.g .ccxml when modifying
device or emulator setting). |
|
SDSCM00043351 |
IDE |
ALL |
Console View Error highlighting does not match |
Build Console context highlighting of errors and warnings seems
offset by a line. |
|
|
SDSCM00043356 |
IDE |
ALL |
Web installer fails if McAfee is installed, CCS hangs |
Machine needs to have McAfee Internet Security Suite installed
Run the web installer Make your installation selections Install
w... |
Use the offline installer or disable the McAfee firewall.
McAfee will allow you disable it for a period of time. 60min
should ... |
|
SDSCM00043384 |
IDE |
ALL |
Installation fails to run on Ubuntu 11.10 64bit |
Installation fails to run on Ubuntu 11.10 Desktop 64bit |
|
|
SDSCM00043435 |
IDE |
ALL |
Active target configuration settings not kept |
When creating a project, if you select a connection type a
target configuration file (ccxml) gets autogenerated. If you
later... |
Manually set the active configuration |
|
SDSCM00043464 |
IDE |
ALL |
Differentiate between Standard Eclipse / CDT help and CCS IDE
help |
Standard Eclipse and CDT help content has screenshots and
instructions that contradict CCS specific documentation. We
should rem... |
|
|
SDSCM00043570 |
IDE |
ALL |
fsclean doesn't work on Linux |
fsclean doesn't do anything on Linux |
Manually delete the content of the /home/.TI/<some number>
folder |
|
SDSCM00043588 |
IDE |
ALL |
would like headless project build,created, import commands to
run without DISPLAY configured on linux |
on Linux, if DISPLAY is not configured (example when a hudson
build) then CCS project create/build will fail with GTK errors.
Wo... |
Configure virtual DISPLAY through xvfb. |
|
SDSCM00043589 |
IDE |
ALL |
Not all warnings are showing up in the problems view |
Some linker warnings are not appearing in the problems view. |
Look in the console view. |
|
SDSCM00043715 |
IDE |
ALL |
Typo in Resource Explorer main page |
There is a typo in the Resource Explorer main page. Basically
the line: "Filters at the top of this window can be use to
narrow... |
|
|
SDSCM00043956 |
IDE |
ALL |
GEL_MemoryLoad parameter "bitsize" is documented as optional,
but an error is thrown if it is omitted |
Whenever attempting to load a binary file using GEL_MemoryLoad()
without the parameter bitsize, CCS throws an error where it
say... |
Include the bitsize parameter. |
|
SDSCM00041210 |
Simulation |
ALL |
C6678 Device Functional Simulator is missing a dll file |
The C6678 Device Functional Simulator has been found to be
missing a dll in CCS 5.1 release M6. The error message shown
is: TMS... |
N/A |
|
SDSCM00041211 |
Simulation |
ALL |
Second Launch of C6678 Device Cycle Approximate Simulator locks
CCS |
In CCS v5.1 M6 it was found that launching a target
configuration a second time locks up CCS. After launching a
debug session ... |
Close CCS before a second launch of the configuration |
|
SDSCM00041861 |
Simulation |
ALL |
Incorrect processor ID in driver xml file causes device to show
up twice in project wizard |
If you have a device file with at C674x core and it has options
for the project wizard it shows up twice in the project wizard. |
Pick either device and it works fine |
|
SDSCM00043153 |
Simulation |
ALL |
Debug Server Scripting creates EP trace files with duplicate
.ept extensions |
Whenever EP trace on a simulator is enabled, it creates a file
with extension .ept in the same directory as the executable.
How... |
N/A |
|
SDSCM00043725 |
Simulation |
ALL |
674 simulator does not flush out pipeline when debugger writes
to the PC |
This issue potentially can occur on any C6000 based simulator
and not just C674 simulator. |
Before doing reload, do a reset in order to workaround this
issue. |
|
SDSCM00043926 |
Simulation |
ALL |
TCI6616 simulator cache tag-RAM viewer displays zero L2 Cache
lines when L2CFG.mode == 0x7 |
|
L2CFG.mode = 0x7 and L2CFG.mode == 0x6 both configure the cache
to 1MB. A workaround is to configure the L!CFG.mode to 0x6. The
... |
|
SDSCM00042994 |
IDE |
ARM Cortex A8 |
OMAP5430 : Problem when loading symbol on cortexM4 and CortexA15
CPU0 |
|
|
|
SDSCM00041464 |
IDE |
ARM Cortex M3 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds
th... |
Simply remove the file TMS320F28335.cmd from the project |
|
SDSCM00042728 |
IDE |
ARM Cortex M3 |
Emulator page in installer should list "Stellaris ICDI emulator"
when Stellaris is being installed |
When you select Stellaris in the device family listing it will
install support for the Stellaris ICDI emulator. However this
is... |
|
|
SDSCM00042994 |
IDE |
ARM Cortex M3 |
OMAP5430 : Problem when loading symbol on cortexM4 and CortexA15
CPU0 |
|
|
|
SDSCM00043593 |
IDE |
ARM Cortex M3 |
Stellaris driver xmls point to the windows driver on Linux |
Unable to launch debug sessions using Stellaris ICDI on Linux. |
|
|
SDSCM00040875 |
Emulation |
ARM Cortex R4 |
Memory mapping for LIN peripheral register in GEL file needs
updating |
Memory mapping for LIN peripheral register in TMS570 GEL file
needs to be updated to a length of 0x200 instead of 0x100. |
|
|
SDSCM00042185 |
Simulation |
ARM Cortex R4 |
Disassembly view of Cortex R4 Functional Simulator BE32 shows
incorrect instructions due to incorrect endianness |
Disassembly view of Cortex R4 Functional Simulator BE32 shows
incorrect instructions due to incorrect endianness |
|
|
SDSCM00034673 |
IDE |
C2800 |
CCS v4 allows usage of 1 hardware breakpoint less than CCS 3.3
for BIOS programs |
CCS v4.0x allows user to set only 1 hardware breakpoint when
debugging BIOS programs in Flash |
|
|
SDSCM00041464 |
IDE |
C2800 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds
th... |
Simply remove the file TMS320F28335.cmd from the project |
|
SDSCM00042703 |
IDE |
C2800 |
C2000 Device Support Feature needs to be renamed |
When you check for updates in CCS you may see an update called
"C2000 Emulators". This feature name is not clear. The updated
... |
|
|
SDSCM00043250 |
IDE |
C2800 |
Debugger does not allow setting breakpoints in some cases when
debugging overlay code |
Debugger sometimes does not allow setting breakpoints in source
files dealing with overlay code |
|
|
SDSCM00038672 |
DVT |
C6416 |
CCSv4.2 RC1 profiler doesn’t correctly report the type of
cycles, cycle.CPU versus cycle.Total |
CCSv4.2 RC1 profiler doesn’t correctly report the type of
cycles, cycle.CPU versus cycle.Total , Simulator used: C6416
device si... |
|
|
SDSCM00041366 |
DVT |
C64x Plus Emulator |
Code Coverage coloring does not work for files that do not have
a CCS Project |
Line coloring works if coverage is done for an executable from a
CCS Project. Does not work E.g. if a .out file is directly
loa... |
|
|
SDSCM00043140 |
IDE |
C66xx |
Events for the profile clock are mis-assigned on C66x |
There are miss-assignments for the events counted by the profile
clock. Event "L1D read hit" is actually counting CPU clock
cycl... |
|
|
SDSCM00042245 |
IDE |
HD-Davinci |
Verification errors on program load for DM6446 |
CSL example for DM6446 EVM loads fine using CCSv3.3 but fails
with a data verification error on v4. The same program and
startup... |
Turing off data verification in v4 allowed the program to load. |
|
SDSCM00042038 |
Emulation |
MSP430 |
MSP 430 Write Register Breakpoint does not work |
Register Write Breakpoints are not functional for MSP430F2xx and
MSP430F4xx derivatives with >64kB Flash memory. |
None, the problem will be addressed in next CCSv5.1 service
release. |
|
SDSCM00043540 |
IDE |
MSP430 |
Re-enable Trace Buffer Support on MSP430 |
Trace support on MSP430 is missing. |
Use CCSv4. |
|
SDSCM00043591 |
IDE |
MSP430 |
Despite available option, can not launch debug without
connecting to target |
|
|
|
SDSCM00043592 |
IDE |
MSP430 |
Program load error message indicate that the cause was GEL |
|
|
|
SDSCM00043910 |
IDE |
MSP430 |
MSP430 REGISTER view descriptions for SR.SCG0 and SR.SCG1
incorrect in CCSv5.1 |
|
|
|
SDSCM00043918 |
IDE |
MSP430 |
ULP Advisor is too intrusive on workflow, disabling the dialogs
needs to be global not per project |
This was pretty apparent when running our MSP430 workshop. I
understand the need to prompt the ULP Advisor tool as otherwise
pe... |
|
|
SDSCM00043998 |
IDE |
MSP430 |
The compiler option setting for Function Subsections displays an
empty drop-down list |
CCS does not allow user to select "Function Subsections"
compiler option via the graphical properties. |
|
|
SDSCM00039679 |
IDE |
OMAP4430 |
erroneous data reported in CCS trace for statistical collector |
|
|
|
SDSCM00043412 |
Simulation |
Shannon Device Functional Simulator |
Error message when starting a debug session for a 6678 device
functional simulator |
When starting a debug session for the 6678 device functional
simulator, the below error occurs for each CPU: Trouble Reading
PC... |
|
|
SDSCM00042212 |
IDE |
TCI6614 Device Functional Simulator |
ASM [Wxxxx] warning options treated as errors in problems view |
Warning [W9999] is displayed as an error in the problems tab. |
|