|
Id |
Component |
CCS
Version |
Affected
Targets |
Headline |
Additional Details |
Workaround (if applicable) |
|
SDSCM00038605 |
DVT |
4.2.0 |
ALL |
STS and CPU Load views should indicate that they are not
supported in stop mode RTA |
Some functionality is not supported when running stop-mode RTA.
Such as the statistics and CPU load views. Ideally we should
d... |
|
|
SDSCM00038738 |
DVT |
4.2.0 |
ALL |
Image Analyzer Help should not be buried under tasks |
Currently it is very hard to find the image analyzer help in CCS
as it is not in a feature section and instead buried in the tas... |
|
|
SDSCM00039329 |
DVT |
4.2.1 |
ALL |
Profiling help topic is missing screen captures |
When you open the help for profiling it has some red X's where
the help references a screen capture but the screen capture is
mi... |
|
|
SDSCM00040055 |
DVT |
4.2.3 |
ALL |
After creating two single time graphs, restarting CCS causes one
of them to become line graph |
After creating two single time graphs, restarting CCS causes one
of them to become a line graph. |
|
|
SDSCM00042046 |
DVT |
5.1.0 |
ALL |
Add Tools main menu in CCS Edit perspective |
Tools menu is only available in CCS Debug perspective |
|
|
SDSCM00042557 |
DVT |
5.1.0 |
ALL |
Image analyzer should implement higher than 8-bit per channel on
RGB modes |
The Image Analyzer should be able to properly recognize images
with higher dynamic range. Currently it supports 8-bit per
chann... |
N/A. |
|
SDSCM00038607 |
Emulation |
4.2.0 |
ALL |
XDS100: When PID/VID is not programmed the emulation error
message should state what the likely problem is |
Not every vendor has been good about making sure the EEPROM on
the FTDI chips are properly programming. As part of a CCS
servic... |
|
|
SDSCM00039615 |
Emulation |
4.2.1 |
ALL |
CCS reports incorrect cycles for POPM.A PUSHM.A instructions |
When viewing the clock in CCS it reports an incorrect number of
cycles for POPM.A and PUSHM.A instructions. It reports them as
... |
|
|
SDSCM00040412 |
Emulation |
4.2.3 |
ALL |
Installation from CP Tracer Update Manager site caused CCS to
not launch configuration |
|
|
|
SDSCM00041300 |
Emulation |
5.1.0 |
ALL |
XDS100 conflicts with USB to Serial cables |
It is possible for there to be a conflict between XDS100 and
Serial to USB cables. |
|
|
SDSCM00042844 |
Emulation |
5.1.0 |
ALL |
REP register not available in Register View for C6678 |
When connected to a C6678 or any C66 device the REP register is
not visible. |
|
|
SDSCM00038571 |
IDE |
5.0.1 |
ALL |
Need excluded files filter for the Project Explorer |
In the Project Explorer, which will be the default project view
in CCSv5 instead of the C/C++ Projects View, there is a list of
... |
|
|
SDSCM00038683 |
IDE |
5.0.1 |
ALL |
[CDT] Project always rebuilds when the active configuration is
switched |
When you switch the active configuration (ex. from Debug to
Release) and then do a build, it will always rebuild, even if
there ... |
|
|
SDSCM00040028 |
IDE |
5.1.0 |
ALL |
Import wizard should prompt user to change compiler version if
needed |
If I am importing a project that uses a different version of the
compiler than what I have installed the wizard should inform
me... |
|
|
SDSCM00040045 |
IDE |
5.1.0 |
ALL |
NullPointerException when renaming project |
Sometimes when renaming an imported project you will get a
dialog complaining of a null pointer exception. |
|
|
SDSCM00040262 |
IDE |
5.1.0 |
ALL |
MMU Page table view should be listed on the view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
SDSCM00040708 |
IDE |
5.1.0 |
ALL |
For header files outside the project folder double clicking on
compile errors in the Problems view does not jump to error |
When a compilation error occurs in a header file that is outside
the project (e.g. system header file or even user header file
l... |
|
|
SDSCM00040717 |
IDE |
5.1.0 |
ALL |
DVT graph button should be disabled if the features are not
available |
In the Debug perspective there is a button to open DVT analysis
views. If you click on this button before launching a debug
ses... |
|
|
SDSCM00040737 |
IDE |
4.2.3 |
ALL |
Installer fails if user folder is linked to another location |
If your user folder or temp folder is symbolically linked to a
different location (called a Junction) you will get an error
when... |
Change your temporary folder to be a different folder that is
not linked. |
|
SDSCM00041269 |
IDE |
5.1.0 |
ALL |
[CDT] Unnecessary builds in CCS5 when using command line builds
for different configurations |
|
|
|
SDSCM00041406 |
IDE |
5.1.0 |
ALL |
US: Project properties is disabled even when there is a project
highlighted |
When you look at the project explorer there is a project
highlighted, but when you to to the project menu, properties
(and many ... |
You need to click again in the project explorer on the project
and then the menu items are enabled. |
|
SDSCM00041417 |
IDE |
5.1.0 |
ALL |
US: StellarisWare examples are not expanded properly in the
Resource Explorer |
StellarisWare should be fully expanded to show the examples in
Resource Explorer |
|
|
SDSCM00041425 |
IDE |
5.1.0 |
ALL |
Importing project should shrink the Editor area |
If I import a project from the project menu it does not make the
Project Explorer visible. The resource explorer and grace welc... |
Double click on a tab in the editor area to make it smaller |
|
SDSCM00041461 |
IDE |
5.1.0 |
ALL |
Update manager generates errors and does not work |
Update manager generates errors and does not work as expected. |
|
|
SDSCM00041649 |
IDE |
5.1.0 |
ALL |
After installing CCS, starting the setup program again causes
"Program Compatibility Assistant" dialog |
|
|
|
SDSCM00042212 |
IDE |
5.1.0 |
ALL |
ASM [Wxxxx] warning options treated as errors in problems view |
Warning [W9999] is displayed as an error in the problems tab. |
|
|
SDSCM00042270 |
IDE |
5.1.0 |
ALL |
Linker - Cmd mapping should be introduced when a user changes
defaults for RTSC projects. |
|
|
|
SDSCM00042280 |
IDE |
5.1.0 |
ALL |
file specific post build step causes error |
When specifying a file specific post build step, an error occurs
when building: Errors occurred during the build. Errors
runnin... |
|
|
SDSCM00042297 |
IDE |
5.1.0 |
ALL |
Emulation Updates Trigger Errors |
Emulator Updates currently trigger problems in CCS. |
Do not install the updates until a fix is implemented. |
|
SDSCM00042329 |
IDE |
5.1.0 |
ALL |
Support ISA aware dynamic support for view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
SDSCM00042367 |
IDE |
5.1.0 |
ALL |
Popup Help Doesn't Line-Wrap |
|
|
|
SDSCM00042473 |
IDE |
5.1.0 |
ALL |
Problems view fails to show a syntax error. Waiting for 42579 to
be fixed before IDE can fix the problem. |
Problems view fails to properly display a missing bracket syntax
error in a C source file. This issue may be due to the fact
t... |
N/A. |
|
SDSCM00042582 |
IDE |
5.1.0 |
ALL |
Adding a virtual folder throws a warning when it should not |
Adding a virtual folder to a project throws a warning when it
should not. "This project contains unresolved buildable
linked... |
|
|
SDSCM00042621 |
IDE |
5.1.0 |
ALL |
Problems view should not throw errors for target configuration
files (.ccxml) linked to projects |
If a target configuration file (.ccxml) is linked to a project
through a Path Variable, the Problems View (and the Project
Manag... |
Add the file using hardcoded path instead. |
|
SDSCM00042670 |
IDE |
5.1.0 |
ALL |
TI816x and TI814x files missing when just installing DaVinci
support |
Today in CCSv5.1.0 if you install support for DaVinci only you
do not get the device files for TI816x and TI814x which are the
r... |
Download and unzip the DaVinci device support package from the
CCS download page. |
|
SDSCM00042750 |
IDE |
5.1.0 |
ALL |
Linux installer gets stuck if identical target content
components are already installed |
On Linux if you already have a version of a target contect
package such as IPC that is exactly the same as what CCS is
trying to... |
Uninstall the existing copy of IPC first or tell CCS not to
install IPC. |
|
SDSCM00042808 |
IDE |
5.1.0 |
ALL |
__FILE__ and __LINE__ are not recognized by the dynamic syntax
checker |
These are replaced by the preprocessor with the name of the file
and the line number and thus are valid. However the dynamic
sy... |
Ignore the question mark |
|
SDSCM00042818 |
IDE |
5.1.0 |
ALL |
Project dependency is not set properly when done via
Properties->Project References |
Project dependency is not set properly when done via
Properties->Project References |
Add the project reference from Properties->CCS
Build->Dependencies |
|
SDSCM00042836 |
IDE |
5.1.0 |
ALL |
Projects created with old versions of CCSv4 (pre and 4.0.x
releases) fail to properly import into CCSv5.1 |
Although the projects are imported correctly and build fine, the
Project Properties do not display the "CCS General" and "CCS
Bu... |
Import the project into a newer CCSv4.2.x version and then
import it to CCSv5.1 |
|
SDSCM00042885 |
IDE |
5.1.0 |
ALL |
Need to automatically discover packages in C:\TI |
The default installation directory for many target content
packages is C:\TI. We should automatically discover RTSC
products in... |
Point CCS to the in installation directory. |
|
SDSCM00042886 |
IDE |
5.1.0 |
ALL |
SYS/BIOS templates before DSP/BIOS templates |
Currently the DSP/BIOS 5 templates show up before the SYS/BIOS
templates in the project wizard. In fact the SYS/BIOS templates
... |
|
|
SDSCM00042888 |
IDE |
5.1.0 |
ALL |
When a .cfg file is active in the editor build actions are
disabled |
When you have a .cfg file as the active file in editor the build
button is disabled. The .cfg file is part of the project so th... |
Open another file in the project. |
|
SDSCM00042924 |
IDE |
5.1.0 |
ALL |
__cregister not recognized by the editor syntax checker |
The editor does not recognize __cregister as a valid keyword and
reports a syntax error. It does recognize cregister fine. |
Ignore the error. It does not impact compilation. |
|
SDSCM00042927 |
IDE |
5.1.0 |
ALL |
License Monitor heartbeat |
CCS needs to be run as administor or else lack of access to
certain folders can cause a java error from the license manager. |
Run as administrator. |
|
SDSCM00042959 |
IDE |
5.1.0 |
ALL |
Renaming .asm source files results in "missing separator" gmake
error |
For a CCSv4 project imported in CCSv5, renaming source files may
result in "missing separator" gmake error |
|
|
SDSCM00042960 |
IDE |
5.1.0 |
ALL |
Changes to source files (location, name etc) causes the project
to no longer find the files properly |
After importing CCSv4 project into CCSv5, making changes to
source file locations may cause the project to no longer find
the fi... |
|
|
SDSCM00042970 |
IDE |
5.1.0 |
ALL |
CCS editor shows unexplainable syntax error for macro |
CCS editor sometimes shows unexplainable syntax errors for some
macros. |
|
|
SDSCM00041210 |
Simulation |
5.1.0 |
ALL |
C6678 Device Functional Simulator is missing a dll file |
The C6678 Device Functional Simulator has been found to be
missing a dll in CCS 5.1 release M6. The error message shown
is: TMS... |
N/A |
|
SDSCM00041211 |
Simulation |
5.1.0 |
ALL |
Second Launch of C6678 Device Cycle Approximate Simulator locks
CCS |
In CCS v5.1 M6 it was found that launching a target
configuration a second time locks up CCS. After launching a
debug session ... |
Close CCS before a second launch of the configuration |
|
SDSCM00041861 |
Simulation |
5.1.0 |
ALL |
Incorrect processor ID in driver xml file causes device to show
up twice in project wizard |
If you have a device file with at C674x core and it has options
for the project wizard it shows up twice in the project wizard. |
Pick either device and it works fine |
|
SDSCM00042742 |
Trace |
5.1.1 |
ALL |
CCS locks up when using Pro Trace and XDS560V2 simultaneously |
|
|
|
SDSCM00041464 |
IDE |
5.1.0 |
ARM Cortex M3 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds th... |
Simply remove the file TMS320F28335.cmd from the project |
|
SDSCM00042646 |
IDE |
5.1.0 |
ARM Cortex M3 |
Request for CPU reset to not be performed when connecting to
Stellaris devices |
Request for CPU reset to not be performed when connecting to
Stellaris devices |
|
|
SDSCM00042728 |
IDE |
5.1.0 |
ARM Cortex M3 |
Emulator page in installer should list "Stellaris ICDI emulator"
when Stellaris is being installed |
When you select Stellaris in the device family listing it will
install support for the Stellaris ICDI emulator. However this
is... |
|
|
SDSCM00040875 |
Emulation |
4.2.3 |
ARM Cortex R4 |
Memory mapping for LIN peripheral register in GEL file needs
updating |
Memory mapping for LIN peripheral register in TMS570 GEL file
needs to be updated to a length of 0x200 instead of 0x100. |
|
|
SDSCM00042185 |
Simulation |
4.2.4 |
ARM Cortex R4 |
Disassembly view of Cortex R4 Functional Simulator BE32 shows
incorrect instructions due to incorrect endianness |
Disassembly view of Cortex R4 Functional Simulator BE32 shows
incorrect instructions due to incorrect endianness |
|
|
SDSCM00034673 |
IDE |
5.1.0 |
C2800 |
CCS v4 allows usage of 1 hardware breakpoint less than CCS 3.3
for BIOS programs |
CCS v4.0x allows user to set only 1 hardware breakpoint when
debugging BIOS programs in Flash |
|
|
SDSCM00041464 |
IDE |
5.1.0 |
C2800 |
The project wizard adds a linker CMD file when a SYSBIOS example
project template is used |
When creating a project for a device that has a linker CMD file
(Stellaris, C2800, some C5500), the wizard automatically adds
th... |
Simply remove the file TMS320F28335.cmd from the project |
|
SDSCM00042703 |
IDE |
5.1.0 |
C2800 |
C2000 Device Support Feature needs to be renamed |
When you check for updates in CCS you may see an update called
"C2000 Emulators". This feature name is not clear. The updated
... |
|
|
SDSCM00041366 |
DVT |
5.1.0 |
C64x Plus Emulator |
Code Coverage coloring does not work for files that do not have
a CCS Project |
Line coloring works if coverage is done for an executable from a
CCS Project. Does not work E.g. if a .out file is directly
loa... |
|
|
SDSCM00038932 |
IDE |
5.0.1 |
C64xx |
Importing CCS 3.3 project results in Java errors |
In certain cases, importing a CCS 3.3 project into CCS5 may
result in Java errors. |
|
|
SDSCM00042212 |
IDE |
5.1.0 |
C66xx |
ASM [Wxxxx] warning options treated as errors in problems view |
Warning [W9999] is displayed as an error in the problems tab. |
|
|
SDSCM00042245 |
IDE |
4.2.4 |
HD-Davinci |
Verification errors on program load for DM6446 |
CSL example for DM6446 EVM loads fine using CCSv3.3 but fails
with a data verification error on v4. The same program and
startup... |
Turing off data verification in v4 allowed the program to load. |
|
SDSCM00042038 |
Emulation |
5.1.0 |
MSP430 |
MSP 430 Write Register Breakpoint does not work |
Register Write Breakpoints are not functional for MSP430F2xx and
MSP430F4xx derivatives with >64kB Flash memory. |
None, the problem will be addressed in next CCSv5.1 service
release. |
|
SDSCM00042469 |
IDE |
5.1.0 |
MSP430 |
Trouble when activating CCS 5.1 license |
|
|
|
SDSCM00042523 |
IDE |
5.1.0 |
MSP430 |
Expressions/variables view does not correctly display long long
variables |
Expressions/variables view does not correctly display long long
variables on MSP430 devices. |
|
|
SDSCM00042928 |
IDE |
5.1.0 |
MSP430 |
Unsupported Linker Options remain after switching devices |
Not all options are checked and removed if changing devices to a
device which does not support the option. Only MSP430 tested.
... |
Currently manually verifying and checking such linker and
compiler options. |
|
SDSCM00039679 |
IDE |
4.2.1 |
OMAP4430 |
erroneous data reported in CCS trace for statistical collector |
|
|
|
SDSCM00042370 |
IDE |
5.1.0 |
OMAP4430 |
CCSv5.1M8.5 : spurious “program file not found” pop up window
when ETB used as trace event receiver |
|
|
|
SDSCM00042968 |
IDE |
5.1.1 |
TMS470 |
RESET problem is DS_LOG |
|
|
|
SDSCM00042973 |
IDE |
5.1.0 |
TMS470 |
ELF loader doesn't zero-initialize difference between "file
size" and "mem size" |
|
|