|
Id |
Domain |
CCS
Version |
Affected
Targets |
Headline |
Additional Details |
Workaround (if applicable) |
|
SDSCM00034172 |
Emulation |
4.0.2 |
ALL |
Windows driver locations are not consistent for XDS100 and XDS560 |
Windows driver locations are not consistent for XDS100 and XDS560.
Sometimes you have to manually locate the windows drivers to ... |
|
|
SDSCM00039742 |
Emulation |
4.2.2 |
ALL |
Error message provided when IP address is invalid should state that the
IP address is invalid |
When using an XDS560v2 emulator on LAN you have to provide an IP
address. By default this is set to x.x.x.x.x. If you forget t... |
|
|
SDSCM00038571 |
IDE |
5.0.1 |
ALL |
Need excluded files filter for the Project Explorer |
In the Project Explorer, which will be the default project view in CCSv5
instead of the C/C++ Projects View, there is a list of ... |
|
|
SDSCM00038658 |
IDE |
5.0.0 |
ALL |
plug-in installation option needs to verify minimum Eclipse version is
present |
When installing CCSv5 you can choose between a complete installation and
a plug-in installation. For the plug-in installation y... |
|
|
SDSCM00038683 |
IDE |
5.0.1 |
ALL |
Project always rebuilds when the active configuration is switched |
When you switch the active configuration (ex. from Debug to Release) and
then do a build, it will always rebuild, even if there ... |
|
|
SDSCM00039195 |
IDE |
5.0.1 |
ALL |
Update sites for CCSv5 on Linux download windows installers |
When you check for updates within CCSv5 Linux it finds updates for the
compilers. However the installer packages that it downlo... |
Contact TI via the E2E forums and request a Linux version of the
compiler installer that you need. |
|
SDSCM00039288 |
IDE |
5.0.1 |
ALL |
Download of Target Content installs in different path than full install |
|
|
|
SDSCM00039326 |
IDE |
5.0.2 |
ALL |
Log file should only be written duing update and install |
|
|
|
SDSCM00039330 |
IDE |
5.0.2 |
ALL |
Installer should detect if target destination is not empty |
When a user uninstalls CCS it can leave a number of files behind. If a
user then installs a new copy of CCS into that directory... |
|
|
SDSCM00039363 |
IDE |
5.0.1 |
ALL |
Batch Project Clean and then project build does not wait for all
projects to be cleaned. |
Selecting multiple projects and doing a clean, immediately followed by a
build will build some projects before all projects have... |
|
|
SDSCM00039472 |
IDE |
5.0.2 |
ALL |
${InputDirRelPath} macro is missing |
The ${InputDirRelPath} macro is no longer working in CCSv5.x. It is
likely that the ${InputFileRelPath} and other Input* macros... |
|
|
SDSCM00039515 |
IDE |
5.0.1 |
ALL |
[CDT] switching active build configuration touches .cproject file, there
are no changes being made to the file |
Switching projects' active build configuration modifies .cproject files
timestamp, causing it to be checkout if version controll... |
|
|
SDSCM00039561 |
IDE |
5.0.1 |
ALL |
Would like to see a warning/error to be generated when BIOS version used
for compilation is different from project settings |
There is no warning or error if BIOS version set in the project is
different than what is installed/discovered by CCS. There sho... |
|
|
SDSCM00039749 |
IDE |
5.0.3 |
ALL |
Unable to add custom dropins folder unless specified folders are
writeable |
Using -Dorg.eclipse.equinox.p2.reconciler.dropins.directory=path is not
working unless certain folders in the Eclipse install a... |
|
|
SDSCM00039360 |
Trace |
5.0.2 |
ALL |
Trace related files written to the installation folder |
Several files are being written to the installation folder (tracecntrl.ini,
log.00000001, topics, __catalog). This may affect mu... |
Make the analysis\bin folder writable. |
|
SDSCM00039209 |
Emulation |
5.0.1 |
ARM Cortex A8 |
CCS fails to throw an error and hangs indefinitely when trying to load
code to non-configured memory |
Whenever code is attempted to be loaded to non-configured memory (i.e.,
external memory), CCS fails to report this occurrence an... |
N/A |
|
SDSCM00027780 |
Emulation |
3.3.0 |
ARM Cortex M3 |
Cortex UDIV and SDIV instructions not disassembled in CCS |
|
|
|
SDSCM00035280 |
Emulation |
3.3 SR9 |
ARM Cortex M3 |
CCS doesn't indicate status change on slave processor after GEL
Restart_Cores() |
CCS doesn't indicate status change on slave processor after GEL
Restart_Cores() |
|
|
SDSCM00011412 |
Emulation |
2.2.1 |
C2800 |
CCS hangs on File -> Data -> Save for lengths above 0x4000 |
CCS 2.21 hangs on 'File -> Data -> Save' for lengths above 0x4000,
when using eZdsp 2812 board connected via xds560 emulator. ... |
Please describe the workaround for this problem. |
|
SDSCM00019419 |
Emulation |
3.1.0 |
C2800 |
The CPU clock cycles show inconsistent values in different iterations of
a particular ISR subroutine. |
|
|
|
SDSCM00011423 |
Emulation |
2.2.1 |
C5400 |
Single stepping through 2 DST instructions generates incorrect results |
Under certain conditions, when single stepping through assembly code
that contains two DSK instructions that write an accumula... |
|
|
SDSCM00039508 |
IDE |
5.0.2 |
C54x |
When using custom install, selecting OMAP also selects C54x and C55x
support |
This is just a nuisance, but since CCSv5 does not officially support the
older OMAP devices that contain C54x and C55x cores any... |
N/A |
|
SDSCM00003362 |
Emulation |
3.1.0 |
C5500 |
Disassembly window still displays using the old C55 syntax. |
Disassembly window still displays using the old C55 syntax. |
|
|
SDSCM00011463 |
Emulation |
2.2.1 |
C5500 |
Timer plugin does not all TLB to set TIM value |
When connected with the XDS560 emulator to the 5510DSK, setting the
TLB bit in the Timer plugin should allow the TIM value to ... |
|
|
SDSCM00011464 |
Emulation |
2.2.1 |
C5500 |
CCS hangs with timer TIM register modified using TImer plugin |
CCS will hang of the Timer TIM register is modified via the Timer
plugin when an XDS560 is used. |
|
|
SDSCM00011486 |
Emulation |
2.2.1 |
C5500 |
TIM register for timer0 does not change in the timer peripheral window |
The TIM register for timer0 does not change in the Timer peripheral
window. |
Please describe the workaround for this problem. |
|
SDSCM00011494 |
Emulation |
2.2.1 |
C5500 |
Memory contents stored on SARAM of DSK5510 gets corrupted. |
Memory contents stored on SARAM of DSK5510 gets corrupted. |
Please describe the workaround for this problem. |
|
SDSCM00011626 |
Emulation |
2.2.1 |
C5500 |
commands in c5509a.gel need to be rearranged; need comment on TMCR |
On running c5509a.gel file in CCS3.1 the following error message pops
up: 'memory map prevented write to target memory at 0x00... |
Please describe the workaround for this problem. |
|
SDSCM00039508 |
IDE |
5.0.2 |
C55X |
When using custom install, selecting OMAP also selects C54x and C55x
support |
This is just a nuisance, but since CCSv5 does not officially support the
older OMAP devices that contain C54x and C55x cores any... |
N/A |
|
SDSCM00011617 |
Emulation |
2.2.1 |
C6000 |
CCS gel file for 6416dsk |
The example gel file (DSK6416.gel) for the 6416dsk does not memory map
the GPPOL register therefor the register does not appea... |
Please describe the workaround for this problem. |
|
SDSCM00014919 |
Emulation |
3.3.0 |
C6000 |
xdsfamily.cfg file reports a non-existent C622x DSP family |
<xdsfamily.cfg> file reports a non-existent C622x DSP family |
No workaround needed. This issue does not affect the functionality of
emulation and Code Composer Studio. |
|
SDSCM00038932 |
IDE |
5.0.1 |
C64xx |
Importing CCS 3.3 project results in Java errors |
In certain cases, importing a CCS 3.3 project into CCS5 may result in
Java errors. |
|
|
SDSCM00039229 |
Emulation |
4.2.1 |
C66xx |
Disassembly output incorrect for C66x |
Some compressed instructions are being incorrectly disassembled |
|
|
SDSCM00039871 |
Emulation |
4.2.3 |
C66xx |
Cannot start debugger due to problem loading TPI disassembly DLL |
|
|
|
SDSCM00039751 |
Emulation |
5.0.2 |
TI814x |
CCS does not display TI814x as available device under any of the
XDS560v2 emulator connections |
CCS does not display TI814x as available device under the XDS560v2
LAN/USB emulator connections. |
|
|
SDSCM00033899 |
Emulation |
4.0.1 |
MSP430 |
Debugger always reset target when using Launch TI Debugger |
When trying to connect to a running target, the "Launch TI Debugger"
menu item in CCS v4 always resets the target even if the se... |
|
|
SDSCM00038216 |
Emulation |
4.1.3 |
MSP430 |
Breakpoints set in one address are being mirrored in all FLASH memory
banks. |
This issue affects MSP430 devices that feature extended memory. If a
breakpoint is set at a given address in one memory bank, th... |
There is a hack to this issue published at the forum thread:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/... |
|
SDSCM00038769 |
Emulation |
4.2.0 |
MSP430 |
Disassembly view is incorrect on F5438 after a function call |
For F5438, a function calll is not returning to the expected location.
When stepping through a funciton call, the disassembly vi... |
|
|
SDSCM00011391 |
Emulation |
2.2.1 |
OMAP |
CIO breakpoints do not function correctly if instruction cache enabled |
CCS crashes if instruction cache is enabled. |
|
|
SDSCM00011664 |
Emulation |
2.2.1 |
OMAP |
No Popup reset window for CCS2.2, for DM310 connected via XDS510 |
When working normally with CCS2.2 for DM310 platform connected via
XDS510 JTAG, if emulator loses power or is disconnected fro... |
Please describe the workaround for this problem. |
|
SDSCM00039508 |
IDE |
5.0.2 |
OMAP |
When using custom install, selecting OMAP also selects C54x and C55x
support |
This is just a nuisance, but since CCSv5 does not officially support the
older OMAP devices that contain C54x and C55x cores any... |
N/A |
|
SDSCM00038967 |
Emulation |
5.0.1 |
TI816x |
CCS fails to reconnect to the 816x device after performing a Emulator
reset. |
When an emulator reset is issued from the CCS IDE, the emulator is
unable to reconnect to the 816x device. The error message i... |
Termiinate the debug session and relaunch. |
|
SDSCM00039847 |
Emulation |
5.0.2 |
TI816x |
Device xml files ti816x*.xml incorrectly list CPU as C64XP instead of
C674X |
Device xml files ti816x*.xml incorrectly list CPU as C64XP instead of
C674X |
|
|
SDSCM00039895 |
Emulation |
5.0.2 |
TI816x |
Linux version of tixds100v2CortexM.xml contains reference to Windows
version of driver hance fails during connection |
Linux version of tixds100v2CortexM.xml contains reference to Windows
version of driver instead of Linux, hence any device config... |
|
|
SDSCM00039898 |
Emulation |
5.0.2 |
TI816x |
Connecting to TI816x EVM with XDS510USB emulator results in GTI errors |
Connecting to TI816x EVM with Spectrum Digital XDS510USB emulator
results in GTI errors |
|
|
SDSCM00011345 |
Emulation |
2.2.1 |
TMS470 |
CCS incorrectly disassembles certain STRH instructions |
Code Composer Studio 2.2x may incorrectly disassemble certain STRH
instructions. For instance, STRH R12, [R1, -R0] is disassemb... |
Please describe the workaround for this problem. |
|
SDSCM00011384 |
Emulation |
2.2.1 |
TMS470 |
When stepping into SWI instruction, SPSR_svc indicates abort mode |
Stepping into a SWI instruction on ARM9 causes strange behavior of
SPSR_svc (supervisor saved program status register). As so... |
Please describe the workaround for this problem. |
|
SDSCM00034673 |
Emulation |
4.0.1 |
|
CCS v4 allows usage of 1 hardware breakpoint less than CCS 3.3 for BIOS
programs |
CCS v4.0x allows user to set only 1 hardware breakpoint when debugging
BIOS programs in Flash |
|
|
SDSCM00034753 |
Emulation |
4.1.0 |
|
When launching becomes unresponsive, dump all thread stacks and other
information to a log file |
|
|
|
SDSCM00035993 |
Emulation |
4.1.2 |
|
Global Breakpoint docs out of date |
|
|
|
SDSCM00037244 |
Emulation |
4.1.3 |
|
Global Breakpoints do not work |
Global Breakpoints are supposed to halt multiple cores when a single
breakpoint in any individual core is reached. Enabling Glo... |
No workaround is available |
|
SDSCM00037923 |
Emulation |
4.1.3 |
|
Emulation installer hangs on Windows XP SP3 32-bit machine while
installing xds560 driver |
|
Workaround for now is the one provided by Aarti Goyle: - Unzip the CCS
package, move the emulation installer to another director... |
|
SDSCM00037938 |
Emulation |
4.1.3 |
|
The CCS v4.1.3 installation does not install the MSP_430 Application
UART driver properly |
The CCS v4.1.3 installation does not install the MSP_430 Application
UART driver properly. As a result, if you plug in a Launch... |
Manually point CCS to the location of the driver |
|
SDSCM00038360 |
Emulation |
4.0.1 |
|
ECOM does not support using two different types of xds560 emulators in a
single CCS session |
|
Either use two xds560 emulators of the same type or use at least one
emulator that is not an xds560 (for example xds100) |
|
SDSCM00038565 |
Emulation |
4.1.3 |
|
Unable to view the EPI memory space in the debug sessions memory browser
window on Stellaris parts. |
|
All you need to do is add the following line to the memorymap_init()
function which is found in the Stellaris *.gel files: ... |
|
SDSCM00038607 |
Emulation |
4.2.0 |
|
XDS100: When PID/VID is not programmed the emulation error message
should state what the likely problem is |
Not every vendor has been good about making sure the EEPROM on the FTDI
chips are properly programming. As part of a CCS servic... |
|
|
SDSCM00039172 |
Emulation |
4.2.1 |
|
CCS generates data verification error when programming to information
memory on G2xx2 devices |
Prorgamming of data into information memory fails with error: MSP430:
File Loader: Data verification failed at address 0x000010... |
|
|
SDSCM00039198 |
Emulation |
4.2.1 |
|
Clock is not available for TMS570 devices |
Clock is not available for any emulator when using a CortexR4 TMS570LS.
All of the menu items are disabled. |
|
|
SDSCM00039615 |
Emulation |
4.2.1 |
|
CCS reports incorrect cycles for POPM.A PUSHM.A instructions |
When viewing the clock in CCS it reports an incorrect number of cycles
for POPM.A and PUSHM.A instructions. It reports them as ... |
|
|
SDSCM00039843 |
Emulation |
4.2.2 |
|
Errors when connecting to ARM926 devices with XDS100v2 |
Attempting to connect to DM365 or DM6467 results in a series of errors
in the console |
Turn on adaptive clocking in target setup. |
|
SDSCM00039371 |
Trace |
4.2.1 |
|
ETB device definitions not present for OMAP3730 |
In attempting to enable ETB trace on OMAP3730 there is an error "Channel
error: Trace Channel Error: ETB device definitions cann... |
|