ARM C/C++ Code Generation Tools v18.1.8.LTS Release Notes
Table of Contents
1 Support Information
1.1 List of Resolved and Known Defects
Resolved defects
| ID | Summary |
|---|---|
| CODEGEN-7227 | Compiler incorrectly optimizes unsigned loop counter which wraps around |
| CODEGEN-7146 | Compiler loses conversion to size_t in length argument to memcpy |
| CODEGEN-7011 | Compiler intermittently fails with INTERNAL ERROR: opt2000 experienced a segmentation fault |
| CODEGEN-6914 | Enum type with no enumerators fails to emit DW_AT_byte_size, crashes CCS |
| CODEGEN-6909 | Compiler mistakenly reorders and combines conditional definitions of volatile objects |
| CODEGEN-6866 | Compiler computes wrong offset for structure member, causing CCS to display it incorrectly |
| CODEGEN-6783 | Ensure C std headers do not issue MISRA warnings |
| CODEGEN-6757 | Use of C++ lambda causes Dwarf debug information to be incorrect, and prevents debugging the code |
| CODEGEN-6710 | MOVT/MOVW without # on constant causes assembler crash INTERNAL ERROR!: failed to locate symbol for relocation entry at offset |
| CODEGEN-6690 | Stack usage incorrect on many hand-coded assembly library functions |
Open defects
| ID | Summary |
|---|---|
| CODEGEN-6509 | Compiler error: no instance of function template matches the argument list |
| CODEGEN-6070 | Erroneous “redeclared with incompatible type” involving two tagless structs with same form |
| CODEGEN-5179 | When a symbol is remapped, DW_TAG_TI_branch/DW_AT_name is not updated |
| CODEGEN-5078 | Simple syntax error causes assembler to fail with INTERNAL ERROR |
| CODEGEN-4985 | Typo on ULP Advisor message |
| CODEGEN-4943 | MISRA 12.2 is incorrectly issued when one variable is used multiple times as an array index in the same expression |
| CODEGEN-4934 | Incorrect issue MISRA diagnostic 10.5: If the bitwise operators ~ and << are applied |
| CODEGEN-4789 | Compiler incorrectly issues MISRA diagnostic 12.7 Bitwise operators shall not be applied to operands whose underlying type is signed |
| CODEGEN-4712 | No MISRA 10.1 and 10.6 diagnostics issued on initializations |
| CODEGEN-4346 | MISRA 19.4 error fails to identify itself as MISRA diagnostic when problem is on the command line |
| CODEGEN-4304 | C++ feature causes runtime failure on unaligned access on ARM9 |
| CODEGEN-4298 | Internal error when passing a temporary array of objects |
| CODEGEN-4297 | Cannot take the address of std::ctype<char>::table_size |
| CODEGEN-4296 | Undefined symbol isblank with -g or -ooff |
| CODEGEN-4290 | wstring runtime failure - likely bug in swprintf |
| CODEGEN-4281 | Unexpected type returned by bitset [] operator |
| CODEGEN-4276 | std::multimap::clear is not noexcept |
| CODEGEN-4275 | std::num_get does not parse floating-point strings correctly |
| CODEGEN-4259 | noexcept(typeid(d)) runtime fail on polymorphic class type |
| CODEGEN-4258 | deeply nested lambda functions hang the codegen |
| CODEGEN-4250 | regex_constants::ECMAScript not expected to be 0 |
| CODEGEN-4248 | armcl allows non-default arguments to be specified after default arguments |
| CODEGEN-4247 | Internal error when assigning default arguments to a parameter pack |
| CODEGEN-4246 | armcl allows illegal attribute in friend declarations |
| CODEGEN-4245 | Multiple non-variables may be declared using auto or decltype(auto) |
| CODEGEN-4244 | armcl errors on legal constexpr constructor call |
| CODEGEN-4234 | No error generated for lambda-expression in default argument cannot capture any entity. |
| CODEGEN-4228 | armcl fails to flag an inconsistent use of alignas between a declaration and definition of an object |
| CODEGEN-4203 | Parser errors on empty enum declaration |
| CODEGEN-4158 | TI compiler does not emit clang error: constexpr function never produces a constant expression |
| CODEGEN-4157 | error with using constexpr for return from end() with empty std::initializer_list |
| CODEGEN-4132 | cannot find matching “==” operator definition |
| CODEGEN-4124 | Failure to defer access control checks |
| CODEGEN-4122 | decltype cannot be used as a destructor name |
| CODEGEN-4119 | user-supplied allocator function is not called |
| CODEGEN-4105 | cannot find definition of “>=” operator |
| CODEGEN-4099 | Composing operations for valarray may fail to compile |
| CODEGEN-4091 | Incomplete class type when using various members of <iterator> |
| CODEGEN-4090 | Unimplemented core issue 475: std::uncaught_exception is not true when constructing the thrown object |
| CODEGEN-4084 | assembler errors with bogus .iendfunc asm directive when using –c_src_interlist |
| CODEGEN-4076 | Exception propagating out of noexcept function does not call std::terminate |
| CODEGEN-4072 | Unimplemented core issue 1769: Catching a thrown derived class by reference to base clas |
| CODEGEN-4071 | <regex> never throws error_ctype |
| CODEGEN-4069 | std::linear_congruential_engine doesn't support 8-bit results |
| CODEGEN-4058 | std::function<T>::target_type() should return typeid(void) if target is empty |
| CODEGEN-4050 | shared_ptr::get_deleter() should return the original deleter class without copying |
| CODEGEN-4044 | libcxx istreambuf_iterator points to end of string instead of character past match |
| CODEGEN-4035 | Compiler allows constant subtraction between pointers to different objects |
| CODEGEN-4032 | wofstream << operator unexpected termination |
| CODEGEN-4026 | Non-standard partial ordering of variadic template partial specialization |
| CODEGEN-4015 | Access of const static member through pointer is not a constant expression. |
| CODEGEN-4002 | Undefined behavior on lambda capturing constexpr by reference |
| CODEGEN-4001 | Unimplemented core issue 588: Unqualified name lookup examines dependent base class |
| CODEGEN-4000 | Core 1601: Overload resolution for enum with fixed type |
| CODEGEN-3999 | Unimplemented core issue 1374: Conversion sequence ranks qualification before reference binding |
| CODEGEN-3998 | Unimplemented core issue 1951: cv-qualified void and scalar types are not literal types |
| CODEGEN-3993 | Constant initialiation may take place before dynamic initialization |
| CODEGEN-3991 | We do not issue diagnostics if an allocation function throws a non bad_alloc exception |
| CODEGEN-3966 | slice_array assignment failures |
| CODEGEN-3965 | Invalid conversion on static_cast from T1 to rvalue reference of T2 |
| CODEGEN-3964 | Unimplemented core issue 1467: Overloads and initializations with single-element initializer_list |
| CODEGEN-3963 | Unimplemented core issue 591: Name lookup in dependent base class that is also the current instantiation |
| CODEGEN-3962 | Core Issue 1804 unimplemented: friend declaration does not apply to class template specializations |
| CODEGEN-3961 | Pack expansion in template parameter list fails |
| CODEGEN-3959 | std::reference_wrapper doesn't define argument_type for classes containing a typedef member named argument_type |
| CODEGEN-3954 | Problem with std::swap and <tuple> |
| CODEGEN-3953 | scoped_allocator_adaptor can't be explicitly instantiated with two arguments |
| CODEGEN-3951 | Spurious error on bypassing initialization of trivially constructible objects |
| CODEGEN-3948 | Spurious syntax error on alignas in alias declaration |
| CODEGEN-3947 | Spurious error on unevaluated use of undefined constexpr function |
| CODEGEN-3946 | Spurious error on global qualifier of struct template |
| CODEGEN-3944 | Raw string d-char-sequence isn't supported |
| CODEGEN-3941 | operator<<(std::basic_ostream<K,T>&, const std::error_code&) is not defined in system_error |
| CODEGEN-3938 | std::rethrow_if_nested does not have standard signature |
| CODEGEN-3937 | nested_exception::rethrow_nested() not supported |
| CODEGEN-3916 | C++ header file cuchar is not provided in libc++ |
| CODEGEN-1499 | #pragma LOCATION and palign do not work together |
| CODEGEN-1498 | Automatic library build fails when an exact library name is used |
| CODEGEN-1495 | Compiler and assembler disagree on format for IT instruction |
| CODEGEN-1484 | The armhex command does not handle spaces in the name of the output binary |
| CODEGEN-1458 | Consider splitting up unified_locale.cpp to save code space |
| CODEGEN-1445 | Compiler inserts unnecessary register copy |
| CODEGEN-1101 | When the imaginary part of z is INFINITY, cprojf(z) is NOT equivalent to INFINITY + I * copysign(0.0, cimagf(z)) |
| CODEGEN-1059 | Compiler does not respect partial overrides in C99 designated initializers |
| CODEGEN-1026 | Disable diagnostic 1558 (–float_operations_allowed diagnostic) in standard header files |
| CODEGEN-989 | Should accept “LDRD R8,[R1]” in Thumb-2 mode |
| CODEGEN-975 | Missing half-precision float conversion functions |
| CODEGEN-974 | Missing __aeabi_read_tp |
| CODEGEN-972 | Missing AEABI_COMPATIBILITY_MODE link-time constants |
| CODEGEN-967 | Assembler accepts but mistranslates BLLT in v7 thumb mode |
| CODEGEN-966 | Should allow “ADD R0, R1, #0xfff” for v6m0 |
| CODEGEN-962 | Should accept 2-operand SUB SP in Thumb1/UAL mode |
| CODEGEN-927 | Should accept 2-operand add in ARM mode |
| CODEGEN-890 | The .label assembler directive should not be accepted when assembling for ELF. |
| CODEGEN-830 | __aeabi_dcmpun returns 1 for Inf and -Inf |
| CODEGEN-793 | Ill advised enum scalar usage gets MISRA diagnostic, but similar usage of enum array does not |
| CODEGEN-792 | Array that is correctly initialized erroneously gets a MISRA diagnostic about size not being specified |
| CODEGEN-753 | Warning generated when using __curpc intrinsic on Thumb 2 |
| CODEGEN-662 | Double constant incorrectly converted to float changes result slightly |
| CODEGEN-578 | MISRA 12.8 and MISRA 10.5 false positives |
| CODEGEN-573 | Cortex-M0 library lacks uread4, etc. |
| CODEGEN-322 | Structure is not initialized correctly when using -o2 or -o3 optimization |
| CODEGEN-316 | The _ssat16 intrinsic allows literals in the range of 0-31, but the SSAT16 instruction only accepts values from 1-16 |
| CODEGEN-315 | _ssatl intrinsic allows 3rd argument to be 0 resulting in an assembler error. |
| CODEGEN-299 | ARM assembler does not issue a warning for PC-relative loads when –embedded_constants=off |
| CODEGEN-237 | Linker outputting wrong build attribute name for EABI TAG_VFP_arch on ARM targets |
| CODEGEN-235 | Section relative ELF symbol values in partially linking object files should hold the section offset for the symbol |
| CODEGEN-104 | Linker gives misleading warning when dot expressions used in SECTION directive for .stack section |
| CODEGEN-63 | DWARF does not correctly represent variables stored in register pairs |
| CODEGEN-56 | Forward reference in .space generates an internal error |
| CODEGEN-30 | Compilers on PC will not work without TMP set |
1.2 Compiler Wiki
A Wiki has been established to assist developers in using TI Embedded Processor Software and Tools. Developers are encouraged to read and contribute to the articles. Registered users can update missing or incorrect information. There is a large section of compiler-related material. Please visit:
https://processors.wiki.ti.com/index.php?title=Category:Compiler
1.3 Compiler Documentation
The “TI ARM Optimizing Compiler User’s Guide” and the “TI ARM Assembly Language User’s Guide” can be downloaded from:
https://www.ti.com/tool/ARM-CGT
1.4 TI E2E Community
Questions concerning TI Code Generation Tools can be posted to the TI E2E Community forums. The Code Composer Studio support forum can be found at:
https://e2e.ti.com/support/tools/ccs/f/81
1.5 Defect Tracking Database
The Code Generation Tools Defect Database can be searched at:
1.6 Long Term Support release
The ARM CGT v18.1.0.LTS release is a long term support (LTS) release. This release will be supported for roughly 2 years with periodic bug fix updates.
2 C++ 2014 support
As of v18.1.0.LTS, the compiler uses the C++14 version of the C++ standard. Previously, C++03 was used. See the C++ Standard ISO/IEC 14882:2014. For a description of unsupported C++14 features, see Section 5.2 of the “TI ARM Optimizing Compiler User’s Guide”.
The move to C++14 will break ABI compatibility with previous C++ RTS releases. Attempting to link old C++ object code with the new RTS will result in a link-time error. Suppressing this error will likely result in undefined symbols or undefined behavior during execution.
C ABI compatibility will not be affected by this change.
In most cases, recompiling old source code with the new RTS should be safe. However, due to the changes made in the language, some constructs will result in syntax errors. Some common issues include:
- Macro expansion immediately adjacent to string literals may fail due to the inclusion of new string literals and literal suffixes. Ex: u8“def” will fail to compile if ‘u8’ is a macro “def”_x will fail to compile if ’_x’ is a macro
- New keywords: alignas, alignof, char16_t, char32_t, constexpr, decltype, noexcept, nullptr, static_assert, and thread_local
- The auto keyword has been repurposed and is no longer a valid storage class specifier. Similarly, the register keyword has been deprecated and will be removed in the future.
A full list can be found in Appendix C, section 2 of the C++14 standard.
3 C++ ABI Compatibility
v17.9.0.STS contains the first planned updates in preparation for the support of C++14 (International Standard ISO/IEC 14882:2014(E)). As part of this update, it is necessary to make changes which might cause errors when building C++ projects containing C++ object files compiled with older versions of the compiler.
These errors will usually include linktime errors involving undefined symbols. If you see undefined symbol errors during a link, pass the “–no_demangle” option to the compiler. If the undefined symbol’s name starts with _Z or _ZVT, then it’s possible that there is a C++ object file or library built with an older version of the tools being used. These will need to be compiled with the v18.1.0.LTS tools to work properly.
4 Support for ARM C Language Extensions (ACLE)
Beginning with the ARM CGT v17.9.0.STS release, support for ARM C Language Extensions (ACLE) as specified in the ACLE Release 2.0 document (Document number: IHI 0053C, Date of Issue: 09/05/2014) has been added for the applicable processor variants that are supported in the ARM CGT. This includes support for new ACLE attributes, intrinsics, and pre-defined symbols as detailed in the sub-sections below.
4.1 ACLE Attributes
In addition to the attributes described in the ACLE specification that the ARM CGT already supports (i.e. aligned, alias, common, nocommon, packed, section, visibility, and weak), the ARM CGT v17.9.0.STS release adds support for the “target” attribute as follows:
attribute((target(“arm”))) void myfunc()
when applied to a function, will force the generation of ARM state code.
This attribute will be interpreted as if the user had specified the
already supported "#pragma CODE_STATE(myfunc, 32)" just in front of the
definition of the function definition of "myfunc".
attribute((target(“thumb”))) void myfunc()
when applied to a function, will force the generation of THUMB state code.
This attribute will be interpreted as if the user had specified the
already supported "#pragma CODE_STATE(myfunc, 16)" just in front of the
definition of the function definition of "myfunc".
The ARM CGT does not support the “pcs” ACLE attribute.
4.2 ACLE Intrinsics
A new header file, arm_acle.h, has been added to the ARM CGT include subdirectory which provides declarations and/or declarations of all of the ACLE intrinsics that are now supported beginning with the v17.9.0.STS release.
The majority of ACLE intrinsics that are newly supported in this release are implemented by already supported intrinsics that may have a slightly different name. For example, the ACLE “__smulbb" intrinsic is implemented in terms of the already supported “_smulbb" intrinsic as follows:
int32_t __BUILTIN _smulbb(int32_t x, int32_t y); #define __smulbb _smulbb
The only difference being that the ACLE “__smulbb" intrinsic name has a prefix of two underscores as opposed to the name of the already supported “_smulbb" intrinsic name which has a prefix of 1 underscore.
The ARM CGT v17.9.0.STS release does not support all of the ACLE intrinsics that are included in the ACLE specification. For example, the __cls, __clsl, and __clsll ACLE intrinsics are not supported since the CLS instruction is not available on the Cortex-M or Cortex-R architectures.
Please see the arm_acle.h file for more details about exactly which ACLE intrinsics are supported and which are not. Where applicable, the declarations of ACLE intrinsics that are not supported are enclosed in comments along with a brief explanation of why the intrinsic is not supported and a reference to the appropriate section in the ACLE specification where the intrinsic is described.
4.3 ACLE Pre-Defined Symbols
The ARM CGT v17.9.0.STS compiler will now define the following ACLE pre-defined symbols:
__ARM_ACLE - defined to ‘200’ for all Cortex-M and Cortex-R processor variants supported by the ARM CGT, not defined otherwise
__ARM_ARCH - indicates which ARM architecture the compiler is generating code for:
value selected processor
----- ------------------
'4' -mv4
'5' -mv5e
'6' -mv6, -mv6m0
'7' -mv7a8, -mv7m3, -mv7m4, -mv7r4, -mv7r5
__ARM_32BIT_STATE - defined to 1 if compiler is generating code for an ARM 32-bit processor variant, otherwise undefined
__ARM_ARCH_ISA_ARM - defined to 1 if compiler is generating code for a processor variant that supports the ARM instruction set; otherwise undefined (not defined when compiling for Cortex-M processor, for example)
__ARM_ARCH_ISA_THUMB - defined to 1 if compiler is generating code for a processor variant that supports the THUMB-1 instruction set; defined to 2 if compiler is generating code for a processor variant that supports the THUMB-2 instruction set; otherwise undefined
__ARM_BIG_ENDIAN - matches endian-ness specified with compiler command-line: 1 (big-endian; default), 0 (little-endian; -me option)
__ARM_FEATURE_CLZ - defined to 1 if compiler is generating code for a processor variant that supports the CLZ instruction; otherwise undefined
__ARM_FEATURE_DSP - defined to 1 if compiler is generating code for a Cortex-M or Cortex-R processor that supports DSP instructions/intrinsics; otherwise undefined
__ARM_FEATURE_SAT - defined to 1 if compiler is generating code for a processor variant tha supports SSAT/USAT instructions/intrinsics; otherwise undefined
__ARM_FEATURE_SIMD32 - defined to 1 if compiler is generating code for a processor variant that supports all SIMD instructions/intrinsics; otherwise undefined
__ARM_FEATURE_UNALIGNED - defined to 1 if compiler is generating code for a processor variant that supports unaligned access to memory; otherwise undefined
__ARM_PCS - defined to 1 if the compiler can assumes that the default procesude calling standard for a translation unit conforms to the “base procedure call standard” as prescribed in the ARM Architecture Procedure Call Standard specification; otherwise undefined
__ARM_SIZEOF_MINIMAL_ENUM - smallest possible enum type size (1 byte for ‘packed’, 4 bytes for ‘int’ (mirroring the –enum_type=[packed|int] option where packed is the default)
__ARM_SIZEOF_WCHAR_T - size of wchar_t type: 16- (default) or 32-bits
__ARM_FP - defined to a non-zero value if the compiler can assume that floating-point hardware support is available when compiling a translation unit. The value will be a combination of:
bit value precision
--- ----- ---------
1 0x2 16-bit
2 0x4 32-bit
3 0x8 64-bit
For example, if --float_support=fpv4spd16 is
selected, then __ARM_FP will have a value of
0x6 since fpv4spd16 supports 32-bit and 16-bit
floating-point hardware.
If no floating-point hardware support is enabled,
then __ARM_FP will be undefined.
__ARM_FP16_ARGS - defined to 1 if a 16-bit float type can be used for an argument and/or result; otherwise undefined
__ARM_FP16_FORMAT_IEEE - defined to 1 if the IEEE format for 16-bit floating-point (according to IEEE 754-2008 standard) is used; otherwise undefined
__ARM_PCS_VFP - defined to 1 if the default procedure calling convention is to pass floating-point arguments / return values in hardware floating-point registers
The ARM CGT v17.9.0.STS release does not support all of the ACLE pre-defined symbols that are included in the ACLE specification. For example, the __ARM_FEATURE_CRYPTO pre-defined symbol is associated with support for CRYPTO instructions which are not supported on any of the processor variants that the ARM CGT v17.9.0.STS release supports. If an ACLE pre-defined symbol in the ACLE specification is not included in the above list, then it will not be defined by the ARM CGT compiler.
5 Improved stack usage with inline functions
The new compiler improves stack usage by sharing aggregate data originally defined in inline functions. Example:
struct ARGS { int f1,f2,f3,f4,f5; };
static inline void func1() { struct ARGS a = {1, 2, 3, 4, 5}; foo(&a); }
static inline void func2() { struct ARGS b = {1, 2, 3, 4, 5}; foo(&b); }
void func3() { func1(); func2(); }
In previous compilers, if func1 and func2 are inlined, the structs a and b would not share the same stack location. This version of the compiler will now share stack memory for local aggregates defined in inline functions.