ARM C/C++ CODE GENERATION TOOLS 18.1.3.LTS Release Notes July 2018 ================================================================================ Contents ================================================================================ 1) Support Information 2) New Features 2.1) C++14 support * Features Included from v17.9.0.STS: 2.2) C++ ABI Compatibility 2.3) Support for ARM C Language Extensions (ACLE) * Features Included from v16.12.0.STS: 2.4) Improved stack usage with inline functions ------------------------------------------------------------------------------- 1. Support Information ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- 1.1) List of Fixed and Known Defects ------------------------------------------------------------------------------- As of the 16.12.0.STS release, the DefectHistory.txt file has been replaced with the two files Open_defects.html and Closed_defects.html. For open bugs, a status of Open or Accepted means that the bug has not been examined yet, whereas a status of Planned means that an evaluation or fix is in progress. ------------------------------------------------------------------------------- 1.2) Compiler Wiki ------------------------------------------------------------------------------- A Wiki has been established to assist developers in using TI Embedded Processor Software and Tools. Developers are encouraged to read and contribute to the articles. Registered users can update missing or incorrect information. There is a large section of compiler-related material. Please visit: http://processors.wiki.ti.com/index.php?title=Category:Compiler ------------------------------------------------------------------------------- 1.3) Compiler Documentation Errata ------------------------------------------------------------------------------- Errata for the "TI ARM Optimizing Compiler User's Guide" and the "TI ARM Assembly Language User's Guide" is available online at the Texas Instruments Embedded Processors CG Wiki: http://processors.wiki.ti.com/index.php?title=Category:Compiler under the 'Compiler Documentation Errata' link. ------------------------------------------------------------------------------- 1.4) TI E2E Community ------------------------------------------------------------------------------- Questions concerning TI Code Generation Tools can be posted to the TI E2E Community forums. The "Development Tools" forum can be found at: http://e2e.ti.com/support/development_tools/f/default.aspx ------------------------------------------------------------------------------- 1.5) Defect Tracking Database ------------------------------------------------------------------------------- Compiler defect reports can be tracked at the Development Tools bug database, SDOWP. The log in page for SDOWP, as well as a link to create an account with the defect tracking database is found at: https://cqweb.ext.ti.com/pages/SDO-Web.html A my.ti.com account is required to access this page. To find an issue in SDOWP, enter your bug id in the "Find Record ID" box once logged in. To find tables of all compiler issues click the queries under the folder: "Public Queries" -> "Development Tools" -> "TI C-C++ Compiler" With your SDOWP account you can save your own queries in your "Personal Queries" folder. ------------------------------------------------------------------------------- 1.6) Long Term Support release ------------------------------------------------------------------------------- The ARM CGT v18.1.0.LTS release is a long term support (LTS) release. This release will be supported for roughly 2 years with periodic bug fix updates. ------------------------------------------------------------------------------- 2. New Features ------------------------------------------------------------------------------- -------------------------------------------------------------------------------- 2.1) C++ 2014 RTS support -------------------------------------------------------------------------------- As of v18.1.0.LTS, the compiler uses the C++14 version of the C++ standard. Previously, C++03 was used. See the C++ Standard ISO/IEC 14882:2014. For a description of unsupported C++14 features, see Section 5.2 of the "TI ARM Optimizing Compiler User's Guide". The move to C++14 will break ABI compatibility with previous C++ RTS releases. Attempting to link old C++ object code with the new RTS will result in a link-time error. Suppressing this error will likely result in undefined symbols or undefined behavior during execution. C ABI compatibility will not be affected by this change. In most cases, recompiling old source code with the new RTS should be safe. However, due to the changes made in the language, some constructs will result in syntax errors. Some common issues include: - Macro expansion immediately adjacent to string literals may fail due to the inclusion of new string literals and literal suffixes. Ex: u8"def" will fail to compile if 'u8' is a macro "def"_x will fail to compile if '_x' is a macro - New keywords: alignas, alignof, char16_t, char32_t, constexpr, decltype, noexcept, nullptr, static_assert, and thread_local - The auto keyword has been repurposed and is no longer a valid storage class specifier. Similarly, the register keyword has been deprecated and will be removed in the future. A full list can be found in Appendix C, section 2 of the C++14 standard. ------------------------------------------------------------------------------- 2.2) C++ ABI Compatibility ------------------------------------------------------------------------------- v17.9.0.STS contains the first planned updates in preparation for the support of C++14 (International Standard ISO/IEC 14882:2014(E)). As part of this update, it is necessary to make changes which might cause errors when building C++ projects containing C++ object files compiled with older versions of the compiler. These errors will usually include linktime errors involving undefined symbols. If you see undefined symbol errors during a link, pass the "--no_demangle" option to the compiler. If the undefined symbol's name starts with _Z or _ZVT, then it's possible that there is a C++ object file or library built with an older version of the tools being used. These will need to be compiled with the v18.1.0.LTS tools to work properly. ------------------------------------------------------------------------------- 2.3) Support for ARM C Language Extensions (ACLE) ------------------------------------------------------------------------------- Beginning with the ARM CGT v17.9.0.STS release, support for ARM C Language Extensions (ACLE) as specified in the ACLE Release 2.0 document (Document number: IHI 0053C, Date of Issue: 09/05/2014) has been added for the applicable processor variants that are supported in the ARM CGT. This includes support for new ACLE attributes, intrinsics, and pre-defined symbols as detailed in the sub-sections below. 2.2.1) ACLE Attributes ---------------------- In addition to the attributes described in the ACLE specification that the ARM CGT already supports (i.e. aligned, alias, common, nocommon, packed, section, visibility, and weak), the ARM CGT v17.9.0.STS release adds support for the "target" attribute as follows: __attribute__((target("arm"))) void myfunc() when applied to a function, will force the generation of ARM state code. This attribute will be interpreted as if the user had specified the already supported "#pragma CODE_STATE(myfunc, 32)" just in front of the definition of the function definition of "myfunc". __attribute__((target("thumb"))) void myfunc() when applied to a function, will force the generation of THUMB state code. This attribute will be interpreted as if the user had specified the already supported "#pragma CODE_STATE(myfunc, 16)" just in front of the definition of the function definition of "myfunc". The ARM CGT does not support the "pcs" ACLE attribute. 2.2.2) ACLE Intrinsics ---------------------- A new header file, arm_acle.h, has been added to the ARM CGT include subdirectory which provides declarations and/or declarations of all of the ACLE intrinsics that are now supported beginning with the v17.9.0.STS release. The majority of ACLE intrinsics that are newly supported in this release are implemented by already supported intrinsics that may have a slightly different name. For example, the ACLE "__smulbb" intrinsic is implemented in terms of the already supported "_smulbb" intrinsic as follows: int32_t __BUILTIN _smulbb(int32_t x, int32_t y); #define __smulbb _smulbb The only difference being that the ACLE "__smulbb" intrinsic name has a prefix of two underscores as opposed to the name of the already supported "_smulbb" intrinsic name which has a prefix of 1 underscore. The ARM CGT v17.9.0.STS release does not support all of the ACLE intrinsics that are included in the ACLE specification. For example, the __cls, __clsl, and __clsll ACLE intrinsics are not supported since the CLS instruction is not available on the Cortex-M or Cortex-R architectures. Please see the arm_acle.h file for more details about exactly which ACLE intrinsics are supported and which are not. Where applicable, the declarations of ACLE intrinsics that are not supported are enclosed in comments along with a brief explanation of why the intrinsic is not supported and a reference to the appropriate section in the ACLE specification where the intrinsic is described. 2.2.3) ACLE Pre-Defined Symbols ------------------------------- The ARM CGT v17.9.0.STS compiler will now define the following ACLE pre-defined symbols: __ARM_ACLE - defined to '200' for all Cortex-M and Cortex-R processor variants supported by the ARM CGT, not defined otherwise __ARM_ARCH - indicates which ARM architecture the compiler is generating code for: value selected processor ----- ------------------ '4' -mv4 '5' -mv5e '6' -mv6, -mv6m0 '7' -mv7a8, -mv7m3, -mv7m4, -mv7r4, -mv7r5 __ARM_32BIT_STATE - defined to 1 if compiler is generating code for an ARM 32-bit processor variant, otherwise undefined __ARM_ARCH_ISA_ARM - defined to 1 if compiler is generating code for a processor variant that supports the ARM instruction set; otherwise undefined (not defined when compiling for Cortex-M processor, for example) __ARM_ARCH_ISA_THUMB - defined to 1 if compiler is generating code for a processor variant that supports the THUMB-1 instruction set; defined to 2 if compiler is generating code for a processor variant that supports the THUMB-2 instruction set; otherwise undefined __ARM_BIG_ENDIAN - matches endian-ness specified with compiler command-line: 1 (big-endian; default), 0 (little-endian; -me option) __ARM_FEATURE_CLZ - defined to 1 if compiler is generating code for a processor variant that supports the CLZ instruction; otherwise undefined __ARM_FEATURE_DSP - defined to 1 if compiler is generating code for a Cortex-M or Cortex-R processor that supports DSP instructions/intrinsics; otherwise undefined __ARM_FEATURE_SAT - defined to 1 if compiler is generating code for a processor variant tha supports SSAT/USAT instructions/intrinsics; otherwise undefined __ARM_FEATURE_SIMD32 - defined to 1 if compiler is generating code for a processor variant that supports all SIMD instructions/intrinsics; otherwise undefined __ARM_FEATURE_UNALIGNED - defined to 1 if compiler is generating code for a processor variant that supports unaligned access to memory; otherwise undefined __ARM_PCS - defined to 1 if the compiler can assumes that the default procesude calling standard for a translation unit conforms to the "base procedure call standard" as prescribed in the ARM Architecture Procedure Call Standard specification; otherwise undefined __ARM_SIZEOF_MINIMAL_ENUM - smallest possible enum type size (1 byte for 'packed', 4 bytes for 'int' (mirroring the --enum_type=[packed|int] option where packed is the default) __ARM_SIZEOF_WCHAR_T - size of wchar_t type: 16- (default) or 32-bits __ARM_FP - defined to a non-zero value if the compiler can assume that floating-point hardware support is available when compiling a translation unit. The value will be a combination of: bit value precision --- ----- --------- 1 0x2 16-bit 2 0x4 32-bit 3 0x8 64-bit For example, if --float_support=fpv4spd16 is selected, then __ARM_FP will have a value of 0x6 since fpv4spd16 supports 32-bit and 16-bit floating-point hardware. If no floating-point hardware support is enabled, then __ARM_FP will be undefined. __ARM_FP16_ARGS - defined to 1 if a 16-bit float type can be used for an argument and/or result; otherwise undefined __ARM_FP16_FORMAT_IEEE - defined to 1 if the IEEE format for 16-bit floating-point (according to IEEE 754-2008 standard) is used; otherwise undefined __ARM_PCS_VFP - defined to 1 if the default procedure calling convention is to pass floating-point arguments / return values in hardware floating-point registers The ARM CGT v17.9.0.STS release does not support all of the ACLE pre-defined symbols that are included in the ACLE specification. For example, the __ARM_FEATURE_CRYPTO pre-defined symbol is associated with support for CRYPTO instructions which are not supported on any of the processor variants that the ARM CGT v17.9.0.STS release supports. If an ACLE pre-defined symbol in the ACLE specification is not included in the above list, then it will not be defined by the ARM CGT compiler. ------------------------------------------------------------------------------- 2.4) Improved stack usage with inline functions ------------------------------------------------------------------------------- The new compiler improves stack usage by sharing aggregate data originally defined in inline functions. Example: struct ARGS { int f1,f2,f3,f4,f5; }; static inline void func1() { struct ARGS a = {1, 2, 3, 4, 5}; foo(&a); } static inline void func2() { struct ARGS b = {1, 2, 3, 4, 5}; foo(&b); } void func3() { func1(); func2(); } In previous compilers, if func1 and func2 are inlined, the structs a and b would not share the same stack location. This version of the compiler will now share stack memory for local aggregates defined in inline functions.