Open Defects in Release

ID Summary State Reported In Release Target Release Workaround Release Notes
CODEGEN-4645 Assembler fails with INTERNAL ERROR!: <symbol name> defined differently in each pass Accepted PRU_2.3.0
SDSCM00050131 Local struct with non-constant initializer treated as static scope variable Accepted PRU_2.3.0
SDSCM00047244 C99 header file fenv.h not supported Accepted PRU_2.3.0
SDSCM00046695 Floating point addition rounding error Accepted PRU_2.3.0
SDSCM00046114 RTS float arithmetic functions rounding error Open PRU_2.3.0 The expression 1+DBL_EPSILON/2 should be rounded DOWN to 1.0 for only mode the TI compiler supports: "round to even".
SDSCM00040934 Structure is not initialized correctly when using -o2 or -o3 optimization Accepted PRU_2.3.0 The initialization will have to be done at run-time, through a __sti initialization routine. You can see this routine when compiling without optimization. To workaround the compiler removing this initialization routine, initialize the object at the beginning of main: Info2.mSize = ((unsigned)_end_isr_stack - (unsigned)_start_isr_stack);
SDSCM00018691 Linker gives misleading warning when dot expressions used in SECTION directive for .stack section Accepted PRU_2.3.0
SDSCM00014430 calloc doesn't check arguments to make sure the requested size is reasonable Accepted PRU_2.3.0
SDSCM00008543 Forward reference in .space generates an internal error Accepted PRU_2.3.0 none

Generated on Mon Jul 2 17:58:35 2018