Open Defects in Release

ID Summary State Reported In Release Target Release Workaround Release Notes
CODEGEN-1995 Pointer math addend incorrectly truncated to ptrdiff_t on MSP430 Planned MSP430_17.6.0.STS
SDSCM00052531 Incorrect value assigned to a forward reference of a symbol defined in terms of the section's PC ($) after jump expansion Open MSP430_17.6.0.STS Two workarounds are possible: 1) Use a label to get the value of the PC at a key location instead of "symbol .equ $" 2) Replace the jump that will be expanded with an already expanded form. In the example, the jump could be replaced with: JLO $+6 BR label1
CODEGEN-1295 MSP430 RTS rint() double routines failing for some inputs Open MSP430_17.6.0.STS Avoid using the rint() RTS routines with double arguments and instead use the corresponding rint() float routines. MSP430 RTS routines rint() rintl() lrint() lrintl() llrint() llrintl() failing for some inputs with double arguments.
SDSCM00051908 Print a more friendly message when using a lnk.cmd with too large memory Accepted MSP430_17.6.0.STS
SDSCM00050131 Local struct with non-constant initializer treated as static scope variable Accepted MSP430_17.6.0.STS
SDSCM00049284 Compiler misreports Misra warning 10.1 Accepted MSP430_17.6.0.STS
SDSCM00049280 Ill advised enum scalar usage gets MISRA diagnostic, but similar usage of enum array does not Open MSP430_17.6.0.STS
SDSCM00049278 Array that is correctly initialized erroneously gets a MISRA diagnostic about size not being specified Open MSP430_17.6.0.STS
SDSCM00047833 msp C++ cpp compiled with printf_support=minimal causes cout to output incorrect results Accepted MSP430_17.6.0.STS Instead either compile without --printf_support, or choose options nofloat or full.
SDSCM00046695 Floating point addition rounding error Accepted MSP430_17.6.0.STS
SDSCM00046115 MSP430 RTS float arithmetic functions do not round correctly Open MSP430_17.6.0.STS
SDSCM00046113 C2000 RTS float arithmetic functions do not round correctly Open MSP430_17.6.0.STS
SDSCM00044526 Compiler emits bogus DW_OP_reg16 for split argument Accepted MSP430_17.6.0.STS
SDSCM00040934 Structure is not initialized correctly when using -o2 or -o3 optimization Accepted MSP430_17.6.0.STS The initialization will have to be done at run-time, through a __sti initialization routine. You can see this routine when compiling without optimization. To workaround the compiler removing this initialization routine, initialize the object at the beginning of main: Info2.mSize = ((unsigned)_end_isr_stack - (unsigned)_start_isr_stack);
SDSCM00038293 Relocation overflows for BIT instruction using 20-bit pointer Accepted MSP430_17.6.0.STS
SDSCM00038178 Should forbid non-const objects larger than 64k in large model if --near_data=globals Accepted MSP430_17.6.0.STS
SDSCM00018691 Linker gives misleading warning when dot expressions used in SECTION directive for .stack section Accepted MSP430_17.6.0.STS
SDSCM00014430 calloc doesn't check arguments to make sure the requested size is reasonable Accepted MSP430_17.6.0.STS
SDSCM00008685 DWARF does not correctly represent variables stored in register pairs Accepted MSP430_17.6.0.STS Although 'var1' and 'var2' are shown to be in single registers, a debugger could determine that they are actually stored in register pairs by looking at the type of the variables: [00000113] DW_TAG_base_type DW_AT_name long long DW_AT_encoding 0x5 DW_AT_byte_size 0x8 The base type indicates that the size of the variables is 0x8 bytes. Since a single register can only store 0x4 bytes of information, it would take two registers to hold this values. On TI architectures, values stored in multiple registers are always stored in consecutive registers. Thus, the debugger would know that if the entire value could not fit in A4, the rest of the value must be in A5. A5 would contain the upper 32 bits of the value.
SDSCM00008652 pow(2,x) has fairly significant rounding error Accepted MSP430_17.6.0.STS Please describe the workaround for this problem.
SDSCM00008630 printf gives wrong value for pointer when its value is incremented Open MSP430_17.6.0.STS To get rid of the warning message modify the printf statement as follows: printf('0x%lx\n', 0x10000 + (t=(long int)&global_var)); This modified code executes correctly too.
SDSCM00008543 Forward reference in .space generates an internal error Accepted MSP430_17.6.0.STS none
SDSCM00008465 Language Conformance: crash because of void pointer dereference Accepted MSP430_17.6.0.STS Please describe the workaround for this problem.
SDSCM00008248 Compilers on PC will not work without TMP set Accepted MSP430_17.6.0.STS Set the TMP environment variable, even if just set to . (current directory)

Generated on Tue Jun 13 13:59:57 2017