C6000 C/C++ CODE GENERATION TOOLS 8.0.1 January 2015 Defect History ------------------------------------------------------------------------------- Table of Contents ------------------------------------------------------------------------------- 1. Defects fixed in C6000 Code Generation Tools release 8.0.1 2. Defects fixed in C6000 Code Generation Tools release 8.0.0 3. Defects fixed in C6000 Code Generation Tools release 8.0.0B4 4. Defects fixed in C6000 Code Generation Tools release 8.0.0B3 5. Defects fixed in C6000 Code Generation Tools release 8.0.0B2 6. Defects fixed in C6000 Code Generation Tools release 8.0.0B1 7. Current Known Issues =============================================================================== 1. Defects fixed in C6000 Code Generation Tools release 8.0.1 =============================================================================== The following 19 defects were fixed in C6000 Code Generation Tools release 8.0.1, released January 2015. ------------------------------------------------------------------------------- FIXED SDSCM00050051 ------------------------------------------------------------------------------- Summary : Table driven exception handling code does not check for malloc returning NULL Fixed in : 8.0.1 Severity : S2 - Major Affected Component : Runtime Support Libraries (RTS) Release Notes: In programs with extremely small .sysmem, one helper function for C++ exception handling would incorrectly handle a failure to allocate the global state for C++ exception handling. Later, if a C++ exception was thrown, the program would write to memory locations near 0 and potentially crash in a confusing manner. The program ought to have aborted when the global state could not be allocated. Defect occurs in C6000 Compiler versions: 7.0.0B1 - 7.0.5, 7.1.0B1 - 7.1.0B3, 7.2.0B1 - 7.2.12, 7.3.0B1 - 7.3.17, 7.4.0B1 - 7.4.11, 7.5.0B1, 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0 Workaround: Allocate more space to .sysmem ------------------------------------------------------------------------------- FIXED SDSCM00050505 ------------------------------------------------------------------------------- Summary : TDEH emergency buffer should be allocated on stack Fixed in : 8.0.1 Severity : S3 - Minor Affected Component : Runtime Support Libraries (RTS) Release Notes: The TI RTS has an "emergency buffer" functionality for C++ exception handling. The emergency buffer pre-allocates enough space for one std::bad_alloc object, so that if an allocation failure occurs in a low-memory situation, we can at least handle the bad_alloc exception gracefully. However, the C++ exception handling code tries to malloc a buffer to hold the register context for phase 1 of the stack unwinding pass. This means that in the very situation where we need the emergency buffer, we couldn't possibly malloc the register context. Thus, despite having been careful to create the emergency buffer, it can't work, because we'll invariably run out of memory trying to use it. Defect occurs in C6000 Compiler versions: 7.0.0B1 - 7.0.5, 7.1.0B1 - 7.1.0B3, 7.2.0B1 - 7.2.12, 7.3.0B1 - 7.3.17, 7.4.0B1 - 7.4.11, 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0 Workaround: Allocate more space to .sysmem ------------------------------------------------------------------------------- FIXED SDSCM00050603 ------------------------------------------------------------------------------- Summary : Variable write not happening in inlined CPP function Fixed in : 8.0.1 Severity : S2 - Major Affected Component : Optimizer Duplicate Defects : SDSCM00050941 Release Notes: In circumstances that are not well understood, structure fields may not be written correctly in the presence of complicated conditional code. Defect occurs in C6000 Compiler versions: 7.3.15 - 7.3.17, 7.4.7 - 7.4.10 Workaround: Compile at -o1 or -o0. ------------------------------------------------------------------------------- FIXED SDSCM00050725 ------------------------------------------------------------------------------- Summary : Hang/crash in partitioning for C674x Fixed in : 8.0.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: The INTERNAL ERROR is caused by an instruction scheduling partitioning failure. Workaround: Use -o0. ------------------------------------------------------------------------------- FIXED SDSCM00050764 ------------------------------------------------------------------------------- Summary : Bound function has incorrect address in DWARF debug info Fixed in : 8.0.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00049433 Release Notes: The TI compiler allows a function to be bound to a specific address, usually with "#pragma location". There was a bug in the way the TI assembler recorded the DWARF debugging information for a bound function that corrupted the DWARF debugging information. This would cause CCS to report "no source available" when stepping attempting to step into such a function. Defect occurs in C6000 Compiler versions: 7.4.0B1 - 7.4.11, 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0 Workaround: Set a breakpoint at the bound function and run to it, rather than attempting to step into it. ------------------------------------------------------------------------------- FIXED SDSCM00050814 ------------------------------------------------------------------------------- Summary : MSP430 compiler has an INTERNAL ERROR segmentation fault while parsing Fixed in : 8.0.1 Severity : S3 - Minor Affected Component : Parser Release Notes: The problem is that the MISRA checker finds what it thinks is a function call in std::string::_Tidy that uses a template parameter as the name of the function to call, which is clearly not correct, but there's no obvious fix. The initial consensus is that you're not supposed to use MISRA C to check C++ code, and that we should consider making it a fatal error to try to use -- check_misra with C++ code. Workaround: Do not use any form of --check_misra with C++ code. ------------------------------------------------------------------------------- FIXED SDSCM00050992 ------------------------------------------------------------------------------- Summary : The optimizer should not make a symbol an alias if it has either the location or code_section pragmas applied. Fixed in : 8.0.1 Severity : S2 - Major Affected Component : Compiler Consultant (ci) Release Notes: For a reason external to the expression of the program, the user relies on function X being at a particular address A. The only method the user has to do this is to put the function in its own special subsection and place it at A in the linker command file. Workaround: Available workarounds are to: 1. Reduce the optimization level to -o2. 2. If using a COFF abi, you can move the functions into separate files. 3. Add an __asm("NOP") to the function which will prevent an alias from being created. ------------------------------------------------------------------------------- FIXED SDSCM00050996 ------------------------------------------------------------------------------- Summary : The file misra.txt is not included with MSP430 and C6000 compiler tools installation Fixed in : 8.0.1 Severity : S3 - Minor Affected Component : C/C++ Compiler (cl) Release Notes: The file misra.txt, that contains the list of MISRA rules checked by the compiler, is not included with MSP430 and C6000 compiler tools installation. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00050997 ------------------------------------------------------------------------------- Summary : lnk6x does not pad code sections properly when user specifies non-zero fill value Fixed in : 8.0.1 Severity : S2 - Major Affected Component : ELF Linker Release Notes: When a non-zero fill value such as 0xefefefef, which itself is a legal encoding of a fetch packet header, is used then the linker may corrupt the encoding of the last execute packet in a section affected by the specified fill value when the linker uses the provided fill value to pad the end of a code section. Workaround: Problem can be worked around by using a more innocuous fill value. A 0x00000000 fill value is preferred since it encodes as a single cycle NOP in an output section containing executable code. ------------------------------------------------------------------------------- FIXED SDSCM00051088 ------------------------------------------------------------------------------- Summary : Optimizer crashes on conversion from integer 0 to float 4 Fixed in : 8.0.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: Some of the rules for widening a scalar to a vector are not correct. Workaround: Initialize with 0.0 instead of 0. ------------------------------------------------------------------------------- FIXED SDSCM00051097 ------------------------------------------------------------------------------- Summary : Output section splitting creates a zero-length section Fixed in : 8.0.1 Severity : S2 - Major Affected Component : ELF Linker Release Notes: In certain rare cases, the linker might split an output section into several output sections such that one of them had zero length. The linker really ought not to create split zero-length sections, as it doesn't improve the linkability of the program. This can only happen if one of the input sections is of zero length. Defect occurs in C6000 Compiler versions: 6.0.1B1 - 6.0.31, 6.1.0B1 - 6.1.23, 7.0.0B1 - 7.0.5, 7.1.0B1 - 7.1.0B3, 6.1.10.101, 7.2.0B1 - 7.2.12, 7.3.0B1 - 7.3.19, 7.4.0B1 - 7.4.11, 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0 Workaround: 1) Do not split the section in question. 2) Change the zero-length section so that it has at least one more byte. ------------------------------------------------------------------------------- FIXED SDSCM00051128 ------------------------------------------------------------------------------- Summary : Alias missed on address of local passed as function argument Fixed in : 8.0.1 Severity : S2 - Major Affected Component : Optimizer Duplicate Defects : SDSCM00047553 Release Notes: In certain cases, the compiler may produce incorrect code when a local variable whose address is passed to a function is then modified by the function, such as in the following example (where y is the affected local written by modf()): double f(double x) { double y = 0.; if(modf(x, &y) < 0.) return y - 1; else return y; } Workaround: Use the -ma (--aliased_variables) option. ------------------------------------------------------------------------------- FIXED SDSCM00051143 ------------------------------------------------------------------------------- Summary : Need compiler fix for SPLOOP-SPKERNEL-interrupt bug Fixed in : 8.0.1 Severity : S2 - Major Affected Component : Code Generator Duplicate Defects : SDSCM00051127 Release Notes: Preliminary! Subject to revision: Two defects on C674 and C66 ISA cores have been identified: (1) When: - On a C6600 core, and - An SPLOOP - with an instruction "A" that is a 3 or 4 cycle multicycle instruction - and instruction "A" is one of those instruction/unit combinations listed below - and instruction "A" writes a register two cycles lexically "after" the SPKERNEL instruction - and a single cycle instruction "B" in the post-epilog code uses the same write port as instruction "A" two cycles after the SPKERNEL instruction - and an interrupt occurs during SPLOOP execution The hardware can incorrectly detect a write port conflict and not write the results of the instruction "A" from the loop buffer. Note that some instructions appear in the S unit list and not the L unit list (marked with a *). This is correct. Note that all of these instruction/unit combinations are only on C66 CPUs. L unit DADDSP L unit DSUBSP L unit DINTSP L unit DINTSPU L unit DINTHSP L unit DINTHSPU L unit FADDSP L unit FSUBSP L unit DSPINTH L unit DSPINT L unit FADDDP L unit FSUBDP L unit DMVD S unit DADDSP S unit DSUBSP S unit DINTSP S unit DINTSPU S unit DINTHSP S unit DINTHSPU S unit FADDSP S unit FSUBSP S unit DSPINTH S unit DSPINT S unit FADDDP S unit FSUBDP S unit SPINT * Compiler currently does not generate SPINT on S for C66 (only on L) S unit INTSP * Compiler currently does not generate INTSP on S for C66 (only on L) S unit INTSPU * Compiler currently does not generate INTSPU on S for C66 (only on L) S unit DMVD (2) When: - On a C6740 or C6600 core, and - an SPLOOP - with an instruction "A" that reserves its functional unit for more than one cycle (list of instructions below) - and instruction "A"'s functional unit reservations occur one or two cycles lexically "after" the SPKERNEL instruction - and an instruction "B" lexically "after" the SPKERNEL instruction in the post-epilog code uses the same functional unit in the same cycle as the "A" instruction - and an interrupt occurs during SPLOOP execution the hardware can incorrectly throw an exception. CMPEQDP, CMPLTDP, CMPGTDP - reserves S1 or S2 for 2 cycles ADDDP, SUBDP - reserves L1, L2, S1, or S2 for 2 cycles MPYI, MPYID, MPYDP, - reserves M1 or M2 for 4 cycles MPYSPDP - reserves M1 or M2 for 2 cycles Defect occurs in C6000 Compiler versions: 7.3.0B1 - 7.3.19, 7.4.8 - 7.4.12, 8.0.0B1 - 8.0.0 Workaround: There are two possible workarounds: (1) Use --disable:sploop on those files whose loops are susceptible to the HW defects (see description of the silicon defects, above). (2) Disable interrupts around the inner loops that are susceptible to the HW defects with the intrinsics _disable_interrupts(), _enable_interrupts(), and _restore_interrupts(...). Please see section 7.5.9 of the TMS320C6000 Optimizing Compiler v7.6 User's Guide, spru187v for guidance on proper usage of these intrinsics. ------------------------------------------------------------------------------- FIXED SDSCM00051155 ------------------------------------------------------------------------------- Summary : Compiler does not define __TI_GNU_ATTRIBUTE_SUPPORT__ as the documentation describes Fixed in : 8.0.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: There is no method by which a customer can implement a compile time check on whether GCC extensions are supported. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00051234 ------------------------------------------------------------------------------- Summary : asm(" nop 5") changes position with another asm statement Fixed in : 8.0.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: When multiple, consecutive inline assembly statements are used together on C6000, they may potentially become reversed in order. This is caused by pipelining, so disabling the pipeliner (option -mu) should resolve the problem. Defect occurs in C6000 Compiler versions: 6.1.0B1 - 6.1.23, 7.0.0B1 - 7.0.5, 7.1.0B1 - 7.1.0B3, 6.1.10.101, 7.2.0B1 - 7.2.12, 7.3.0B1 - 7.3.19, 7.4.11 - 7.4.12, 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0 Workaround: Disable the pipeliner (option -mu) for files containing affected inline assembly statements. ------------------------------------------------------------------------------- FIXED SDSCM00051241 ------------------------------------------------------------------------------- Summary : Output section splitting creates a zero-length section Fixed in : 8.0.1 Severity : S2 - Major Affected Component : ELF Linker Release Notes: In certain rare cases, the linker might split an output section into several output sections such that one of them had zero length. The linker really ought not to create split zero-length sections, as it doesn't improve the linkability of the program. This can only happen if one of the input sections is of zero length. Defect occurs in C6000 Compiler versions: 6.0.1B1 - 6.0.31, 6.1.0B1 - 6.1.23, 7.0.0B1 - 7.0.5, 7.1.0B1 - 7.1.0B3, 6.1.10.101, 7.2.0B1 - 7.2.12, 7.3.0B1 - 7.3.19, 7.4.0B1 - 7.4.11, 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0 Workaround: 1) Do not split the section in question. 2) Change the zero-length section so that it has at least one more byte. ------------------------------------------------------------------------------- FIXED SDSCM00051273 ------------------------------------------------------------------------------- Summary : Performance degrades moving from v7.2.8 to v7.4.11 Fixed in : 8.0.1 Severity : S2 - Major Classification : Performance Affected Component : Optimizer Release Notes: A loop whose index variable has a type shorter than int may not achieve the expected performance. The known case is a downcounting loop using an unsigned-char variable i, which also uses the expression i-1 in the loop. The two instances of i-1 (for the decrement and the explicit use) in combination with the shorter-than-int type of i are apparently the two factors required to exhibit the problem. Defect occurs in C6000 Compiler versions: 7.3.0B1 - 7.3.20, 7.4.0B1 - 7.4.12, 8.0.0B1 - 8.0.0 Workaround: Use signed-int loop variables instead of types shorter than int. ------------------------------------------------------------------------------- FIXED SDSCM00051314 ------------------------------------------------------------------------------- Summary : Under --opt_level=3 compiler generated code ignores pointer check for NULL present in the source Fixed in : 8.0.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: A for-loop which includes at least two early exits, with one exit testing if a pointer is NULL and another testing if something reached by that pointer is NULL, may compile incorrectly and dereference a NULL pointer. The problem is specific to C6000. Defect occurs in C6000 Compiler versions: 6.0.1B1 - 6.0.31, 6.1.0B1 - 6.1.23, 7.0.0B1 - 7.0.5, 7.1.0B1 - 7.1.0B3, 6.1.10.100 - 6.1.10.101, 7.2.0B1 - 7.2.12, 7.3.0B1 - 7.3.20, 7.4.0B1 - 7.4.12, 7.5.0B1, 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0 Workaround: Compile at -o1 or -o0. ------------------------------------------------------------------------------- FIXED SDSCM00051346 ------------------------------------------------------------------------------- Summary : After unrolling loop, compiler ignores the iterations left over Fixed in : 8.0.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: A loop may unroll incorrectly, losing some iterations, if its known trip counts are divisible by a factor that is not evenly divisible by the unroll factor. In this case, the known trip counts are 143 and 165, which share the factor 11. The compiler unrolls by 2X, which makes the trip counts 71 and 82 (with one excess iteration), and erroneously determines that the new factor is 5. Defect occurs in C6000 Compiler versions: 6.1.0B2 - 6.1.23, 7.0.0B1 - 7.0.5, 7.1.0B1 - 7.1.0B3, 6.1.10.101, 7.2.0B1 - 7.2.12, 7.3.0B1 - 7.3.20, 7.4.0B1 - 7.4.12, 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0 Workaround: Use "#pragma UNROLL(1)" to inhibit unrolling, or compile with -o1 or -o0. In at least some cases, using -ms1 or greater, or -mf2 or less, will also inhibit unrolling in a way that avoids the problem. =============================================================================== 2. Defects fixed in C6000 Code Generation Tools release 8.0.0 =============================================================================== The following 4 defects were fixed in C6000 Code Generation Tools release 8.0.0, released September 2014. ------------------------------------------------------------------------------- FIXED SDSCM00050597 ------------------------------------------------------------------------------- Summary : Backward reference to array-in-struct may miss an alias Fixed in : 8.0.0 Severity : S2 - Major Affected Component : Optimizer Release Notes: Given a struct containing two adjacent fields that are arrays of the same type -- ie, "struct { short a[100]; short b[100]; }" -- a loop with accesses like "p->b[i] = p->b[i-1]" may compile incorrectly. Defect occurs in C6000 Compiler versions: 7.3.0B1 - 7.3.17, 7.4.0B1 - 7.4.10, 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0B4 Workaround: Insert a field between the two arrays that has a different element type, or move the troublesome array to the beginning of the struct, or compile at -o1 or -o0. The key details are adjacent array fields of the same element type and an array index with a negative offset. ------------------------------------------------------------------------------- FIXED SDSCM00050713 ------------------------------------------------------------------------------- Summary : Optimization level -o3 inlines weak function body Fixed in : 8.0.0 Severity : S2 - Major Affected Component : Optimizer Release Notes: A function declared as weak may be inlined, which is incorrect because the linker may override the weak definition later. Defect occurs in C6000 Compiler versions: 7.6.0B1 - 7.6.0, 8.0.0B1 - 8.0.0B4 Workaround: Use the FUNC_CANNOT_INLINE pragma to directly inhibit inlining. ------------------------------------------------------------------------------- FIXED SDSCM00050763 ------------------------------------------------------------------------------- Summary : Only the C6000 compiler accepts the GCC builtin function __builtin_constant_p Fixed in : 8.0.0 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: Error emitted that GNU __builtin_constant_p function not supported. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00050811 ------------------------------------------------------------------------------- Summary : Linker fails with INTERNAL ERROR: lnk2000 experienced an unhandled exception Fixed in : 8.0.0 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00050957, SDSCM00050799 Release Notes: This bug occurs in the C preprocessor used for reading linker command files, and results in an unhandled exception from the linker. If no C preprocessor directives are used, the bug should not occur. The --disable_pp option can be used to turn off the preprocessor if no directives are present. Defect occurs in C6000 Compiler versions: 7.4.9 - 7.4.10, 8.0.0B3 - 8.0.0 Workaround: Remove C preprocessor directives from linker command files. =============================================================================== 3. Defects fixed in C6000 Code Generation Tools release 8.0.0B4 =============================================================================== The following defect was fixed in C6000 Code Generation Tools release 8.0.0B4, released September 2014. ------------------------------------------------------------------------------- FIXED SDSCM00050677 ------------------------------------------------------------------------------- Summary : Using --opt_level=1 or higher causes compiler to fail with INTERNAL ERROR: >>>Register allocation failed Fixed in : 8.0.0B4 Severity : S2 - Major Affected Component : Code Generator Release Notes: Floating point registers are causing INTERNAL ERROR: register allocation failure. Workaround: Use _itof and _ftoi intrinsics =============================================================================== 4. Defects fixed in C6000 Code Generation Tools release 8.0.0B3 =============================================================================== The following defect was fixed in C6000 Code Generation Tools release 8.0.0B3, released August 2014. ------------------------------------------------------------------------------- FIXED SDSCM00050365 ------------------------------------------------------------------------------- Summary : openMP parser emit error message for #pragma omp critial (name) Fixed in : 8.0.0B3 Severity : S2 - Major Affected Component : Parser Release Notes: No Information Available; please see defect details. Workaround: pragma critical with a name is generating an error message when the name was not a variable declared in the compilation unit. Remove the name or use the name of a variable that is declared in the compilation unit. =============================================================================== 5. Defects fixed in C6000 Code Generation Tools release 8.0.0B2 =============================================================================== The following 3 defects were fixed in C6000 Code Generation Tools release 8.0.0B2, released July 2014. ------------------------------------------------------------------------------- FIXED SDSCM00050243 ------------------------------------------------------------------------------- Summary : Scary but harmless warning: FAILURE in mark_use_of_function_local_static() Fixed in : 8.0.0B2 Severity : S2 - Major Affected Component : Optimizer Release Notes: Compiling for C++ and using -pm or -o4 may produce a warning like FAILURE in mark_use_of_function_local_static() fname1: __sti fname2: __sti_ symbol: _$P$T62$2$1 This warning, despite its dramatic wording, is harmless. The compiler will build the program just as it should, and the warning does not indicate any change in behavior. It's a debugging message that should not have been visible outside the development team. Defect occurs in C6000 Compiler versions: 6.0.1B1 - 6.0.31, 6.1.0B1 - 6.1.23, 7.0.0B1 - 7.0.5, 7.1.0B1 - 7.1.0B3, 6.1.10.100 - 6.1.10.101, 7.2.0B1 - 7.2.12, 7.3.0B1 - 7.3.17, 7.4.0B1 - 7.4.8, 7.5.0B1, 7.6.0B1 - 7.6.0, 8.0.0B1 Workaround: Avoid -pm or -o4. But the warning doesn't indicate any change of the compiler's behavior, so you might as well ignore it. ------------------------------------------------------------------------------- FIXED SDSCM00050520 ------------------------------------------------------------------------------- Summary : strip crashes on files with more than 64k sections Fixed in : 8.0.0B2 Severity : S2 - Major Affected Component : Strip Utility Release Notes: The strip utility will abnormally terminate if its input is an ELF file with more than 64k sections (actually exactly 0xff00), and its output would be less than 64k sections. Defect occurs in C6000 Compiler versions: 7.0.0B1 - 7.0.5, 7.1.0B1 - 7.1.0B3, 7.2.0B1 - 7.2.12, 7.3.0B1 - 7.3.17, 7.4.0B1 - 7.4.8, 7.6.0B1 - 7.6.0, 8.0.0B2 - 8.0.0B1 Workaround: Don't strip the file ------------------------------------------------------------------------------- FIXED SDSCM00050554 ------------------------------------------------------------------------------- Summary : cmp6x (compressor) fails with error message "Backtracked too many times" Fixed in : 8.0.0B2 Severity : S2 - Major Affected Component : Compressor (cmp) Release Notes: This update fixes an issue where the cmp6x executable was abnormally terminating with an error message "Backtracked too many times". Workaround: Use the --no_compress option. Code size will likely be worse. =============================================================================== 6. Defects fixed in C6000 Code Generation Tools release 8.0.0B1 =============================================================================== The following 3 defects were fixed in C6000 Code Generation Tools release 8.0.0B1, released July 2014. ------------------------------------------------------------------------------- FIXED SDSCM00047517 ------------------------------------------------------------------------------- Summary : Complex math operations are inefficient Fixed in : 8.0.0B1 Severity : S2 - Major Classification : Performance Affected Component : C/C++ Compiler (cl) Release Notes: Improvements to the speed of C99 float complex will be appearing in v8.0 of the C6000 compiler. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00050405 ------------------------------------------------------------------------------- Summary : Incorrect error message when combining #pragma PERSISTENT and DATA_SECTION Fixed in : 8.0.0B1 Severity : S3 - Minor Affected Component : C/C++ Compiler (cl) Release Notes: The error message mentions noinit when it should say persistent instead. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00050535 ------------------------------------------------------------------------------- Summary : Compiler does not accept documented option --c++03 Fixed in : 8.0.0B1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: Compiler emits a fatal error when --c++03 option is encountered on the command line. The --c++03 option is deprecated and will be interpreted as an alias for the --c++ option. Workaround: Use the --c++ option instead. =============================================================================== 7. Current Known Issues =============================================================================== The following 31 known issues exist for C6000 Code Generation Tools release 8.0.1 as of January 2015. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00008248 ------------------------------------------------------------------------------- Summary : Compilers on PC will not work without TMP set Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00034609 Description: When compiling on the PC, the code generator cannot find the icode file produced by the parser if the environment variable TMP is no set. If TMP is set, then all appears well. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00008465 ------------------------------------------------------------------------------- Summary : Language Conformance: crash because of void pointer dereference Affected Component : Parser Description: Compiler generates multiple INTERNAL ERRORs when code like the following is compiled: void dr106_1(void *pv, int i) { *pv; i ? *pv : *pv; *pv, *pv; } ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00008534 ------------------------------------------------------------------------------- Summary : Linker -xml_link_info option doesn't work when in a command file Affected Component : Linker Description: The option --xml_link_info=file.xml does not work when it is placed inside a linker command file. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00008537 ------------------------------------------------------------------------------- Summary : assembler expression ~(0x80000000) evaulates as 0x80000000 Affected Component : Assembler Description: The following expression is evaluating incorrectly in the assembler: .eval ~(0x80000000), mask mask ends up getting assigned 0x80000000, whereas I expect it to be 0x7FFFFFFF. It seems that any constant with bit 31 set will incorrectly return 0x80000000 ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00008543 ------------------------------------------------------------------------------- Summary : Forward reference in .space generates an internal error Affected Component : Assembler Description: If you attempt to assemble: .space 0+a b a .set 1 the assembler will generate an internal error. This happens with v3.83 and v4.1.0B1 on Solaris. If you change the code to: .space a b b .set 1 the correct error message is generated, 'Absolute, well-defined integer value expected'. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00008928 ------------------------------------------------------------------------------- Summary : Extern inline functions are not supported in the C/C++ Compiler Affected Component : Parser Duplicate Defects : SDSCM00018364 Description: Users cannot create global accessible code with INLINE functions. The V3.00 compiler/code generator does not create globally accessible code for functions which are declared inline. A simple example is: inline int x() { return 1; } int y() {return 2;} When compiled with 'cl6x -k -c test.c', a warning is produced: 'test.c', line 1: warning: function 'x' was declared but never referenced and the resulting assembler file (test.asm) does not contain any code for x(). The documentation states that code declared inline will be inlined in that module but global code will also be generated (section 2.10.3.2 in v3.00 C Compiler manual). The new compiler is overly aggressive in its optimizations. If y() is modified to call x() then code is generated for x() unless the optimizer is also invoked (by using -x2). ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00014430 ------------------------------------------------------------------------------- Summary : calloc doesn't check arguments to make sure the requested size is reasonable Affected Component : Runtime Support Libraries (RTS) Description: The function calloc() is required to return a pointer to memory representing "nelem" copies of "size" bytes, or NULL if the request cannot be satisfied. However, for some values of "nelem" and "size" (specifically when the result of nelem*size wraps around), calloc can return a pointer to an object that is not large enough, rather than NULL. For example, on a 32-bit target, if the user calls calloc(0x00010001, 0x00010001), even though each argument by itself is reasonable, the request cannot be satisfied because the product is 0x000100020001, which exceeds size_t. (Note that we cannot check for overflow by checking if the product is less than either argument, which is commonly done for unsigned addition.) Arguably, we can try to claim that it is undefined behavior to make a call to calloc where the product would exceed size_t, but there doesn't seem to be anything in the standard which says so. The problem is worse on 16-bit targets, where calloc(0x0101, 0x0101) is enough to overflow size_t. It may not be obvious to the user that this overflows. Another concern is that it is hard to figure out whether a multiplication will overflow without having a double-width multiply available. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00018691 ------------------------------------------------------------------------------- Summary : Linker gives misleading warning when dot expressions used in SECTION directive for .stack section Affected Component : Linker Description: Linker gives the warning: warning: creating ".stack" section with default size of 0x800; use the -stack option to change the default size even when the application does not link in boot code from RTS lib. A linker command file is used that contains a specialized SECTION directive for the ".stack" section. Because of a series of ". += " assignments in the section spec, the linker is forced to increase the size of the .stack section to 0xc00. The linker is doing the correct thing by making a .stack section large enough to accommodate the dot expressions, but the diagnostic is misleading, as 0x800 isn't the final size of the .stack section. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00023977 ------------------------------------------------------------------------------- Summary : compiler is scheduling use of A8 too early causing an incorrect branch Affected Component : Code Generator Duplicate Defects : SDSCM00038899, SDSCM00033497, SDSCM00027812, SDSCM00026420, SDSCM00025367, SDSCM00024562 Description: The below code is generated by the compiler. The MVKL of _sqrt into A8 does not occur correctly which results in an incorrect branch. MVKH .S2 0x2de00d1b,B16 || OR .L2X A8,B7,B1 || MVKL .S1 _sqrt,A8 ; |80| || STW .D2T2 B29,*+SP(144) ; |88| There appears to some type of dependency with what happens several instructions above in: SUBDP .L1X A7:A6,B11:B10,A5:A4 ; |88| || ADDDP .S1 A11:A10,A11:A10,A7:A6 ; |81| If the NOPS between the instructions are increased, the error goes away. Increasing the NOP 1 to NOP 3 in line following the parallel SUBDP||ADDDP and the load works correctly. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00031374 ------------------------------------------------------------------------------- Summary : C6x 6.1.6 performance degradation compared with 6.0.14 Affected Component : C/C++ Compiler (cl) Description: Details of performace drop can be found the attached Email ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00036152 ------------------------------------------------------------------------------- Summary : Compiler generates internal error from parser when compiling a source file containing gcc "labels as values" extension Affected Component : Parser Duplicate Defects : SDSCM00036148 Description: Use of GCC extension "labels as values" in a source file causes the compiler to generate an internal error and abort. Compiler needs to either properly support labels as values extension, or diagnose attempted use of "labels as values" and reject it as an unsupported feature. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00037671 ------------------------------------------------------------------------------- Summary : XML output needs encoding specification Affected Component : Linker Description: Any tool that emits XML output (OFD or linker with --xml_info_file) needs to specify the encoding (e.g. encoding="ISO-8859-1") and be sure to handle "extended" characters correctly. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00039264 ------------------------------------------------------------------------------- Summary : When building with -o2, compiler sometimes fails to complete compilation Affected Component : Optimizer Description: Compiler fails to complete compilation of user-provided test case and eventually crashes. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00040934 ------------------------------------------------------------------------------- Summary : Structure is not initialized correctly when using -o2 or -o3 optimization Affected Component : Optimizer Description: There is a problem with the initialization of a structure using symbols generated in the linker command file. We use symbols generated in the linker cmd file using the dot operator. These symbols are used as an initial value for a class/struct with a constructor. In our case we want the difference of two addresses that the linker generates. When using optimization -o2 or -o3, the compiler generates .cinit entries instead of the constructor call. In those .init-entries it doesn't use the difference of the addresses; instead it uses the first symbol. When turning off optimization or using lower level of opt than -o2, the constructor calls are generated and the struct is initialized correctly. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00042559 ------------------------------------------------------------------------------- Summary : modf(-Inf, 1.0) with -mv6740 enters infinite loop Affected Component : C/C++ Compiler (cl) Description: Attempting to call modf(-Inf, 1.0) will result in an infinite loop. C6000 doesn't guarantee to handle Inf values correctly, but this should at least not be an infinite loop. Also calling modf(x, NaN) where x is negative will also result in an infinite loop. Not sure if this is the same bug. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00043877 ------------------------------------------------------------------------------- Summary : Emit warning message when objects of size 256MB or larger truncated Affected Component : C/C++ Compiler (cl) Description: Data objects of size 256MB or larger are silently truncated to a much smaller size. This is most easily seen for an object of size 512MB. The compiler should emit a warning message that indicates we don't support objects of size 256MB or larger. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00046391 ------------------------------------------------------------------------------- Summary : When failing to place a section, include size of trampolines in error message Affected Component : Linker Description: The C6000 linker generates a strange error: lnk6x -mv=6600 _tsk.obj debug\single\_linker.cmd "_linker.cmd", line 5: error: program will not fit into available memory. placement with alignment fails for section ".text" size 0x1220 . Available memory ranges: MEM_18 size: 0x1220 unused: 0x1220 max hole: 0x1220 error: errors encountered during linking; "$kernel.out" not built The alignment of the .text section is 32 (from ofd6x): 18 .text 0x00000000 0x00000000 0x1220 32 Y The relevant part of the command file is: MEMORY { MEM_18: o=0x00800420 l=0x00001220 } SECTIONS { .text > MEM_18 } The error indicates that the linker can't fit 0x1220 bytes into a properly- aligned hole at 0x00800420 that is 0x1220 bytes long! There are no other .text sections or subsections. [ response: The error message is a bit misleading about the size of .text. The reported size is the total size of the input sections named .text, but doesn't account for the trampolines that the linker had to add. If you look at the linker map file (the linker option --map_file), you'll see that the actual size of .text after trampolines are added is 0x14e0. Certainly that error message needs to be made clearer ] ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00046659 ------------------------------------------------------------------------------- Summary : global labels defined in .cproc region are discarded Affected Component : Code Generator Description: The linear assembler accepts global label definitions inside a .cproc region, and even puts them in the I-file, but the codegen discards them. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00046690 ------------------------------------------------------------------------------- Summary : pow(min, max) and pow(max, max) incorrect Affected Component : Runtime Support Libraries (RTS) Description: pow(DBL_MIN, DBL_MAX) should be 0, but RTS routine returns ??? pow(DBL_MAX, DBL_MAX) should be +Inf, but RTS routine returns ??? ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00046695 ------------------------------------------------------------------------------- Summary : FP rounding error, 1 ULP makes P70590.c fail Affected Component : Runtime Support Libraries (RTS) Description: IEEE-754 requires exact rounding for float addition. GCC gets 4056cf03 290a0f79 const folding gets 4056cf03 290a0f79 C6000 RTS gets 4056cf03 290a0f79 C6740 simulator gets 4056cf03 290a0f78 C6600 simulator gets 4056cf03 290a0f78 correct answer is ???? ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00046929 ------------------------------------------------------------------------------- Summary : Hex converter fails to process RAM model .cinit records for initialized sections Affected Component : Hex Converter (hex) Description: For a COFF RAM-model (-cr) program, hex converter fails to process the .cinit records for any initialized section. This is the same as SDSCM00036443, except that that covers the case when we are creating a boot table, and this request represents the case when we are not creating a boot table. Note that it's difficult to legitimately create an initialized section with .cinit records. The only way I was able to accomplish it was to create a distinct initialized section and combine them in the linker command file output section specification for .bss ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00046931 ------------------------------------------------------------------------------- Summary : Hex converter map file does not list all sections for RAM model program with initialized sections with .cinit records Affected Component : Hex Converter (hex) Description: For a COFF RAM-model (-cr) program, when creating a boot table, the hex converter will process the .cinit records for any initialized section. However, the hex converter infrastructure gets confused because it keeps track of the end of a section's data in the boot table, and there might now be two parts: the initialized data and the converted .cinit records. This ultimately leads to almost no sections appearing in the hex converter map file. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00047243 ------------------------------------------------------------------------------- Summary : isunordered not supported Affected Component : Runtime Support Libraries (RTS) Description: C6x does not support C99 function isunordered ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00047244 ------------------------------------------------------------------------------- Summary : C99 header file fenv.h not supported Affected Component : Runtime Support Libraries (RTS) Description: C6x does not provide fenv.h ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00047245 ------------------------------------------------------------------------------- Summary : C99 math.h macros not supported Affected Component : Runtime Support Libraries (RTS) Description: C99 math.h does not provide support for several macros (i.e. FLT_EVAL_METHOD, MATH_ERRNO, MATH_ERREXCEPT, FP_ILOGB0, FP_ILOGBNAN). ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00047568 ------------------------------------------------------------------------------- Summary : Disassembler fails to disassemble DPINT DPTRUNC DPSP Affected Component : Disassembler (dis) Description: The disassembler disassembles valid DPINT, DPTRUNC, and DPSP instructions as .word ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00048083 ------------------------------------------------------------------------------- Summary : %#x should not prefix 0x to a zero value Affected Component : Runtime Support Libraries (RTS) Description: C99 7.19.6.1 ("fprintf") says that with '#', "For x (or X) conversion, a nonzero result has 0x (or 0X) prefixed to it." However, we prefix the 0x even for zero values. Most other compilers do not prefix the 0x for a zero value. Strictly speaking, what we do could be argued to be conforming, but we really should just do what other compilers do. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00048582 ------------------------------------------------------------------------------- Summary : Use of short form of options in C_OPTION may cause spurious warning Affected Component : ELF Linker Description: If the C_OPTION environment variable is set with the short form of an option, the compiler will sometimes emit a warning that the option is invalid for the linker and will be ignored. To recreate: setenv C_OPTION -pden bugslayer --t C6000 CQ10569 You will see: cl6x -mv6400 --abi=coffabi ... >> WARNING: invalid linker option -pden (ignored) ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00049284 ------------------------------------------------------------------------------- Summary : Compiler misreports Misra warning 10.1 Affected Component : Parser Description: Compiler misreports MISRA warning 10.1/R for the following code. typedef enum _MyEnum { One, Two } MyEnum; MyEnum MyVariable; int foo(void) { int result = 1; if (One == MyVariable) // fails here with MISRA-C:2004 10.1/R { result = 2; } return result; } ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00050131 ------------------------------------------------------------------------------- Summary : Local struct with non-constant initializer treated as static scope variable Affected Component : Parser Description: We've discovered a problem where the C++ compiler places a local structure variable not on the stack but in the data segment, as if it was a static structure. The problem is especially insidious because the issue will only have an impact on re-entrance. The problem seems to occur only for C++ files, and only if the structure initializer list contains a variable. Constant initializer lists do not trigger the issue. The structure in the first function will be allocated on the stack, but the structure in the second will be compiled as if it was declared static. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00051243 ------------------------------------------------------------------------------- Summary : Cannot create stack or heap of size 0x80000000 Affected Component : Linker Description: If you ask for a heap or stack of size 2^31 or larger, the linker will incorrectly sign-extend to 64 bits and treat it as 0xffffffff80000000, which can't be allocated.