C2000 C/C++ CODE GENERATION TOOLS 17.3.0.STS Release Notes March 2017 ================================================================================ Contents ================================================================================ 1) Support Information 2) New Features ------------------------------------------------------------------------------- 1. Support Information ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- 1.1) List of Fixed and Known Defects ------------------------------------------------------------------------------- As of the 16.12.0.STS release, the DefectHistory.txt file has been replaced with the two files Open_defects.html and Closed_defects.html. For open bugs, a status of Open or Accepted means that the bug has not been examined yet, whereas a status of Planned means that an evaluation or fix is in progress. ------------------------------------------------------------------------------- 1.2) Compiler Wiki ------------------------------------------------------------------------------- A Wiki has been established to assist developers in using TI Embedded Processor Software and Tools. Developers are encouraged to read and contribute to the articles. Registered users can update missing or incorrect information. There is a large section of compiler-related material. Please visit: http://processors.wiki.ti.com/index.php?title=Category:Compiler ------------------------------------------------------------------------------- 1.3) Compiler Documentation Errata ------------------------------------------------------------------------------- Errata for the "TI C2000 Optimizing Compiler User's Guide" and the "TI C2000 Assembly Language User's Guide" is available online at the Texas Instruments Embedded Processors CG Wiki: http://processors.wiki.ti.com/index.php?title=Category:Compiler under the 'Compiler Documentation Errata' link. ------------------------------------------------------------------------------- 1.4) TI E2E Community ------------------------------------------------------------------------------- Questions concerning TI Code Generation Tools can be posted to the TI E2E Community forums. The "Development Tools" forum can be found at: http://e2e.ti.com/support/development_tools/f/default.aspx ------------------------------------------------------------------------------- 1.5) Defect Tracking Database ------------------------------------------------------------------------------- Compiler defect reports can be tracked at the Development Tools bug database, SDOWP. The log in page for SDOWP, as well as a link to create an account with the defect tracking database is found at: https://cqweb.ext.ti.com/pages/SDO-Web.html A my.ti.com account is required to access this page. To find an issue in SDOWP, enter your bug id in the "Find Record ID" box once logged in. To find tables of all compiler issues click the queries under the folder: "Public Queries" -> "Development Tools" -> "TI C-C++ Compiler" With your SDOWP account you can save your own queries in your "Personal Queries" folder. ------------------------------------------------------------------------------- 1.6) Short Term Support release ------------------------------------------------------------------------------- The C2000 CGT v17.3.0.STS release is a short term support (STS) release. This release will be supported only until the next STS or LTS release. ------------------------------------------------------------------------------- 2. New Features ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- 2.1) Improved stack usage with inline functions ------------------------------------------------------------------------------- The new compiler improves stack usage by sharing aggregate data originally defined in inline functions. Example: struct ARGS { int f1,f2,f3,f4,f5; }; static inline void func1() { struct ARGS a = {1, 2, 3, 4, 5}; foo(&a); } static inline void func2() { struct ARGS b = {1, 2, 3, 4, 5}; foo(&b); } void func3() { func1(); func2(); } In previous compilers, if func1 and func2 are inlined, the structs a and b would not share the same stack location. This version of the compiler will now share stack memory for local aggregates defined in inline functions. ------------------------------------------------------------------------------- 2.2) C2000/CLA: Optimization of volatile bitfield assignments ------------------------------------------------------------------------------- Prior to this release, asignments to volatile bitfields would follow the read, modify, write methodology, even when such an operation is not needed. Consider the following code segment: short a; struct str16 { short x:16; }; volatile struct str16 str16_vol; void foo(void) { str16_vol.x = a; } Prior to this optimization, str16_vol.x would be read before being assigned to, resulting in the C2000 assembly: MOVW DP,#_str16_vol MOV AL,@_str16_vol MOV AL,@_a MOV @_str16_vol,AL The initial MOVW is unnecessary. With this release, such a move will not be generated on either C2000 or CLA. ------------------------------------------------------------------------------- 2.3) CLA: Prefer direct addressing with --cla_support=cla[12] ------------------------------------------------------------------------------- When accessing and object multiple times in succession, earlier versions of the compiler would generate inefficient indirect addressing operations. For example, the following code: struct { short x; short y; } dst_struct; dst_struct.y = 0; Might generate the following assembly: MMOVI16 MAR1,#_dst_struct MNOP MNOP MMOVZ16 MR0,#0 MMOV16 *MAR1+[#1],MR0 In this release, the following assembly will be genereated instead: MMOVZ16 MR0,#0 MMOV16 @_dst_struct+1,MR0