7.9.8.74. GEL_SharedMemHaltOnWriteOn()ΒΆ

Affected cores are halted during a write to shared memory.

Syntax

GEL_SharedMemHaltOnWriteOn( void );

Parameters

None

Description

Multiple cores on a single processor can share a block of memory. While writing to memory, the breakpoints in that block have to be cleared for a short time by the driver. This function specifies that all cores with executable code on that block are halted to ensure that no breakpoints are missed and invalid code is not executed.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_SharedMemHaltOnWriteOn();

Related Topics

GEL_SharedMemHaltOnWriteOff

GEL_SharedMemHaltOnStepOff

GEL_SharedMemHaltOnStepOn