7.9.8.40. GEL_MapOn()ΒΆ

Enables memory mapping.

Syntax

GEL_MapOn()

Parameters

None.

Description

This function enables memory mapping. The Code Composer Studio debugger does not attempt to read from a map segment that is not readable or attempt to write to a map segment that is not writeable. When mapping is first turned on, the entire memory range is assumed to have no reading or writing capabilities. You must add memory sections (using the GEL_MapAdd() function) to allow the debugger to access valid sections. On power up, memory mapping is turned off by default.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_MapOn();

Related Topics

GEL_MapAdd

GEL_MapOff

GEL_MapDelete

GEL_MapReset