7.9.8.7. GEL_BreakPtAdd()

Adds a breakpoint.

Syntax

GEL_BreakPtAdd( address [,”Condition] );

Parameters

address identifies the location of the breakpoint.

Condition(optional) specifies the condition used in the conditional breakpoint If you specify a condition, it must be enclosed in quotation marks.

Description

This function sets a software breakpoint at a specific address. If a condition is specified, the breakpoint becomes a conditional breakpoint and execution stops only if the condition evaluates to true. The address can be any GEL expression that evaluates to a program address, or a string that specifies a symbolic location.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: No

Example

GEL_BreakPtAdd(0x2000);
GEL_BreakPtAdd(TargetLabel + 100);
GEL_BreakPtAdd(“main”);
GEL_BreakPtAdd(0x2000, “a < b”);

Related Topics

GEL_BreakPtDel

GEL_BreakPtReset

GEL_BreakPtDisable