7.9.2.1. Legacy unsupported functionsΒΆ

The following GEL Built-In functions are not supported. The GEL will recognize these functions, however, no operation will be performed when they are called.

GEL_CloseWindow

GEL_Exit

GEL_OpenMemoryWindow

GEL_OpenWindow

GEL_ProjectAddSubProj

GEL_ProjectBuild

GEL_ProjectBuildConfi g

GEL_ProjectClose

GEL_ProjectCreateCopy Config

GEL_ProjectCreateDefa ultConfig

GEL_ProjectLoad

GEL_ProjectRebuildAll

GEL_ProjectRebuildAll Config

GEL_ProjectRemoveConf ig

GEL_ProjectRemoveSubP roj

GEL_ProjectSave

GEL_ProjectSetActive

GEL_ProjectSetActiveC onfig

GEL_ProjectSetSubProj ConfigSel

GEL_SrcDirAdd

GEL_SrcDirRemoveAll

GEL_StopTransferToFil e

GEL_TransferToFile

GEL_TransferToFileCon fg

GEL_WatchAdd

GEL_WatchDel

GEL_WatchReset

The following GEL Built-In functions are only supported in the Windows platform.

GEL_System