Release Notes for Code Composer Studio™ v6.2.0

These release notes contain valuable information which may not be included in other product documentation. This information will assist you in the use of Code Composer Studio™.
The release notes are divided into four sections:

·         General Information

·         New in CCSv6.2.0

·         New in CCSv6.1.3

·         New in CCSv6.1.2

·         New in CCSv6.1.1

·         New in CCSv6.1.0

·         New in CCSv6.0.1

·         New in CCSv6.0.0

·         Component Versions

·         Known Issues


General Information

CCSv6.2.0 uses an unmodified Eclipse Version 4.5.1 and CDT 8.7.
They are packaged together under “Eclipse IDE for C/C++ Developers” package available from www.eclipse.org. Additional plug-ins or 3rd party tools may be installed that are compatible with Indigo release.

For additional information and support, please go to: https://processors.wiki.ti.com/index.php/Category:Code_Composer_Studio_v6  

Installation:

Please note that use of anti-virus software or a firewall may cause issues during installation.
McAfee software in particular has been especially troublesome.
If possible, disable anti-virus and firewall software during installation.
If not, use of the Offline Installer is strongly recommended.

On Windows:

If you are using an Offline CCS Installer, the zip file in which it is
distributed must first be extracted:

1. Right-click on CCS_6.x.x.xxxxx_win32.zip and select "Extract All...".
2. Enter the directory where you wish to extract the files.
3. Click on Extract.

Once extraction has successfully completed, proceed with the installation steps below.

To install Code Composer Studio:

1. Run ccs_setup_6.x.x.xxxxx.exe.
2. Choose where you want to install.
3. Select the components you wish to install.

On OS X:

If you are using an Offline CCS Installer, the zip file in which it is
distributed must first be extracted:

1. Right-click on CCS_6.x.x.xxxxx_osx.zip and select "Open”.  This will extract the directory from the zip file..

Once extraction has successfully completed, proceed with the installation steps below.

To install Code Composer Studio:

1. Run ccs_setup_6.x.x.xxxxx by clicking on the application in the Finder
2. Choose where you want to install.
3. Select the components you wish to install.

On Linux:

Please visit https://processors.wiki.ti.com/index.php/Linux_Host_Support_CCSv6 before installing CCS on Linux. It contains important information on
installing CCS on different Linux distributions, including CCS dependencies that may need to be installed first.

Before installing CCS, the tarball file in which the CCS Installer is distributed must first be extracted:

untar CCS_6.x.x.xxxxx_linux-x64.tar.gz or CCS_6.x.x.xxxxx_web_linux-x64.tar.gz and extract all files.

If installing from DVD, you also need to either mount the DVD with execute permissions first, or copy the files off the DVD to a local drive and change permissions there to run the installer.

Once extraction has successfully completed, proceed with the installation steps below.

Note: To facilitate the installation of emulation drivers, it is necessary to run part of the installation process as root.
You may if you wish install all of CCS as root. However, it is preferred that you first install CCS as a normal user and then install the drivers as root.

To install Code Composer Studio as a normal user and emulation drivers as root:

1. Run ccs_setup_6.x.x.xxxxx.bin as a normal user.
2. Choose where you want to install.
3. Select the components you wish to install.
4. Navigate to directory <Install-Folder>/ccsv6/install_scripts.
5. As root, execute script "install_drivers.sh".

To install all of Code Composer Studio as root:

1. Run ccs_setup_6.x.x.xxxxx.bin as root.
2. Choose where you want to install.
3. Select the components you wish to install.

Activation:

  1. Go to https://processors.wiki.ti.com/index.php/Activating_CCSv6
  2. Follow step-by-step instructions

Managing Your License:

  1. CCS requires a valid license to be used.  There are a number of free license options, you will be given the opportunity to create one of the free licenses when you first run CCS. 
  2. Note that you are not able to use a CCSv5 license with CCSv6; it requires a CCSv6 license.
  3. Web interface for managing your licenses: www.ti.com/myregisteredsoftware 
    Use it if you want to see expiry info, or move the license to a different machine.
     

 


 

 

New in CCSv6.2.0

·        General Enhancements

·         Bug fixes

·         CCS 6.2.0 is 64bit native on Linux.   The 32bit native Linux is no longer supported as of this release. 

·         Resource Explorer 2.0 (Beta)

·        Bug Fixes

dbid

id

Component

Headline

DVT-1170

SDSCM00050088

Code Composer Studio

Show semaphore names in Execution Graph

DBGTRC-3071

SDSCM00051862

Code Composer Studio

Command-line programming via UniFlash causes java exception on Linux

DBGTRC-2242

SDSCM00051311

Code Composer Studio

Blackhawk XDS200 debuggers do not install firmware update utilities

DBGTRC-2272

SDSCM00051827

Code Composer Studio

GTI error issued when loading code

DBGTRC-2379

SDSCM00052658

Code Composer Studio

Improve the text of the message that comes up when waking device from lower power mode to clarify what each action does

DBGTRC-2378

SDSCM00052657

Code Composer Studio

CCS shuts down when user clicks on "Yes" in pop-up message that tries to wake up device from low power mode

DBGTRC-2268

SDSCM00051819

Code Composer Studio

XDS GDB Agent should have a configurable base port number

CCSIDE-1605

SDSCM00043955

Code Composer Studio

Errors show up in problems view even after rebuilding with no errors

CCSIDE-1037

SDSCM00040045

Code Composer Studio

NullPointerException when renaming project

CCSIDE-2237

SDSCM00049856

Code Composer Studio

CCSv6 experiences high CPU usage when chromium based tool is opened

CCSIDE-2305

SDSCM00050293

Code Composer Studio

Spell-checker in the editor does not work

CCSIDE-2487

SDSCM00051622

Code Composer Studio

Copy & paste of a project in the Project Explorer does not copy the Debug settings

CCSIDE-2406

SDSCM00051082

Code Composer Studio

Remember that clock was visible from previous debug session and show it again

CCSIDE-2418

SDSCM00051157

Code Composer Studio

Debug view toolbar (Resume, suspend, Terminate, etc.) disappears under certain circumstances

CCSIDE-2579

SDSCM00052362

Code Composer Studio

Breakpoints set from the editor and Breakpoints view are not displayed in the Disassembly view

CCSIDE-2643

SDSCM00052763

Code Composer Studio

Project incorrectly fails to build when option -mfpu=vfpv3-d16 is used

CCSIDE-2555

SDSCM00052129

Code Composer Studio

Breakpoints view does not display current current count if a skip count is set

CCSIDE-2404

SDSCM00051072

Code Composer Studio

Launching a debug session when a previous one is still active leaves its header lingering in the Debug view

CCDSK-1942

SDSCM00052435

Code Composer Studio

Request to add a notification in CCS installer to inform users about which Launchpads are not supported

CCDSK-1938

SDSCM00052349

Code Composer Studio

Update to antivirus warning dialog

CCDSK-1923

SDSCM00052007

Code Composer Studio

Default installation directory to be C:\ti\ccs_<version>

CCDSK-1720

SDSCM00049478

Code Composer Studio

CCSv6 should be integrated in Ubuntus Dash menu

CCDSK-2042

SDSCM00051587

Code Composer Studio

Updates that apply only for CCSv6 appear as updates for CCSv5

CCDSK-469

 

Code Composer Studio

[Eclipse] Infinite loop when copying or renaming a project

CCDSK-2027

 

Code Composer Studio

Projects created with older compilers on newer CCS cannot be imported by another user

CCDSK-1924

SDSCM00052008

Code Composer Studio

Integrate CCS Install with App Center

CCDSK-1900

SDSCM00051593

Code Composer Studio

The install_logs subdirectories should be placed in a single subdirectory under ccsv6

CCBT-1745

SDSCM00051813

Code Composer Studio

CCS Mac: should not parse .DS_Store files

CCBT-1929

SDSCM00052132

Code Composer Studio

Launching a debug server session with two F28069 devices fails with error 1006: Unable to allocate memory

CCBT-1794

SDSCM00052217

Code Composer Studio

When loading a .hex file, CCS and Uniflash incorrectly report loading zero bytes to target

CCBT-1826

SDSCM00052511

Code Composer Studio

CCS crashes when loading a program with "Align program segments to 64-bit memory regions" flash option is enabled

CCBT-1825

SDSCM00052509

Code Composer Studio

Invalid resets can cause a DS crash

CCBT-1819

SDSCM00052457

Code Composer Studio

Register view prevents changes to registers on C2000 devices

CCBT-1817

SDSCM00052425

Code Composer Studio

Linux version of gti_uart_driver.xml contains reference to Windows driver file (JavaToGtiAdapter.dvr) instead of Linux

CCBT-1815

SDSCM00052413

Code Composer Studio

Hercules Flash - Problem with loading programs with non-64bit aligned segments

CCBT-1823

SDSCM00052496

Code Composer Studio

XDS510 JTAG debuggers fail to finish flashing CortexM devices

CCBT-1764

SDSCM00051971

Code Composer Studio

CCS launched with wrong product id when launched via DSS

CCBT-1785

SDSCM00052150

Code Composer Studio

Need DSS memory read APIs that natively return a floating point value

CCBT-1790

SDSCM00052197

Code Composer Studio

Under certain circumstances, GEL does not properly work with the ternary "?" operator

CCBT-1834

SDSCM00052535

Code Composer Studio

Typo in error message

CCBT-1801

SDSCM00052283

Code Composer Studio

The values of packed structure members are not displayed correctly in Expressions view

CCBT-1781

SDSCM00052110

Code Composer Studio

Debug info about GCC C++ namespaces are not processed correctly

 New in CCSv6.1.3

·        General Enhancements

·         Enhancements to IDE:

o   Integration with Eclipse v4.5.1 and CDT 8.7

·         Added support for OS X for MCU devices.

·         Support for GCC for MSP430

·         Improved Cortex A15 SM debug support
 

·         MSP EnergyTrace

o   Improved EnergyTrace tool for profiling application’s energy consumption, battery lifetime, monitoring internal device states and determining execution hotspots (statistical function profile)

·        Bug Fixes

dbid

id

Component

Headline

33607210

SDSCM00052778

Code Composer Studio

Compiler discovery msp gcc use xml file for buildid

33607191

SDSCM00052759

Code Composer Studio

Project wizard for PRU cores does not automatically pull a linker CMD file

33607181

SDSCM00052749

Code Composer Studio

CCS does not recognize Linaro GCC toolchain GNU v5.2.1

33607147

SDSCM00052715

Code Composer Studio

Energia sketch imported into CCS generates build error "Un-terminated string literal detected during code-generation!"

33607054

SDSCM00052622

Code Composer Studio

CCS hex utility for C55x does not allow user to pass values correctly to reg_config option

33607052

SDSCM00052620

Code Composer Studio

Compiler discovery does not distinguish between gcc_msp430_4.9.14r1_167 and gcc_msp430_4.9.14r1_364

33607045

SDSCM00052613

Code Composer Studio

CCS throws Java.lang.NULL error when importing a project via projectspec for an unsupported device

33607042

SDSCM00052610

Code Composer Studio

Command line ProjectCreate sometimes fails when the batch file also contains other commands

33607021

SDSCM00052589

Code Composer Studio

When the device variant is changed for a project, any prebuild and postbuild steps that were set for the project disappear

33606994

SDSCM00052562

Code Composer Studio

Cannot enable 'View' menu in custom Perspective

33606993

SDSCM00052561

Code Composer Studio

Editor greys out wrong conditional code on Ubuntu

33606928

SDSCM00052496

Code Composer Studio

XDS510 JTAG debuggers fail to finish flashing CortexM devices

33606928

SDSCM00052496

Code Composer Studio

XDS510 JTAG debuggers fail to finish flashing CortexM devices

33606911

SDSCM00052479

Code Composer Studio

Updated editor file associations to recognize .sv7A as an assembly file

33606908

SDSCM00052476

Code Composer Studio

Setting up breakpoints from the Editor view of a non-CCS project causes several views to be disconnected from the target

33606907

SDSCM00052475

Code Composer Studio

Disassembly view shows a disabled breakpoint if it is set to the source code line instead of an opcode

33606906

SDSCM00052474

Code Composer Studio

Cannot set breakpoints from the Editor view on a Cross GCC project

33606901

SDSCM00052469

Code Composer Studio

GCC Linker option for passing options file should be "@file" instead of the "-@file" that is currently generated

33606894

SDSCM00052462

Code Composer Studio

Explicitly name auto-generated make dependency files to something.d, to avoid user confusion with .pp files

33606889

SDSCM00052457

Code Composer Studio

Register view prevents changes to registers on C2000 devices

33606873

SDSCM00052441

Code Composer Studio

Help for GEL_EvalOnTarget needs to mention what the return value is

33606872

SDSCM00052440

Code Composer Studio

GEL_Connect() is not documented in the CCS Help

33606871

SDSCM00052439

Code Composer Studio

GEL_Disconnect not listed in help

33606867

SDSCM00052435

Code Composer Studio

Request to add a notification in CCS installer to inform users about which Launchpads are not supported

33606857

SDSCM00052425

Code Composer Studio

Linux version of gti_uart_driver.xml contains reference to Windows driver file (JavaToGtiAdapter.dvr) instead of Linux

33606847

SDSCM00052415

Code Composer Studio

Adding Eclipse Static library project as dependency to a CCS project causes the libraries to be moved under -T option

33606845

SDSCM00052413

Code Composer Studio

Hercules Flash - Problem with loading programs with non-64bit aligned segments

33606839

SDSCM00052407

Code Composer Studio

Error parser does not detect compiler error on the last source line

33606826

SDSCM00052394

Code Composer Studio

[CDT] Renaming a file or project results in the message "The participant 'Header File Rename' caused an internal error

33606795

SDSCM00052363

Code Composer Studio

Memory Allocation View does not display bargraphs in Ubuntu

33606792

SDSCM00052360

Code Composer Studio

Build fails with program mode compilation enabled as generated makefile passes incorrect object files to linker

33606781

SDSCM00052349

Code Composer Studio

Update to antivirus warning dialog

33606772

SDSCM00052340

Code Composer Studio

Browse examples button on Getting Started Page hides MSPWare examples

33606715

SDSCM00052283

Code Composer Studio

The values of packed structure members are not displayed correctly in Expressions view

33606709

SDSCM00052277

Code Composer Studio

The DGrid widget disappears when any text is added to the Widget Column Names field

33606631

SDSCM00052199

Code Composer Studio

Importing legacy CCSv3 project fails via command-line import

33606630

SDSCM00052198

Code Composer Studio

Enable Sync Group cores should somehow warn the user this is only applicable to SMP or be overall disabled

33606629

SDSCM00052197

Code Composer Studio

Under certain circumstances, GEL does not properly work with the ternary "?" operator

33606628

SDSCM00052196

Code Composer Studio

When grouped together, problems and Console view tabs flicker during a project build

33606626

SDSCM00052194

Code Composer Studio

Unable to read 40 bit addresses

33606582

SDSCM00052150

Code Composer Studio

Need DSS memory read APIs that natively return a floating point value

33606553

SDSCM00052121

Code Composer Studio

Preserve search paths and predefines when changing from TI to GCC

33606513

SDSCM00052081

Code Composer Studio

[CDT] BIOS CFG file is not passed to xdctools when building project on Windows with Turkish language settings

33606488

SDSCM00052056

Code Composer Studio

Problems warning for compilers should not redirect user to the CCS App Center

33606449

SDSCM00052017

Code Composer Studio

[CDT] Under certain circumstances, dependent projects are built even when they are up-to-date

33606448

SDSCM00052016

Code Composer Studio

Changing GCC compiler version resets any file-specific build options

33606448

SDSCM00052016

Code Composer Studio

Changing GCC compiler version resets any file-specific build options

33606448

SDSCM00052016

Code Composer Studio

Changing GCC compiler version resets any file-specific build options

33606443

SDSCM00052011

Code Composer Studio

Make it possible to exclude built in RTSC discovery paths

33606442

SDSCM00052010

Code Composer Studio

enable parallel builds by default

33606439

SDSCM00052007

Code Composer Studio

Default installation directory to be C:\ti\ccs_<version>

33606435

SDSCM00052003

Code Composer Studio

Changing compiler version resets any modifications made to the Command-line pattern

33606403

SDSCM00051971

Code Composer Studio

CCS launched with wrong product id when launched via DSS

33606230

SDSCM00051798

Code Composer Studio

Making changes to a header file does not trigger rebuild of the source file that includes that header file

33606219

SDSCM00051787

Code Composer Studio

Request to be able to add file specific options using "Set Additional Flags" button

33606161

SDSCM00051729

Code Composer Studio

If Problems view is minimized and focus is on a source file in the editor, then errors/warnings disappear from Restored view

33606158

SDSCM00051726

Code Composer Studio

Switching to CCS Debug perspective and back to CCS Edit makes Editor Navigate buttons disappear

33606146

SDSCM00051714

Code Composer Studio

Memory View does not refresh and show content after relaunching a debug session

33606072

SDSCM00051640

Code Composer Studio

Request to be able to import archive of projectspecs

33606071

SDSCM00051639

Code Composer Studio

After importing a projectspec with path variable defined, the Location of linked resource shows weird characters

33606027

SDSCM00051595

Code Composer Studio

Disassembly style option in the debugger shows Cortex M3 when debugging Cortex M4 devices

33605977

SDSCM00051545

Code Composer Studio

'New CCS Project' dialog content is truncated (with no scroll bar) if the vertical resolution is too small

33605973

SDSCM00051541

Code Composer Studio

Allow support for batch operations on all build configurations of a project

33605971

SDSCM00051539

Code Composer Studio

Setting a CDT breakpoint in a CCS debug session can cause various views to stop updating

33605962

SDSCM00051530

Code Composer Studio

Add build button and Build Project menu to Debug Perspective, Remove Build All menu

33605594

SDSCM00051162

Code Composer Studio

GC: Tab widget not sending selectedTabIndex binding to target variable

33605534

SDSCM00051102

Code Composer Studio

tiobj2bin folder within \ccsv6\utils should be installed irrespective of which processors are selected for custom install

33605265

SDSCM00050833

Code Composer Studio

Callstack line numbers are off by 1 when using imported Energia project

33604942

SDSCM00050510

Code Composer Studio

Hide the 'RemoteSystemsTempFile' project as an option when browsing projects in the workspace

33604661

SDSCM00050229

Code Composer Studio

The ability to set file specific linker options should not be exposed

33604633

SDSCM00050201

Code Composer Studio

[CDT] Removing file should remove all associated settings

33604378

SDSCM00049946

Code Composer Studio

EVE CCS/Load Program/Browse Project not working

33604378

SDSCM00049946

Code Composer Studio

EVE CCS/Load Program/Browse Project not working

33604378

SDSCM00049946

Code Composer Studio

EVE CCS/Load Program/Browse Project not working

33604218

SDSCM00049786

Code Composer Studio

GC: support bi-directional char array binding

33604021

SDSCM00049589

Code Composer Studio

variables decalred in annoymous namspace cannot be accessed  (GCC compiler )

33603910

SDSCM00049478

Code Composer Studio

CCSv6 should be integrated in Ubuntu's Dash menu

33602012

SDSCM00047580

Code Composer Studio

Linking MSP FETS and sessions

33593104

SDSCM00038672

DVT

CCSv4.2 RC1 profiler doesn’t correctly report the type of cycles, cycle.CPU versus cycle.Total

 

New in CCSv6.1.2

·        General Enhancements

·         Bug fixes  

·        Bug Fixes

dbid

Id

Component

Headline

33606933

SDSCM00052501

Code Composer Studio

OFS inadvertently loads the whole debug info section when printing out a log msg.

33606897

SDSCM00052465

Code Composer Studio

java.lang.NullPointerExecptionError when opening the Memory View

33606735

SDSCM00052303

Code Composer Studio

CCS is unable to build ARM projects for 66AK2* devices set to use the GNU compiler

33606413

SDSCM00051981

Code Composer Studio

Energia location is not recognized on CCS for Mac

33606933

SDSCM00052501

Code Composer Studio

OFS inadvertently loads the whole debug info section when printing out a log msg.

33606897

SDSCM00052465

Code Composer Studio

java.lang.NullPointerExecptionError when opening the Memory View

33606735

SDSCM00052303

Code Composer Studio

CCS is unable to build ARM projects for 66AK2* devices set to use the GNU compiler

 

New in CCSv6.1.1

·        General Enhancements

 

·         Added support for SimpleLink™ CC26xx and CC13xx MCU platform of devices.
 

·         Added support for automatic firmware update for XDS110
 

·         Added OS X platform support for CCS for MCU devices (Beta) 

·         MSP EnergyTrace

o    Improved EnergyTrace tool for profiling application’s energy consumption, battery lifetime, monitoring internal device states and determining execution hotspots (statistical function profile)

·        Bug Fixes

dbid

Id

Component

Headline

33606192

SDSCM00051760

C2000 Code Generation Tools

Compiler error for missing brace "}" at end of source is not reported in Problems view

33594903

SDSCM00040471

DVT

Show profile data in call graph

33606099

SDSCM00051667

DVT

Graph export/import should save/restore autoscale and y-axis range settings.

33606155

SDSCM00051723

DVT

symbol names not show for EnergyTrace on MSP430

33606293

SDSCM00051861

DVT

Improve EnergyTrace UI for power graph to clearly show whether measurements are relative or absolute

33602008

SDSCM00047576

IDE

Unable to generate code coverage data via DSS

33602046

SDSCM00047614

IDE

Scripting Console: Button to open/load a javascript file

33602176

SDSCM00047744

IDE

legacy format header files not handled correctly

33602266

SDSCM00047834

IDE

DS initiated progress dialog should consider the dialog option "Always Run on Background"

33602278

SDSCM00047846

IDE

Once I start a CCS debug session, build all will popup a modal progress box

33602500

SDSCM00048068

IDE

[C28 Flash] Flash programming does not work with "Auto Run on Reset" option on

33602584

SDSCM00048152

IDE

Importing a SYS/BIOS project created with older version of CCS causes migration errors

33602609

SDSCM00048177

IDE

Scan compiler options files to improve conditional formatting

33602657

SDSCM00048225

IDE

Flash programming sometimes results in error "Timed out while writing to Flash memory"

33602680

SDSCM00048248

IDE

Breakpoint on a single source line causes the debugger to break twice before resuming execution

33602690

SDSCM00048258

IDE

Importing a CCS3.3 library project with project dependencies results in java.lang.NullPointerException

33602697

SDSCM00048265

IDE

In the compiler selection drop-down the listing for gcc should include the executable name

33602741

SDSCM00048309

IDE

Missing .ebss and .reset directive highlights for C2000 cmd file

33602776

SDSCM00048344

IDE

Class members are not shown in Variables view for code built with GCC

33602789

SDSCM00048357

IDE

MSP430 Trace View does not refresh properly when decoding instructions

33602816

SDSCM00048384

IDE

Project import tool sometimes does not resolve paths correctly

33602820

SDSCM00048388

IDE

Provide more precise error messages in Import CCS Project wizard

33602840

SDSCM00048408

IDE

Switching between two projects can sometime get GUI Composer out of sync

33602849

SDSCM00048417

IDE

The compiler option -v that specifies the silicon version is retained when switching device variants

33602878

SDSCM00048446

IDE

Flashing fails on Stellaris TM4C129X devices

33602894

SDSCM00048462

IDE

Makefile validation errors prevent makefile re-generation

33602900

SDSCM00048468

IDE

The Location of local variables is sometimes displayed incorrectly for GCC ELF files

33602985

SDSCM00048553

IDE

Include paths using "workspace_loc: variable are not passed to the compiler if the path does not exist

33603000

SDSCM00048568

IDE

Request to have LCD option for meter widget

33603001

SDSCM00048569

IDE

Request to have an out of range indicator option for gauges and meters

33603044

SDSCM00048612

IDE

CCS fails to program certain .out files when "Auto ECC generation" is enabled in Flash Settings

33603191

SDSCM00048759

IDE

Deadlock due to "buddy" classloading

33603338

SDSCM00048906

IDE

Invoking gmake with -s option causes the Problems view to not update after errors have been corrected

33603350

SDSCM00048918

IDE

Would like a method to disable Optimization Advice

33603434

SDSCM00049002

IDE

App center in installer shows MSP430 content even when MSP not selected

33603485

SDSCM00049053

IDE

Request fpr Memory Allocation view to show UNION sections

33605396

SDSCM00050964

IDE

Hex Utility (and GNU Objcopy in the case of GNU tools) should run before post build steps in CCS

33605484

SDSCM00051052

IDE

When using SW breakpoints in source file, the LDR instruction does not work correctly on a Cortex-A8 (AM335x)

33605678

SDSCM00051246

IDE

User is prompted to terminate existing debug session when running a multi-session DSS script from the Console

33605704

SDSCM00051272

IDE

The CCS Online Help content for "Data File Formats" is outdated

33605866

SDSCM00051434

IDE

Multiple copies of the same header file are opened when clicking on a error/warning in the Problems view

33605961

SDSCM00051529

IDE

Debugserver should release files that are opened in the target application when a debug session is terminated

33606052

SDSCM00051620

IDE

TI-RTOS template project fails to build with GNU build tools

33606056

SDSCM00051624

IDE

DefaultToolChain property on Device XML files is not being properly acknowledged by the Project wizard

33606059

SDSCM00051627

IDE

Passing XDCROOT as a parameter to batch file in post build step does not work as expected

33606063

SDSCM00051631

IDE

CCS crash in a gcc compiled C++ program when expanding a class pointer

33606075

SDSCM00051643

IDE

Tiva E device support does not get installed

33606136

SDSCM00051704

IDE

90 day eval license activation is broken

33606202

SDSCM00051770

IDE

Closing and restarting CCS when in CCS Simple mode causes debugger to no longer work (all debug functions are grayed out)

33606220

SDSCM00051788

IDE

Update Linux dependency checker to include Chrome libraries

33606238

SDSCM00051806

IDE

Some variables do not display correct values when debugging DWARF3+ output

33606285

SDSCM00051853

IDE

When exporting GUI Composer project there is no UART Connection option for F28069 device

33606288

SDSCM00051856

IDE

Memory Fill silently fails if Length is preceded with '0x'

33606303

SDSCM00051871

IDE

AppCenter failed to install app due to isWare exception

33606304

SDSCM00051872

IDE

AppCenter failed to install app due to feature not found

33606311

SDSCM00051879

IDE

The function Import from the Target Configurations view has a typo

33606331

SDSCM00051899

IDE

Variables allocated to address 0x0 do not appear correctly in Expressions view

33606357

SDSCM00051925

IDE

Unable to create Energia sketches for MSP432

33606367

SDSCM00051935

IDE

disassembly view does not always refresh correctly.

33606367

SDSCM00051935

IDE

disassembly view does not always refresh correctly.

33606372

SDSCM00051940

IDE

Unable to use $(GEL_file_dir) with GEL_AddInputFile

33606377

SDSCM00051945

IDE

Variables view is pointing to incorrect values in stack in Cortex A9

33606496

SDSCM00052064

IDE

Executable built by custom GCC version with crash CCS when symbols are loaded

33601294

SDSCM00046862

Simulation

66AK2H12 simulator : Source line Step over on  function calls  is not working for CortexA15 cores

33599709

SDSCM00045277

Trace

ETB is not working on DM365 and DM368

33600578

SDSCM00046146

Trace

Setting a trace end job completely disables the Trace generation

33603026

SDSCM00048594

Trace

DM814x Trace shows a Device ID mismatch in Linux

33603028

SDSCM00048596

Trace

DM816x core Trace shows nothing at the Trace Analyzer view in Linux

33603029

SDSCM00048597

Trace

OMAP4 and OMAPL138 Trace fails to properly initialize in CCS for Linux

33603029

SDSCM00048597

Trace

OMAP4 and OMAPL138 Trace fails to properly initialize in CCS for Linux

33606067

SDSCM00051635

Trace

STM pin trace fails to initialize on Centaurus (DM8148) boards

33606106

SDSCM00051674

Trace

Trace viewer locks up CCSv6.1 when displaying data from Cortex A core

 


New in CCSv6.1.0

·        General Enhancements

·         Enhancements to IDE:

·         Integration with Eclipse v4.4.1
 

·         Added support for SimpleLink™ CC26xx and CC13xx MCU platform of devices.
 

·         Added support for on-board USB XDS110 debug (Hercules RM46x LaunchPad).
 

·         Support for GCC for MSP430.
 

·         MSP EnergyTrace

o    Improved EnergyTrace tool for profiling application’s energy consumption, battery lifetime, monitoring internal device states and determining execution hotspots (statistical function profile)

·        Bug Fixes

Id

Component

Headline

SDSCM00051190

CCS App Center

Update "CDT GNU Support" package to include GDB h/w debug feature

SDSCM00050028

DVT

Code coverage trace job freezes CCS

SDSCM00050080

DVT

Support dynamic TSK/HWI/SWI name in System Analyzer

SDSCM00050599

DVT

ProTrace/FunctionExecutionGraph fails to visualize >512 functions

SDSCM00051019

DVT

Add CSV format to the exported EnergyTrace data

SDSCM00051019

DVT

Add CSV format to the exported EnergyTrace data

SDSCM00051073

DVT

EnergyTrace configurations view fails to show if the workspace is brand new or "cleaned"

SDSCM00051169

DVT

Code Coverage source code coloring is not working well

SDSCM00049303

Emulation

C6671 device file specifies 2 C66x cores when it should be one

SDSCM00050110

Emulation

Imported TivaWare project missing links files on CCS Linux

SDSCM00050124

Emulation

Unable to step over an ARM embedded BKPT instruction if it is BKPT 123, works if it is BKPT #123

SDSCM00050343

Emulation

Change Project wizard's default binary format for C674x families from COFF to ELF

SDSCM00050412

Emulation

Some PRU0 registers are mapped to PRU1 registers on AM437x devices

SDSCM00050413

Emulation

The debug register for PRU0 core of the ICSS1 has a typo

SDSCM00050421

Emulation

Support CC3200 with XDS100/200/560v2

SDSCM00050444

Emulation

When two XDS100 emulators are connected to a USB3.0 Hub, only one emulator is able to be connected to CCS

SDSCM00050586

Emulation

CCS for Linux collapses when trying to connect to more than seven cores on a Keystone 2 EVM

SDSCM00051029

Emulation

dbgjtag can communicate with xds200 but debug launch fails with unable to communicate message

SDSCM00051033

Emulation

The word "Emulator" is still present in several emupack messages

SDSCM00051077

Emulation

C6455 and TCI6482 PLLC2 register bank is broken

SDSCM00051077

Emulation

C6455 and TCI6482 PLLC2 register bank is broken

SDSCM00051182

Emulation

Cycle counts are not available for profile clock on C64x targets

SDSCM00042270

IDE

Linker - Cmd mapping should be introduced when a user changes defaults for RTSC projects.

SDSCM00042650

IDE

[TISB] Project Manager should add the RTSC Platform file to the Project Explorer view

SDSCM00044613

IDE

XDC Content Assist is triggering a lot exceptions in customer workspace logs

SDSCM00046255

IDE

JLink: loading and running program in a debug session on LM3S9D92 behaves oddly

SDSCM00047366

IDE

Improve usability for setting linked resource path variables and build variables

SDSCM00047368

IDE

Ability to import/export project and workspace level variables (to/from a file)

SDSCM00047370

IDE

Add support for easily leveraging build variables when setting build properties

SDSCM00047827

IDE

Would like ability to rename memory view "tabs" to user specified name

SDSCM00047828

IDE

Enhancement to use last specified data format for new views.

SDSCM00048029

IDE

CCS flash programmer fails with message "Timed out while writing to Flash memory"

SDSCM00048546

IDE

variables decalred in annoymous namspace cannot be accessed

SDSCM00049004

IDE

MSP430 GTI driver is getting installed even when MSP is not installed

SDSCM00049095

IDE

The wrench/push-pin icon that denotes a file with file specific options does not appear when expected

SDSCM00049211

IDE

Need erase flash option for MSP430

SDSCM00049404

IDE

msp430 emulation logic not restored on a hard reset

SDSCM00049534

IDE

Windows ERRORLEVEL code is not set for headless project import error

SDSCM00049537

IDE

Installation dialog shows "Not Responding"

SDSCM00049538

IDE

Digital Gauge rapaint issue when threshold value is small

SDSCM00049540

IDE

CCS GUI does not allow for compiler option --interrupt_threshold with threshold value omitted

SDSCM00049562

IDE

Renaming widget ID causes existing binding to disappear.

SDSCM00049613

IDE

case sensitive mismatch when importing v3 projects to v5

SDSCM00049687

IDE

CCS not creating proper INTEL-HEX for msp430

SDSCM00049742

IDE

Pop up a warning dialog when 1 day is left on eval license

SDSCM00049763

IDE

headless project import: Add option to auto-import dependant projects

SDSCM00049804

IDE

CCS fails in the presence of VMWare shared folders

SDSCM00049845

IDE

App Center search should search the title as well

SDSCM00049910

IDE

Adding a source look up from Debug View context menu does not works

SDSCM00049947

IDE

New CCS EVE project does not run out of the box

SDSCM00049947

IDE

New CCS EVE project does not run out of the box

SDSCM00049988

IDE

Switching compiler tools from Red Hat GNU to TI does not set linker command file properly

SDSCM00050100

IDE

The Pending Installation Dialog for the App Center has the wrong menu item listed

SDSCM00050101

IDE

Indexer settings not maintained

SDSCM00050102

IDE

Changing part should trigger reindexing

SDSCM00050108

IDE

If a GUI Composer app already contains appInitDS.js file, then it should be used during export

SDSCM00050132

IDE

Dependency Checker having issues with libusb on CentOS 6.5

SDSCM00050137

IDE

A basic new project for Tiva does not run to main when built with Linaro GCC

SDSCM00050189

IDE

Scroll bars missing on Getting Started View

SDSCM00050230

IDE

Browse box of Debug Server log is missing the filename designator

SDSCM00050275

IDE

License location is lost after an update

SDSCM00050324

IDE

Switching between Linaro GNU and TI compiler does not include/exclude linker command file and startup file properly

SDSCM00050342

IDE

When trying to manually load an executable to a PRU core, Browse project returns no hits

SDSCM00050353

IDE

Scanner config builder is very slow for projects where many files override build-settings

SDSCM00050356

IDE

DSS documentation for the description for memory.loadData2() API has typos.

SDSCM00050491

IDE

Manual-mode MPU Project-Property Settings don't persist

SDSCM00050552

IDE

assembly source debug for PRU does not work

SDSCM00050555

IDE

Memory Usage View should state that a non-TI compiler is not supported

SDSCM00050559

IDE

Register view cannot export registers if group has more than 100 registers in it

SDSCM00050580

IDE

CCS for Linux shows GTK and DVT errors errors when launched from the command line

SDSCM00050639

IDE

Profile clock produces different results through each run of the program when benchmarking floating point math

SDSCM00050647

IDE

CCS for Linux shows GTK and DVT errors errors when launched from the command line (Operation Completed in # ms.)

SDSCM00050659

IDE

Enabling parallel build with specific number of jobs along with a pre-build step causes the parallelism to not take effect

SDSCM00050660

IDE

Build option --exceptions correctly used on the compile, incorrectly missing on the link

SDSCM00050702

IDE

CIOServer documentation is missing descriptions

SDSCM00050708

IDE

GC: Not able to select UART for Tiva device

SDSCM00050730

IDE

Update "CDT GNU Support" package to include GDB h/w debug feature

SDSCM00050735

IDE

Continuous Refresh button disappears for Expressions View

SDSCM00050787

IDE

Data corruption occurs when loading memory in 8-bit TI Raw Data mode

SDSCM00050789

IDE

CCS stack trace does not work if stack is in far RAM

SDSCM00050791

IDE

Remove PRU from list of Targets in the target filter field

SDSCM00050797

IDE

Would like a method to disable Optimization Advice or not have it come to the foreground if in the background

SDSCM00050816

IDE

Backslashes in overridden tool-commands cause error-parser problems

SDSCM00050822

IDE

Unexpected behavior after pressing the ctrl key in GUI Composer editor

SDSCM00050844

IDE

Setting TCL_LIBRARY environment variable can cause the CCS installer to not start

SDSCM00050857

IDE

Wrong console output when programming a MSP430 FRAM device

SDSCM00050869

IDE

OMAPL137 and OMAP5912 board XML files are not available in CCS

SDSCM00050877

IDE

CCSv6: CCS Support dialog does not have the correct path for the installation logs

SDSCM00050888

IDE

CCS Memory view: "Copy to clipboard > Selection" limited by range in view

SDSCM00050894

IDE

CCS crashes when loading an ARM relocateable object file

SDSCM00050906

IDE

Add the ability to load a prebuilt linker xml file into the Memory Allocation View

SDSCM00050989

IDE

Request to suppress the message "Unrecognized product of type com.ti.rtsc.XDAIS" that appears during project import

SDSCM00051007

IDE

Memory browser does not display Q values

SDSCM00051063

IDE

Bundle a readme.txt file (with url to CCS Linux Host support page) with all CCS Linux installers

SDSCM00051084

IDE

Code Composer Help content has not been updated for v6. It is still for v5.

SDSCM00051118

IDE

CCSv6: CCS Support dialog does not have the correct path for the installation logs

SDSCM00051173

IDE

CCS deadlock during build

SDSCM00051265

IDE

Problems view displays garbled messages

SDSCM00051279

IDE

Scripting Console command 'eval' is overriding JavaScript 'eval' function

SDSCM00051293

IDE

MSPMathlib does not link in CCS by default; libmath.a library placed after libc.a

SDSCM00051414

IDE

FPv4SPD16 is shown as being set for CC3200 (but really is not)

SDSCM00044490

Trace

Need to load installed libbz2.dll and not the first one found on the windows path

SDSCM00047338

Trace

connecting to multiple cores in two separate debug sessions (each using a different emulator/target) will crash one CCS

SDSCM00049598

Trace

ETB Trace fails to collect data in CCSv6 for Linux

SDSCM00049598

Trace

ETB Trace fails to collect data in CCSv6 for Linux

SDSCM00049896

Trace

Trace Server Crashes on Debugger Terminate after using ITM

SDSCM00050239

Trace

Hardware watchpoint halts more often than expected when configured to halt on writes with specified data value

SDSCM00050528

Trace

Unable to set breakpoint while target is running on Tiva LaunchPad

SDSCM00050628

Trace

Trace Fails to Function after Flash Programming on Hercules Products

SDSCM00050762

Trace

Cortex M4 Trace jobs fail to properly initialize

SDSCM00051035

Trace

Trace analyzer does not think SWO is enabled when it in fact is

SDSCM00051040

Trace

Hang when running Statistical Profiling on TM4C129

SDSCM00051187

Trace

CCS Linux crashes when connecting to EVE coprocessor on a DRA74x

 


New in CCSv6.0.1

·        General Enhancements

·         Support for Hercules RM57L and TMS570LC (Cortex-R4)
 

·         Support for SimpleLink CC32xx.

 

·         MSP430 EnergyTrace

o    New EnergyTrace tool for profiling application’s energy consumption, monitoring internal device states and determining execution hotspots (statistical function profile)
 

·         Note: Texas Instruments is moving away from providing simulators and instead is focusing on providing low cost development boards.
As a result in the standard installation you will not see any simulators.
If you require a simulator they are available on a very limited exception basis. Please contact your TI business contact to request a simulator.

·        Bug Fixes

Id

Component

Headline

SDSCM00050287

IDE

Tools menu activation can take a long time on Ubuntu.

SDSCM00050260

IDE

Example Project Import hangs

SDSCM00050224

IDE

Parameter -D PART_XXXXXXX missing from default build options for Tiva devices

SDSCM00050208

IDE

CCS not creating proper INTEL-HEX for msp430

SDSCM00050195

IDE

Importing a library project ends up as an executable project instead

SDSCM00050150

IDE

Installing an update of MSP GCC via CCS App Center deletes older version

SDSCM00050125

IDE

Rename "Integra Device Support" to "OMAPL/Integra Device Support"

SDSCM00050119

IDE

Project takes very long time to build when error parser is turned on

SDSCM00050109

IDE

msp hex utility improperly naming TI-TXT files

SDSCM00049970

IDE

Changing compiler version causes the compiler include paths to get corrupted

SDSCM00050185

DVT

DSP/BIOS dynamically created objects do not display their names in the ROV

SDSCM00050386

Emulation

Cannot step over on 28 after emu update

SDSCM00050117

MSP Compiler

ULP Advice links do not show up in the Advice view

 


New in CCSv6.0.0

·        General Enhancements

·         Enhancements to IDE:

·         Integration with Eclipse v4.3.1

·         Integration with CDT 8.2.1

·         Introduction of Code Composer Studio App Center.

o    CCS now consists of a core image and a set of recommended & optional add-ons, available thru the App Center.

o    These add-ons include, but are not limited to: TI compilers, GCC, Examples (e.g., MSP430Ware), TI-RTOS, GUI Composer, Simulators, etc.

o    This results in vastly improved product installation experience.
 

·         Support for GCC for MSP430.
 

·         Support for Energīa projects.
 

·         Support for new devices: CC26xx, Dual-core Delfino TMS320F2837xD
 

·         Trace Analyzer

o    Code Coverage for Optimized code

§  All code coverage results are now based on instruction executed. This enable coverage for optimized code

§  Coverage results are provided for Instruction, Source Line, Function and File

o    Context Aware Inclusive Function Profiler

§  Added inclusive function profiling to the profiler (exclusive profiling already supported)

§  Support BIOS context awareness in Function Profiler to provide accurate inclusive function profiling

§  Included per-call function profiling (i.e. result for each instance of execution)

§  Detail view showing profile results based on caller and callee

o    New STM usecase for Memory Transaction Logging

o    ITM

§  Numerous usability improvements
 

·         RTOS Analyzer and System Analyzer

o    RTOS and System Analyzer improvements to support the following

§  Minimal footprint logger (loggerMin)

§  Improve performance of all loggers

§  Improve usability for configuring target application instrumentation

§  Validate target configuration and provide feedback in Analyzer launch dialog

·        Bug Fixes

Id

Component

Headline

SDSCM00036459

DVT

Graph shows fractional numbers of samples on x-axis

SDSCM00038605

DVT

STS and CPU Load views should indicate that they are not supported in stop mode RTA

SDSCM00042689

DVT

Graph tool should allow user to set fixed values for the axis

SDSCM00043761

DVT

The "Display Data Size" parameter of the graph tool seems limited to 512

SDSCM00045320

DVT

Show Coverage option in CodeGen Coverage DVT view does not work

SDSCM00046965

DVT

Analysis (DVT) table views are slow to scroll on Linux

SDSCM00046966

DVT

Trace Analyzer delta cycle count is one row off on ARM targets

SDSCM00047977

DVT

CCS will hang if you terminate the debug session while ITM data is still being processed

SDSCM00048382

DVT

CCS install fails in the presence of VMWare shared folders

SDSCM00049506

DVT

Trace is not working on Linux for Sitara devices

SDSCM00044821

Emulation

CCSv5 is loading emulation DLLs from v3.3

SDSCM00044859

Emulation

CCS hangs when coming out of Windows 7 'Sleep' mode when using XDS560 PCI

SDSCM00045482

Emulation

CCSv5.1 f2811.gel typo

SDSCM00046465

Emulation

Hardware watchpoint set on a 32-bit variable halts the CPU for 16-bit access width when it should not

SDSCM00046908

Emulation

CCS hangs for long moments when debugging BIOS programs with RTDX enabled

SDSCM00047340

Emulation

Errors when starting up a debug session for a single target configuration with a multiple emulator and multicore setup

SDSCM00047514

Emulation

When a device is set for Boundary Scan, any attempt to connect yields a vague error message

SDSCM00048095

Emulation

memory mapped register reading performance degradation between CCS v5.2 and 5.4

SDSCM00048719

Emulation

Floating point option for save memory utility is not available on 66x

SDSCM00048815

Emulation

Connecting to ARM9 cores in Linux using emupack 5.1.320.0 causes a JVM failure

SDSCM00049032

Emulation

profile clock does not work on mid-GEM devices with XDS560v2 and XDS100

SDSCM00049535

Emulation

PRU Disassembly and Memory views show inconsistent data in the 0x1000 address boundary

SDSCM00038282

IDE

CCSv4: After launching target configuration, the debug window is not automatically brought to top

SDSCM00039487

IDE

EASY: Hex utility options should be exposed in the project options dialog

SDSCM00039794

IDE

Prompt user with confirmation dialog box when clicking on "Restore Defaults" in Project Build Properties

SDSCM00041406

IDE

US: Project properties is disabled even when there is a project highlighted

SDSCM00041649

IDE

After installing CCS, starting the setup program again causes "Program Compatibility Assistant" dialog

SDSCM00042122

IDE

Request to support loading of raw data format to Flash memory using Tools->Load Memory

SDSCM00043464

IDE

Differentiate between Standard Eclipse / CDT help and CCS IDE help

SDSCM00043913

IDE

In multicore debugging sessions, the debugger should have differentiator/identifiers of its elements for each core

SDSCM00044278

IDE

Install size reported is inflated

SDSCM00044371

IDE

CCS5.2.0.00069_linux crash shortly after startup when welcome screen displayed - Resource explorer/browser collides ds' xul

SDSCM00044374

IDE

CCS Editor: The parallel instruction syntax ('ll') is considered as a syntax for commenting for assembly files

SDSCM00045135

IDE

Headless projectCreate: add ability to set file/folder-level build-options

SDSCM00045301

IDE

CCS refresh compiler options GUI for each new compiler patch release (only currently for major/minor releases)

SDSCM00045352

IDE

Syntax highlighting for GEL files

SDSCM00045780

IDE

Full Verification of Code Download to MSP430 BSL fails

SDSCM00045853

IDE

RTSC Product Discovery should allow you to not be reminded for specific products

SDSCM00045895

IDE

Uninstaller hangs

SDSCM00045932

IDE

Linux: CCS crash when install GUI app or export app from GUI Composer

SDSCM00046042

IDE

CCS should automatically create the CGT built-in macros according to the project settings

SDSCM00046162

IDE

Hide hello world template for C2000 devices that don't have enough memory

SDSCM00046163

IDE

Helloworld template does not work for Stellaris

SDSCM00046166

IDE

Helloworld template doesn't work for common MSP devices

SDSCM00046393

IDE

Unable to connect to Stellaris Launchpad on Linux

SDSCM00046611

IDE

Request for command line projectBuild to be able to specify path/version of compiler tools to use for build

SDSCM00047075

IDE

MSP 430 only install contains ARM, C2000 and C6000 bios examples in TI Resource Explorer

SDSCM00047169

IDE

Improve usability for replacing tabs with spaces in the editor

SDSCM00047262

IDE

CCS Installer should by published by Texas Instruments

SDSCM00047339

IDE

'Test Connection' option in Target Configuration editor only tests first emulator defined

SDSCM00047365

IDE

Support comments in macros.ini and vars.ini files

SDSCM00047371

IDE

Ability to warn user to check their build and path variables on project import

SDSCM00047372

IDE

Ability to manage and modify/fix header specifications in the source

SDSCM00047399

IDE

Problems view does not display full text of error/warning

SDSCM00047457

IDE

Ability to sort 'Discovered projects' list alpha-numerically

SDSCM00047462

IDE

Breakpoint doCelarTriggerBps can run into concurrent modification exception

SDSCM00047524

IDE

Request to be able to modify flags set using "Set Additional Flags" using the same dialog box rather than the GUI options

SDSCM00047561

IDE

MSP430 - manual JTAG or Spy-Bi-Wire selection offered

SDSCM00047562

IDE

Rebuild of main project passes even if build of dependent library project fails

SDSCM00047576

IDE

Unable to generate code coverage data via DSS

SDSCM00047614

IDE

Scripting Console: Button to open/load a javascript file

SDSCM00047744

IDE

legacy format header files not handled correctly

SDSCM00047834

IDE

DS initiated progress dialog should consider the dialog option "Always Run on Background"

SDSCM00047846

IDE

Once I start a CCS debug session, build all will popup a modal progress box

SDSCM00047876

IDE

Floating point format not available in the Memory Browser view for C66x

SDSCM00048068

IDE

[C28 Flash] Flash programming does not work with "Auto Run on Reset" option on

SDSCM00048113

IDE

Adding RTSC support to a non-RTSC project sets it to wrong RTSC target

SDSCM00048152

IDE

Importing a SYS/BIOS project created with older version of CCS causes migration errors

SDSCM00048177

IDE

Scan compiler options files to improve conditional formatting

SDSCM00048225

IDE

Flash programming sometimes results in error "Timed out while writing to Flash memory"

SDSCM00048248

IDE

Breakpoint on a single source line causes the debugger to break twice before resuming execution

SDSCM00048258

IDE

Importing a CCS3.3 library project with project dependencies results in java.lang.NullPointerException

SDSCM00048265

IDE

In the compiler selection drop-down the listing for gcc should include the executable name

SDSCM00048309

IDE

Missing .ebss and .reset directive highlights for C2000 cmd file

SDSCM00048344

IDE

Class members are not shown in Variables view for code built with GCC

SDSCM00048357

IDE

MSP430 Trace View does not refresh properly when decoding instructions

SDSCM00048384

IDE

Project import tool sometimes does not resolve paths correctly

SDSCM00048388

IDE

Provide more precise error messages in Import CCS Project wizard

SDSCM00048408

IDE

Switching between two projects can sometime get GUI Composer out of sync

SDSCM00048410

IDE

Display demangled names instead of root name in disasm view

SDSCM00048417

IDE

The compiler option -v that specifies the silicon version is retained when switching device variants

SDSCM00048446

IDE

Flashing fails on Stellaris TM4C129X devices

SDSCM00048462

IDE

Makefile validation errors prevent makefile re-generation

SDSCM00048468

IDE

The Location of local variables is sometimes displayed incorrectly for GCC ELF files

SDSCM00048553

IDE

Include paths using "workspace_loc: variable are not passed to the compiler if the path does not exist

SDSCM00048568

IDE

Request to have LCD option for meter widget

SDSCM00048569

IDE

Request to have an out of range indicator option for gauges and meters

SDSCM00048612

IDE

CCS fails to program certain .out files when "Auto ECC generation" is enabled in Flash Settings

SDSCM00048700

IDE

Using a custom perspective copied from the 'CCS Debug' perspective is missing some DVT menus

SDSCM00048759

IDE

Deadlock due to "buddy" classloading

SDSCM00048906

IDE

Invoking gmake with -s option causes the Problems view to not update after errors have been corrected

SDSCM00048918

IDE

Would like a method to disable Optimization Advice

SDSCM00049002

IDE

App center in installer shows MSP430 content even when MSP not selected

SDSCM00049053

IDE

Request fpr Memory Allocation view to show UNION sections

SDSCM00049115

IDE

GUI Composer launcher.exe should accepts additional vmargs from the command line

SDSCM00049202

IDE

Directory structure affecting project import

SDSCM00049209

IDE

Post-build steps to generate flash images need to be updated for GCC

SDSCM00049212

IDE

List .hex in the list of valid extensions for a program to load

SDSCM00049265

IDE

Dependency build order is not as expected

SDSCM00049332

IDE

Unable to change options set via "Additional Flags" unless enclosed in quotes

SDSCM00049339

IDE

Profile Clock shows incorrect count on MSP430

SDSCM00049426

IDE

Unable to save memory contents to file on Windows Desktop

SDSCM00049438

IDE

Project Import dialog should not resize off the screen

SDSCM00049449

IDE

CCS Installer reports  gnome-vfs2 as a missing dependency even when it is installed

SDSCM00049450

IDE

CCS Installer dependency checker misses libcanberra-gtk-module:i386

SDSCM00049451

IDE

Project Wizard device drop-downs are VERY slow on Linux

SDSCM00049473

IDE

CCSv6.0 installer creates bogus Start Menu entries

SDSCM00049495

IDE

Some projectspec settings are lost when imported in Turkish locale Windows

SDSCM00049563

IDE

CCS does not use the correct bit size for long long variables ( c2x, COFF debug info )

SDSCM00049569

IDE

Fast Verification does not work

SDSCM00049593

IDE

CCS App center throws a java.null.lang error if the PC does not have an active internet connection

SDSCM00049602

IDE

Implementation of SDSCM00039843 (default adaptive clocking setting) broke in CCSv5.4

SDSCM00049604

IDE

Hello world program built with Linaro GCC for Tiva C does not load to target

SDSCM00049606

IDE

A ControlSuite project that builds without errors in CCS 5.5 now generates build error in CCSv6

SDSCM00049656

IDE

Update setpath.bat to apply to CCSv6

SDSCM00049724

IDE

Changing the compiler tools from TI to MSP GCC does not automatically change the linker command file

SDSCM00049768

IDE

Project Wizard device drop-downs are VERY slow on Linux

SDSCM00049798

IDE

It takes too long to display all the tabs for a multi-core device in the project wizard.

SDSCM00049803

IDE

CCS fails in the presence of VMWare shared folders

SDSCM00046862

Simulation

66AK2H12 simulator : Source line Step over on  function calls  is not working for CortexA15 cores

SDSCM00045277

Trace

ETB is not working on DM365 and DM368

SDSCM00046146

Trace

Setting a trace end job completely disables the Trace generation

SDSCM00048594

Trace

DM814x Trace shows a Device ID mismatch in Linux

SDSCM00048596

Trace

DM816x core Trace shows nothing at the Trace Analyzer view in Linux

SDSCM00048597

Trace

OMAP4 and OMAPL138 Trace fails to properly initialize in CCS for Linux

SDSCM00049318

Trace

Data Mask property missing for Data Watchpoints on 28x

SDSCM00049499

Trace

Crash on Terminate with XDS200 on Ubuntu 12.04 LTS 32bit

 


Component Versions

Windows/Linux

 

Software Components

Version

IDE

 

Eclipse

4.5.1

Code Composer Plugins

6.2.0.N201608311100

CCS Launcher

6.2.0.20160106

CCS Utilities

1.0.0.20160210

JRE

1.7.0.80

TIREX Desktop

v2.0.2.125

Compilers

 

C2800 

15.12.3.LTS

C5500 

4.4.1

C6000 v7 

7.4.18

C6000 v8

8.1.1

MSP430 

15.12.3.LTS

ARM 

15.12.3.LTS

GCC ARM (LaunchPad)

4.9.3.2015q3_20150921

On-line Documentation

1.1.4.0

Device Support

 

C2000

4.1.7.0

C55xx 

1.1.6

C6000 

1.1.2

C6000 Multicore 

1.0.5

CC2538 

2.0.0.00

CC26xx

2.0.0.00

CC32xx

1.0.8

DaVinci 

1.1.3

Hercules 

6.0.7.0

Keystone1 

1.0.12.0

Keystone2

1.1.7.0

MSP430 

6.3.4.4

MSP432

6.3.0.5

OMAP 

1.0.9

OMAPL / Integra 

1.0.9

Sitara 

1.3.2

Stellaris 

2.0.3.12770

Tiva-C Series ARM MCU

2.1.1.15071

Tiva-E Series ARM MCU

2.1.1.15071

UCD31xx

1.1.0

Other / Shared

1.0.9

Debugger / Emulation

 

Debug Server

6.2.1.1781

Debug Server Flash

6.2.1.1781

TI Debug/Trace 

6.0.407.3

C2000 Flash 

1.0.0.2

Tiva/Stellaris ICDI Debug Probe

2.1.3.15

BeagleBone FTDI Drivers

2.8.30.20140130

Blackhawk 

6.0.83.003

Spectrum Digital 

5.2.0.14

Analysis Tools

 

Data Visualization Tools

4.1.0.201608181627

Other Tools

 

Graphical Modeling Framework

1.7.0

Target Content Core

3.32.1.22

MSVC 2012

11.0.61030

MSVC 2005

6.0.2900.2180

Add-ons

 

E.g., MSP430Ware, GCC/MSP430, GUI Composer, ControlSuite, TI-RTOS, etc.

available via
Resource Explorer and CCS App Center

OS X 

Software Components

Version

IDE

 

Eclipse

4.5.1

 

Code Composer Plugins

6.2.0.N201608311100

 

CCS Launcher

6.2.0.20160106

 

CCS Utilities

1.0.0.20160210

 

JRE

1.7.0.80

 

TIREX Desktop

v2.0.2.125

 

Compilers

 

C2800 

15.12.3.LTS

 

C5500 

4.4.1

 

MSP430 

15.12.3.LTS

 

ARM 

15.12.3.LTS

 

GCC ARM (LaunchPad)

4.9.3.2015q3_20150921

 

On-line Documentation

1.1.4.0

 

Device Support

 

C2000

4.1.7.0

 

C55xx 

1.1.6

 

CC2538 

2.0.0.00

 

CC26xx

2.0.0.00

 

CC32xx

1.0.8

 

Hercules 

6.0.7.0

 

MSP430 

6.3.4.4

 

MSP432

6.3.0.5

 

Stellaris 

2.0.3.12770

 

Tiva-C Series ARM MCU

2.1.1.15071

 

Tiva-E Series ARM MCU

2.1.1.15071

 

Debugger / Emulation

 

Debug Server

6.2.1.1781

 

Debug Server Flash

6.2.1.1781

 

TI Debug/Trace 

6.0.407.3

 

C2000 Flash 

1.0.0.2

 

Tiva/Stellaris ICDI Debug Probe

2.1.3.15

 

Analysis Tools

 

Data Visualization Tools

4.1.0.201608181627

Other Tools

 

Graphical Modeling Framework

1.7.0

Target Content Core

3.32.1.22

Add-ons

 

E.g., MSP430Ware, GCC/MSP430, GUI Composer, ControlSuite, TI-RTOS, etc.

available via
Resource Explorer and CCS App Center

 


Known Issues

dbid

id

Component

Headline

Workaround

Planned Resolution

CCBT-1833

SDSCM00052534

Code Composer Studio

Disabling "Auto ECC generation" Flash Option does not have any effect

 

CCS 6.2.0

CCBT-1862

SDSCM00052782

Code Composer Studio

Debug info about GCC C++ namespaces alias and namespace import are not processed correctly

 

CCS 6.2.0

CCBT-1321

SDSCM00047055

Code Composer Studio

Support for debugging RealView Compiler output including Semi-hosting

 

CCS 7.0.0

CCBT-1484

SDSCM00048600

Code Composer Studio

CCS needs to interpret .debug_macinfo ( was: Symbol not found when adding expression )

Inspect the generated map file for the program. Look for the symbol name and note its fully qualified name. Use the long name in the watch window or in the disassembly window when setting breakpoints.

CCS 7.0.0

CCBT-1607

SDSCM00050372

Code Composer Studio

CCS needs to interpret .debug_macinfo (GCC support)

Inspect the generated map file for the program. Look for the symbol name and note its fully qualified name. Use the long name in the watch window or in the disassembly window when setting breakpoints.

CCS 7.0.0

CCBT-1780

SDSCM00052109

Code Composer Studio

static string constants cannot be displayed if gcc stores the string in .debug_str using DW_AT_const_value TAG.

 

CCS 7.0.0

CCBT-1782

SDSCM00052111

Code Composer Studio

Debug info about GCC C++ templated functions are not processed correctly

 

CCS 7.0.0

CCBT-1814

SDSCM00052390

Code Composer Studio

Estimated RAM usage printed in the console is not accurate

The Memory Allocation view tends to display more accurate information

CCS 7.0.0

CCBT-1625

SDSCM00050620

Code Composer Studio

Request command line utility to dump out the type information for every symbol

 

Revisit 2015 Q2

CCBT-1726

SDSCM00051715

Code Composer Studio

Add ability to edit flash contents from the memory view for MCUs other than MSP430

 

Revisit 2016 Q2

CCBT-1350

SDSCM00047285

Code Composer Studio

Support Linux OS Aware Debug

 

Revisit 2016 Q4

CCDSK-2165

 

Code Composer Studio

ARM GCC add-on fails to install from App Center on MacOS X due to an error in the update feature

Install ARM GCC using the main CCS installer rather than from App Center. To do this:
- Re-run the CCS installer
- For "CCS Install Folder" choose your existing install folder
- expand the Product Family tree and select GCC ARM Compiler
- proceed with the installation

CCS 6.2.0

CCDSK-2051

 

Code Composer Studio

In Linux, chromium browser should open PDF internally

6.2 will use xulrunner as the browser engine by default on linux. In order to get inplace viewing of pdf files to work, the following steps are required :

Install acrobat reader : follow instructions at the link http://askubuntu.com/questions/89127/how-do-i-install-adobe-acrobat-reader-deb-package-downloaded-from-adobe-website

then create a directory in CCSInstallDir/ccsv6/eclipse/xulrunner called "plugins"

then copy nppdf.so file, which should be located in /usr/lib/mozilla/plugins to above created directory (i.e. it should be in CCSInstallDir/ccsv6/eclipse/xulrunner/plugins)

Note that the above workaround is not confirmed on all Linux environments.

CCS 7.0.0

CCDSK-2103

 

Code Composer Studio

[Eclipse] Project import errors should be formatted to the size of the message box

 

CCS 7.0.0

CCDSK-2104

 

Code Composer Studio

Project import wizard should not leave failed attempts in the workspace

 

CCS 7.0.0

CCDSK-2188

 

Code Composer Studio

Emulation driver install scripts failing to restart udev on CentOS 7

Execute
sudo systemctl restart systemd-udevd

CCS 7.0.0

CCDSK-2202

 

Code Composer Studio

kernel usb rules for msp430 are not installed

After installation execute the following script with sudo permissions
<install folder>/ccsv6/ccs_base/../install_scripts/msp430uif_install.sh --install

CCS 7.0.0

CCSIDE-1944

SDSCM00047490

Code Composer Studio

Rebuild of index for updating macro expansions does not permeate through multiple levels of include files

 

3P

CCSIDE-2328

SDSCM00050521

Code Composer Studio

Autoformat (ctrl + shift + F) can alter formatting of source files which can cause compiler errors.

 

3P

CCSIDE-2491

SDSCM00051637

Code Composer Studio

Refactor->Rename does not work for structure members inside extern "C

 

3P

CCSIDE-2495

SDSCM00051647

Code Composer Studio

Scanner discovery functionality for GCC projects is not working

N/A. Use CCSv6.0.1

3P

CCSIDE-28

SDSCM00034880

Code Composer Studio

CCS is not finding source files from an included library

 

4.1, CCS 4.1.1 GA

CCSIDE-2809

SDSCM00034676

Code Composer Studio

CCS hangs on startup if Source Control integration is enabled and the provider is ClearCase 7.x

 

4.1

CCSIDE-215

SDSCM00036170

Code Composer Studio

Real-time mode menu items are displayed with funny characters

 

4.1.3, CCS 4.1.3 GA

CCSIDE-80

SDSCM00035255

Code Composer Studio

Need scripting console function to set active build configuration

 

5.0.0 LR, CCS 5.0.0 LR, idecore_setup_5.0.0.N201008311900

CCSIDE-2575

SDSCM00052319

Code Composer Studio

On OS X, several dialogs that are meant to allow user to save to file do not give the option to specify file name

 

CCS 6.1.2 OS X GA

CCSIDE-982

SDSCM00039747

Code Composer Studio

Changing a device should not reset the properties of an emulator

 

CCS 6.2.0

CCSIDE-1969

SDSCM00047723

Code Composer Studio

In the Target Configuration Editor, changing the "Device" or the "Connection" should not reset to all defaults

N/A.

CCS 6.2.0

CCSIDE-2512

SDSCM00051812

Code Composer Studio

After refactoring a project or simply changing XDCTools version, the RTSC Target field gets changed

 

CCS 6.2.0

CCSIDE-2499

SDSCM00051716

Code Composer Studio

Need connection between Project Debug Properties and the ccxml (target configuration) file

 

CCS 6.3.0

CCSIDE-813

SDSCM00038559

Code Composer Studio

[CDT] Add the ability to specify the build-directory for CCS projects

 

CCS 7.0.0

CCSIDE-814

SDSCM00038571

Code Composer Studio

Need excluded files filter for the Project Explorer

 

CCS 7.0.0

CCSIDE-2191

SDSCM00049607

Code Composer Studio

[CDT] Enhance Codan plug-in with the ability to create custom rules

Use other 3rd party Code Analysis plug-ins that support this feature

CCS 7.0.0

CCSIDE-2323

SDSCM00050489

Code Composer Studio

Once launch configuration has been created, can't switch from load symbols back to load program

Simplest way of making the change without deleting launch configuration is to use "Debug Configurations..." dialog (Run-> Debug Configurations...) change the load program/load symbols setting works correctly using that path.

CCS 7.0.0

CCSIDE-2329

SDSCM00050527

Code Composer Studio

App Center should display current version, new version and link to release notes

 

CCS 7.0.0

CCSIDE-2333

SDSCM00050556

Code Composer Studio

Memory Usage View should support GCC

 

CCS 7.0.0

CCSIDE-2500

SDSCM00051717

Code Composer Studio

Remember register expansion state and position across debug invocations

 

CCS 7.0.0

CCSIDE-2508

SDSCM00051773

Code Composer Studio

In TI-RTOS programs, source file correlation and interleaved source in disassembly view is incorrect for the boot routine

 

CCS 7.0.0

CCSIDE-2515

SDSCM00051839

Code Composer Studio

Cannot open PDFs from Resource Explorer

 

CCS 7.0.0

CCSIDE-2516

SDSCM00051840

Code Composer Studio

Provide a large icon set on Eclipse for a better experience with High Definition monitors

A hack is proposed at the following link:
http://stackoverflow.com/questions/20718093/eclipse-interface-icons-very-small-on-high-resolution-screen-in-windows-8-1

CCS 7.0.0

CCSIDE-2529

SDSCM00051932

Code Composer Studio

Remove MMU Page Table view from CCS

Use DSS APIs instead, as documented here:
https://processors.wiki.ti.com/index.php/Page_Table_Visibility_DSS_API%27s

CCS 7.0.0

CCSIDE-2607

SDSCM00052518

Code Composer Studio

When multiple target configurations are created for a project, is debug configuration manglee the loadable cores

Additional details at the forum thread below:
https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/471579

CCS 7.0.0

CCSIDE-2620

SDSCM00052612

Code Composer Studio

Add ability to delete generated assembly listing files as part of "clean" operation

 

CCS 7.0.0

CCSIDE-2878

 

Code Composer Studio

Enabling parallel build on MacOS results in "fcntl(): Bad file descriptor" message

 

CCS 7.0.0

CCSIDE-2905

 

Code Composer Studio

Head-less project import command should fail if specified workspace folder is in use

Close any CCS instance that is using the same workspace folder

CCS 7.0.0

CCSIDE-1938

SDSCM00047442

Code Composer Studio

New project wizard should only create one default build configuration

 

Revisit 2015 Q2

CCSIDE-2570

SDSCM00052235

Code Composer Studio

Resource Explorer fails to create a project from the MSPWare Code Examples

N/A

Revisit 2015Q4

CCSIDE-2525

SDSCM00051903

Code Composer Studio

Formatter will add improper indentation when used on code where __attribute__ is used to pack structs and union

 

Revisit 2016 Q2

CCSIDE-2583

SDSCM00052402

Code Composer Studio

[CDT] CDT should not persist build options names on the .cproject file

Make the modifications and check-in the version of the file with the additional “name” attributes, and after that there shouldn’t see these bogus changes anymore.

Revisit 2016 Q2

DVT-786

SDSCM00045827

Code Composer Studio

Using JTAGRunMode with stairstep example on LM4F232 results in "trouble reading memory block" error

 

CCS 6.2.0

DVT-1241

SDSCM00051727

Code Composer Studio

System Analyzer does not work if Runmode and buffer in DDR3

 

CCS 6.2.0

DVT-269

SDSCM00039329

Code Composer Studio

Profiling help topic is missing screen captures

 

CCS 7.0.0

DVT-796

SDSCM00046280

Code Composer Studio

Image Analyzer does not process 8bit data read in big endian for RGB correctly

Customer was able to workaround this using 32bit Data Read. See Forum Post for details:

http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/240677/844253.aspx#844253

CCS 7.0.0

DVT-1169

SDSCM00050087

Code Composer Studio

Ability to show user events in Execution Graph

 

CCS 7.0.0

DVT-1234

SDSCM00051495

Code Composer Studio

Graph Q_Value parameter should allow values larger than 30

N/A.

CCS 7.0.0

DVT-1264

SDSCM00052155

Code Composer Studio

Loading a saved trace configuration does not work

 

CCS 7.0.0

DVT-1266

SDSCM00052254

Code Composer Studio

Request to enhance the visibility of the plot inside the Graph tool when using grids

 

Revisit 2016 Q2

DVT-46

SDSCM00035897

Code Composer Studio

Dual graphs should support independent data Types

 

Revisit 2016 Q4

DVT-53

SDSCM00035986

Code Composer Studio

Useful to have magnitude in logarithmic although db would be even better

 

Revisit 2016 Q4

DVT-203

SDSCM00037952

Code Composer Studio

Graph Tool should allow the use of arrow keys to navigate through the buffer and the graph

The graph can be navigated using the mouse.

Revisit 2016 Q4

DVT-329

SDSCM00040280

Code Composer Studio

Ability to select cached or uncached external memory access in the Graph Tool and Image Analyzer

N/A.

Revisit 2016 Q4

DVT-343

SDSCM00040469

Code Composer Studio

Use profile data to compute CPU loading

 

Revisit 2016 Q4

DVT-346

SDSCM00040472

Code Composer Studio

Would like to pick out a range of data to display

 

Revisit 2016 Q4

DVT-459

SDSCM00041366

Code Composer Studio

Code Coverage coloring does not work for files that do not have a CCS Project

 

Revisit 2016 Q4

DVT-1166

SDSCM00050047

Code Composer Studio

System Analyzer/UIA data transfer via JTAG should have a progress bar

N/A.

Revisit 2016 Q4

DVT-1250

SDSCM00051816

Code Composer Studio

Number of records on Trace display roll over for large data collections

N/A

Revisit 2016 Q4

DVT-1270

SDSCM00052456

Code Composer Studio

In Graph view, measurement markers set for Y-axis or both axes do not display values

 

Revisit 2016 Q4

DVT-1272

SDSCM00052660

Code Composer Studio

Request to be able to save and restore debug perspective with Graph view open during successive invocations of CCS

 

Revisit 2016 Q4

DVT-1316

SDSCM00050650

Code Composer Studio

CCS for Linux shows GTK and DVT errors errors when launched from the command line (DVT Text)

 

Revisit 2016 Q4

DVT-1324

SDSCM00050619

Code Composer Studio

Trace viewer should not reset its display arrangement when a column is added/restored

N/A.

Revisit 2016 Q4

DVT-1325

SDSCM00050622

Code Composer Studio

Trace display should allow cumulative storing of data between start/stop jobs

Save to .csv/.tdf every step on the way.

Revisit 2016 Q4

DVT-1265

SDSCM00052222

Code Composer Studio

Lose editor area if Trace Viewer is the only editor open when you restart CCS

Go to the Window menu and select Switch to Editor. Click the select all button. Then click on the close button.

CCS 7.1

CCBT-1971

 

Code Composer Studio

Debugger loses line debugging and stack frame with GCC assembly code

N/A

 

CCDSK-2203

 

Code Composer Studio

kernel usb rules for msp430 contain a typo preventing G2 devices from working

The typo is that the value F432 should be f432. The complete line should be:

MSP430EZ430="ATTRS{idVendor}=="\"0451\"",ATTRS{idProduct}=="\"f432\"",MODE="\"0666\"""

in order to generate a line in the rules file like this:

ATTRS{idVendor}=="0451",ATTRS{idProduct}=="f432",MODE="0666"

 

CCSIDE-855

SDSCM00038857

Code Composer Studio

EASY: Simplified Build Options Dialog

 

 

CCSIDE-956

SDSCM00039559

Code Composer Studio

Would like ability to adjust file specific options on multiple selected files.

 

 

CCSIDE-1102

SDSCM00040259

Code Composer Studio

Merge the two CCS project import wizards

 

 

CCSIDE-1105

SDSCM00040262

Code Composer Studio

MMU Page table view should be listed on the view menu

 

 

CCSIDE-2573

SDSCM00052300

Code Composer Studio

When creating a new AM5726/28 project the target configuration will have errors

Open the ccxml file and click on 3 of the 4 ICECrusher nodes and give them a unique name.

Also if you create the target configuration from the target config editor it works fine and the entries all have unique names.

 

CCSIDE-2895

 

Code Composer Studio

Cannot step into C++ polymorphic function call

 

 

CCSIDE-2911

 

Code Composer Studio

Compiling with predefined symbol --define=SYM='A' strips off the single quotes around the character constant

 

 

CCSIDE-2922

 

Code Composer Studio

NullPointerException error when switching between build configurations for a project with out file generated outside project folder

Go into the project properties->Linked Resources and remove the “invalid” .out file resource that automatically gets added on every build

 

DBGTRC-2248

SDSCM00051476

Emulation

Add ability to view D0 - D31 and S0 - S31 floating point registers on Cortex A15

 

 

DBGTRC-2280

SDSCM00051900

Emulation

GDB Agent should perform flash operations on MSP432, Tiva and C2000 devices

Use Uniflash or CCS to flash your code.

 

DBGTRC-2349

SDSCM00052458

Emulation

Automatic firmware update for XDS200

Use the xds2xx_conf utility in \ccsv6\ccs_base\emulation\specdig\xds2xx to update the firmware. You must have installed support for Spectrum Digital Debug Probes.

 

DBGTRC-2353

SDSCM00052492

Emulation

dbgjtag should have a timeout option

N/A.

 

DBGTRC-2393

SDSCM00052733

Emulation

CC3200 SWD load failure on Linux

 

 

DBGTRC-2982

SDSCM00048795

Emulation

Trace: "End at address" of the "Trace Range" parameter fails to stop and display trace data

Use "Range" or "Start and stop at address" instead.

 

DBGTRC-3160

 

Emulation

CCS disassembly view was showing the raw .word value for some instructions rather than the actual instruction

 

 

DBGTRC-3183

 

Emulation

SIGSEGV when disconnecting from XDS100v1 on Ubuntu 16

 

 

DVT-484

SDSCM00041756

Code Composer Studio

Add ability in image analyzer to flip the image on either axis: up/down or left/right

 

 

DVT-1177

SDSCM00050408

Code Composer Studio

Request for a way to clear the printf log data without having to close the view

 

 

DVT-1178

SDSCM00050409

Code Composer Studio

Request for a way to be able to adjust and save column settings in system analyzer data views

 

 

DVT-1179

SDSCM00050410

Code Composer Studio

Request to add commas to timestamps in RTOS Analyzer views to make it easier to analyze the numbers

 

 

DVT-1190

SDSCM00050680

Code Composer Studio

Bookmarks in any DVT view (Trace/RTOS/System Analyzer) does not work with filtering and sorting.

None.

 

DVT-1326

SDSCM00052798

Code Composer Studio

Request to add back TPIU ITM trace support for Concerto

 

 

 


For up-to-date status information, go to:

https://cqweb.ext.ti.com/cqweb/main?command=GenerateMainFrame&service=CQ&schema=SDO-Web&contextid=SDOWP&username=readonly&password=readonly&queryID=37808810


Windows XP, Windows Vista, Windows 7, Windows 8, Windows 8.1, Visual SourceSafe, Visual Basic, and Visual C++ are all trademarks and/or registered trademarks of Microsoft Corporation.
C2000, C5000, C54x, C55x, C6000, C6x, CC2538, CC26xx, CC32xx, OMAP, TMS320, TMS570, MSP430, Stellaris, Tiva-C, Hercules, GUI Composer, Grace, Code Composer Studio, Code Composer Studio App Center, TI-RTOS, SYS/BIOS, XDS560, XDS510, XDS200, XDS100 and XDS110 are trademarks of Texas Instruments.
© Copyright 2015