Code Composer Studio 6 for Linux README --------------------------------------- Please visit http://processors.wiki.ti.com/index.php/Linux_Host_Support_CCSv6 before installing CCS on Linux. It contains important information on installing CCS on different Linux distributions, including CCS dependencies that may need to be installed first. Before installing CCS, the tarball file in which the CCS Installer is distributed must first be extracted: Untar CCS_6.x.x.xxxxx_linux.tar.gz or CCS_6.x.x.xxxxx_web_linux.tar.gz and extract all files. If installing from DVD, you also need to either mount the DVD with execute permissions first, or copy the files off the DVD to a local drive and change permissions there to run the installer. Once extraction has successfully completed, proceed with the installation steps below. Note: To facilitate the installation of emulation drivers, it is necessary to run part of the installation process as root. You may if you wish install all of CCS as root. However, it is preferred that you first install CCS as a normal user and then install the drivers as root. To install Code Composer Studio as a normal user and emulation drivers as root: 1. Run ccs_setup_6.x.x.xxxxx.bin as a normal user. 2. Choose where you want to install. 3. Select the components you wish to install. 4. Navigate to directory /ccsv6/install_scripts. 5. As root, execute script "install_drivers.sh". To install all of Code Composer Studio as root: 1. Run ccs_setup_6.x.x.xxxxx.bin as root. 2. Choose where you want to install. 3. Select the components you wish to install.